+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Resistance - definition

Resistance is a physical property of a material or an electrical circuit element that defines its ability to oppose the flow of electric current. Technically, it is a measure of electrical opposition that results in the conversion of electrical energy into thermal energy, in accordance with Joule's law. The resistance value depends on the type of material, its length, cross-sectional area, and temperature. The SI unit of resistance is the [ohm (Ω)](/dk/en/news/library-articles/page/61968/.

The phenomenon of resistance is associated with the interaction of free charge carriers, such as electrons, with the atoms of a conductor’s crystal lattice, which leads to energy loss in the form of heat. For materials with stable physical properties and constant temperature, the relationship between voltage and current is linear and described by Ohm's law, according to which resistance is the ratio of voltage to current. In practice, not all elements exhibit linear behavior—in such cases, the term nonlinear dynamic or differential resistance is used.

Resistance plays a fundamental role in the design and analysis of electrical circuits, influencing voltage drops, power distribution, and circuit stability. It is one of the key parameters used to characterize passive components such as resistors, which are primarily used to limit current, divide voltage, generate heat, or match impedance. Resistance also appears as an unwanted element in conductors, inductors, or printed circuit layouts, where it can cause losses and reduce efficiency.

In the context of materials science, the concept of resistivity—a material-specific parameter—allows for comparing the conductivity of different substances. Materials with low resistivity, such as copper or silver, are considered excellent conductors, whereas insulators exhibit high resistance and virtually block current flow. In power supply and signal transmission systems, accounting for resistance is essential to minimize energy losses and ensure the proper operation of devices.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO