+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Should the lithium-ion battery only be charged with the original charger?

No, a rechargeable lithium-ion battery does not need to be charged exclusively with the original charger, but the charger used must be technically compatible, safe and matched to the parameters of the device.

Why is not every charger suitable?

Modern lithium-ion Rechargeable Batteries require precise control of the charging voltage and current so that the process is safe and does not shorten the life of the cell. This function is usually supervised by the device's built-in battery management system (BMS), which protects the battery from overcharging, overheating or charging too quickly. However, the wrong charger, e.g. a cheap counterfeit or uncertified model, can generate unstable voltage, electromagnetic interference or too much current. In extreme cases, this leads to chemical degradation of the cell, loss of capacity and even the risk of overheating or ignition.

What chargers are safe?

The most important thing is that the charger is compatible with the voltage and amperage required by the device. Good quality Power Supplies, even replacements, should be certified (e.g. CE, UL, FCC) and equipped with protection systems - short circuit, overcurrent and temperature. When charging via USB-C connectors, it is also important to comply with fast charging standards, such as USB Power Delivery (PD) or Qualcomm Quick Charge. Non-compliance can result in slow charging or a completely unresponsive device.

What does the original charger give you?

Chargers supplied with your device are designed with your device's specific energy needs in mind and are tailored to your battery's operating profile. They therefore offer the highest assurance of correct charging, but are not the only safe option as long as the replacement used is proven and branded.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO