+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Dynamic compression - Definition

Dynamic compression is a technique used in the field of signal processing audio to reduce the dynamic range of an audio signal, i.e. the difference between its quietest and loudest parts. It involves automatically reducing the level of the louder signals and leaving or amplifying the quieter ones, so that the whole becomes more uniform in terms of loudness. This makes it easier to listen in noisy environments, improves speech intelligibility and reduces the risk of overdriving the acoustic path.

The circuit that performs this function, called compressor, analyses the amplitude level of the input signal and reduces its value if it exceeds a set threshold. This process takes place in real time, taking into account parameters such as attack time, return time, compression ratio and threshold point. This makes it possible to precisely shape the dynamic characteristics of the signal, which is important in studio recordings as well as in live broadcasting, radio broadcasting, public address systems or portable devices.

Dynamics compression does not change the content of the signal, but modifies its perception by equalising volume levels, which improves listening comfort and facilitates further audio processing. In professional productions, it is also used to create sound, emphasise transients or produce characteristic sound effects. In digital and analogue systems, tone mapping can be implemented using electronics, DSP algorithms or in the form of software plug-ins in DAW environments.

The use of tone mapping requires precise adjustment of the parameters to the type of audio material and listening conditions, as excessive compression can lead to a loss of naturalness and spatiality in the sound. In broadcast systems and application equipment, this technique is often integrated with automatic level control and peak limiting processes, forming an important part of the quality control of acoustic transmission.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.