+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
SCSI (Small Computer System Interface) is a standardised communication interface used to connect and transfer data between a computer and peripherals such as hard drives, optical drives, scanners, printers or magnetic tapes. SCSI was developed in the 1980s as a versatile and architecture-independent solution for high performance, flexibility and compatibility in workstation and server-class computer system environments.
The basis of SCSI is a bus to which multiple devices (typically up to 8 or 16) can be connected, with the ability to address them by unique SCSI IDs. Each device can act as an initiator (controller) or a target (peripheral), allowing data to be transferred between each other without involving the CPU in the detailed transmission flow. This interface supports both parallel and serial transmission modes, depending on the version of the standard.
SCSI versions have evolved from classic parallel SCSI (e.g. SCSI-1, SCSI-2, Ultra SCSI) to modern high-speed serial implementations such as Serial Attached SCSI (SAS), providing much higher bandwidth and better scalability. Parallel versions required signal terminators and were more susceptible to interference with longer cable lengths, limiting their use in very large systems.
SCSI gained recognition in professional applications due to its support for command queuing, independence of data protocols from the physical hardware layer, and the ability to support multiple operations in parallel.](/ng/en/news/library-articles/page/69352/) In operating systems and hardware controllers, the protocol is supported by a layer of drivers, allowing efficient management of I/O operations and integration with enterprise-class Mass Storage systems [. Despite the growing popularity of interfaces such as SATA, NVMe and USB, SCSI-based solutions are still used in servers, disk arrays and data archiving systems, especially where reliability and high availability are important.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.