+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Favourites

Favourites (former name: Parking) facilitate shopping at TME. They contain products added by the user, as well as those automatically added by the system, e.g. in the case of unsettled orders. This allows you to keep track of your choices without having to search through the product tree or use the search engine. Favourites can be accessed after you log in to the system.

You can either add individual products from the catalogue to your Favourites or transfer there entire orders which were not sent with the use of the “complete order” button. Favourites are also available from the Quick Buy level.

When adding items to your Favourites, select or create a folder in which the products are to be placed. Grouping products in this way will allow for easy product management and facilitate product search.

Please note that leaving products in your Favourites does not result in the booking of goods in the warehouse and does not guarantee that the prices that were valid at the moment of adding products to the folder will remain the same.