+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Induction motor - definition

The induction motor, also known as an asynchronous motor, is the most widely used type of electric motor alternating current (AC), in which torque is generated by the phenomenon of electromagnetic induction between the stator and the rotor. The principle of operation is based on the fact that the alternating magnetic field generated by the stator windings induces current in the conductors of the rotor, which in turn generates its own magnetic field that interacts with the stator field, causing the rotor to rotate.

A characteristic feature of the induction motor is that there is no direct electrical connection between the power supply and the rotor, which simplifies the design and increases reliability. The rotor, depending on the type of design, can be made in the form of a so-called cage (squirrel-cage induction motor) or have windings, as in the case of ring motors. In both cases, torque occurs due to the difference in speed between the magnetic field rotating in the stator and the actual speed of the rotor - hence the origin of the term 'asynchronous'.

Induction motors are most commonly found in three-phase versions, due to their better starting characteristics and higher energy efficiency, although single-phase versions are also available, mainly used in household and simple mechanical appliances. Speed control is possible by varying the frequency of the power supply, which in practice is achieved by means of frequency converters (inverters).

Thanks to their simple design, durability, low operating costs and high efficiency, induction motors are the primary source of drive in industry, especially in pump systems, fans, compressors, conveyor belts and many other mechanical devices. Today's Automation systems use them in combination with modern control systems, allowing precise and energy-efficient management of technological processes.

[Asynchronous motors](/en https://www.tme.eu/pl/katalog/silniki-elektryczne_100611/?params=1885:1454931;1886:1499856_typ-silnika:ac;rodzaj-silnika:synchroniczny){.cs-btn-primary}

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO