+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Can I use the Arduino as a joystick emulator (HID)?

Yes, the Arduino can emulate a joystick (USB-HID), but not all boards can do this. The HID function is supported by models with a native USB controller, most notably Arduino Leonardo and Arduino Micro based on ATmega32U4. These boards can report to the computer as an HID device (e.g. joystick) and work with dedicated libraries.

Which boards are suitable for HID?

The key is the presence of a USB controller in the microcontroller itself. The ATmega32U4 has a built-in USB interface so that the Leonardo and Micro can act as a mouse, keyboard or joystick without additional circuitry. In practice, libraries in the style of ArduinoJoystickLibrary, which provide axes, buttons and hat-switch in the HID standard, are used. The operating system sees such a board as a normal gamepad. The Arduino Uno and Nano (ATmega328P) do not have native USB, so their USB connector is implemented by a separate bridge chip (e.g. ATmega16U2 in the Uno R3 or CH340 in clones). Such boards present themselves to the system by default as virtual-serial port (USB-Serial), not as an HID device. This is an architectural difference: the lack of a USB controller in the MCU means that, without additional hardware, these models do not emulate a Joystick 'out of the box'. Identification by microcontroller type is the surest test: 32U4 ⇒ HID possible, 328P ⇒ no native HID.

How does this work in practice?

On boards with 32U4, the sketch configures the HID descriptor and maps the inputs (e.g. Potentiometers, buttons) to the axes and buttons of the joystick. The system recognises the device immediately as HID, without installing additional game controllers. This path is well documented and commonly used in simulator projects, control panels and DIY cockpits.

What to look out for technically?

When choosing a board for HID, make sure you really have a variant with either the ATmega32U4 or another platform with native USB. You can quickly check this by the microcontroller designation on the PCB or in the board's specification; the document distinguishes this explicitly by indicating the 32U4 as an MCU with native USB-HID. It's also worth remembering that boards without native USB (Uno/Nano), although great for I/O control, communicate with the PC as a serial port and won't appear in the system as a joystick without changing the hardware platform. If you're after simplicity and full gaming compatibility, choosing a Leonardo or Micro significantly shortens the path to a working controller.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO