+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Yes, frequent writes to an SD Memory Cards shorten its lifespan, as each write operation consumes the flash memory cells of which the medium is composed. The more intensively the card is used, the faster it reaches the limit of its technological capacity.
Memory Cards use NAND flash memory, which has a specific number of write and erase cycles assigned to each cell. In simple terms, each write of data causes microscopic degradation of the memory cell structure, until the cell becomes unstable and loses its ability to store information. This phenomenon is referred to as wear-out. In consumer cards, typical endurance values are a few thousand write cycles for each cell. Once these are exceeded, the card may start to become unstable, lose data or switch to read-only mode (which prevents further writes, but still allows some data to be read).
The greatest wear and tear occurs in devices that generate a continuous stream of data, such as car DVRs, surveillance cameras, drones or cameras in continuous shooting mode. In these cases the card can wear out after just a few months, especially if it is a cheaper model with a low endurance rating. In contrast, with occasional use, e.g. for carrying documents or photos, write cycles are used much more slowly, so a card can operate without failure for many years.
Modern Memory Cards use 'wear leveling' techniques, i.e. distributing writes evenly between cells to avoid rapid wear and tear of only part of the memory. However, this does not change the fact that the total number of write cycles is limited. For high-volume applications, it is recommended to use "high endurance" cards, which contain more robust cells and are designed specifically for long-term writing. Such media can achieve write limits up to ten times higher than standard cards. By understanding the limitations of flash technology, it is possible to better match a card to a specific application and avoid the risk of sudden data loss.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.