+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

How long can the Raspberry Pi run on batteries?

Raspberry Pi's battery life depends mainly on the model, the type of power supply used and the system load - and can range from a few tens of minutes to several hours.

Power consumption vs. runtime

Raspberry Pi is a single board computer that, unlike typical microcontrollers, has a fairly complex architecture, including a full operating system, communication ports and a multi-core processor. This means that its power consumption is relatively high compared to simple embedded devices. For the Raspberry Pi 5, typical power consumption is around 2.7 W at rest and even 11 W under full load. In contrast, Raspberry Pi 4 consumes correspondingly less - between 1.4 and 6.5 W on average, depending on the operating mode and the number of active peripherals.

Practical example of power supply from a powerbank

The Raspberry Pi is most often powered by so-called powerbanks, which are portable batteries with a voltage of 5V and a capacity in the order of 10,000mAh (or 10Ah). In order to estimate the operating time, it is necessary to convert the battery capacity into energy expressed in watt-hours (Wh). For 10,000mAh at 3.7V (the typical voltage of lithium-ion cells in a powerbank), this gives approximately 37Wh of available energy (in practice less due to losses). If the Raspberry Pi 4 is operating under typical conditions and consuming around 4W, the runtime from such a battery will be around 9 hours. For the Raspberry Pi 5, which can consume up to 11W, the same powerbank will only be sufficient for about 3 hours of heavy-duty operation. It is worth remembering that the real operating time will depend on a number of factors, such as:

  • processor mode (default ondemand or forced performance)
  • type of storage media (an SSD consumes more power than a microSD card)
  • connected peripherals (mouse, keyboard, screen)
  • presence of active cooling (fan also consumes power)

    Battery power in practice

    In mobile or field applications where mains power is not available, a Raspberry Pi powered by Batteries can serve as a measurement station, IoT terminal or portable computer. In such projects, it is very important to optimise power consumption - it is a good idea to disable unnecessary interfaces (e.g. HDMI, Wi-Fi) and to run the system in headless mode, without a graphical environment.

The lower the load on the system, the lower the power consumption and therefore the longer the battery life.

For projects that require very long continuous operation (e.g. environmental monitoring), it is possible to use larger lithium polymer (LiPo) batteries or solar power with an energy buffer, allowing 24-hour operation.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO