+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
No, magnets do not have positive and negative poles. Instead, they have north (N) and south (S) poles, which are not equivalent to electric charges. This common misunderstanding is due to confusion between the concepts of a magnetic field and an electrostatic field, where there are actually positive and negative charges.
Magnet poles are the areas where the magnetic field strength is strongest. We call one end of a magnet the north pole and the other the south pole. This nomenclature comes from the observation that a freely suspended magnet (e.g. a compass needle) aligns along the line of the Earth's magnetic field, while the end pointing north is considered the 'north' pole. Unlike electrical charges, magnetic poles cannot be separated. Cutting a magnet in half does not create separate poles - each of the resulting fragments will have its own north and south poles. This is due to the physical structure of the magnet itself, based on so-called "magnetic domains". this is due to the physical structure of the magnet itself, based on so-called magnetic domains, i.e. microscopic areas in which the magnetic moments of the atoms are oriented in unison.
An electric field is generated by electric charges (positive or negative), which can exist separately. One can have a single positive or negative charge and study its effect on other particles. In the case of a magnet, the situation is different - there is no such thing as a 'magnetic charge' and the field arises as a result of the movement of charges (e.g. current in a Coils) or the ordering of electron spins in a material. For this reason speaking of 'positive' and 'negative' poles in the context of Magnets is physically incorrect. Such nomenclature can lead to confusion, especially in the context of electronic devices, where there is actually a distinction between plus and minus.
The principle of magnets is based on the fact that oppositely directed poles attract each other and identical poles repel each other. The north pole of one magnet attracts the south pole of another, but repels its own north pole. This phenomenon is due to the direction of the magnetic field lines, which always leave the north pole and 'flow' into the south pole. Although this resembles the principles of electric charges, the physical mechanism is different. The magnetic field is not carried by particles with magnetic charge, but by the vector orientation of electron spins.
In technology, physics and electronics using the correct terminology is crucial. A conceptual error can lead to inappropriate circuit design, misinterpretation of interactions and misunderstandings when working with devices that use magnetic fields, such as motors, Hall sensors, digital compasses or magnetic resonance imaging (MRI) devices.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.