+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Release label

Appearance of the Release Label

Content of Individual Fields on the Release Label

LP. Fields on the Label Additional Description
1. Name of the TME office where the Client placed the Order. Information about the EU importer The release label must indicate the seller (understood as the office) and the importer or distributor. The invoice is issued with the address of the office where the Client placed the order.
2. Product location in the warehouse Location 07-01-07 means: 07- shelf; 01- shelf number counted from the top; 07- place on the shelf. Used in the order picking process.
3. Area in the warehouse from which the goods were released The area in the warehouse to which the location is assigned, from which we pick the goods.
4. Quantity of ordered goods in the basic unit of measure Quantity of ordered goods in the basic unit of measure (the lowest in which the goods are sold), e.g., pieces, meters, packs [QTY].
5. Transfer order number in SAP recorded in the form of a QR CODE Record of the transfer order in the form of a QR code. Used in the order picking process.
6. TME article symbol in SAP TME symbol – the name of the article assigned by TME [PN].
7. Article description Description of the article containing the most important information about the product [MDS].
8. Manufacturer's Name Manufacturer's Name [MFR].
9. Manufacturer's article symbol Symbol assigned by the Manufacturer [MPN].
10. Client's article symbol If the Client wishes to indicate their own product symbol, it will be printed according to the provided instruction. The condition is that this data must be entered into the system beforehand. This information may be used if the Client selects the option [CPO]. Otherwise, the field on the label remains empty [CPN].
11. Client's order number The order number is automatically assigned by the SAP system during the order placement. If the Client indicates a different number, it will be printed according to the provided instruction. The condition is that this data must be entered into the system beforehand [CPO].
12. Sales order number Number automatically assigned by the system [PO].
13. Date code Information for the Client about the date code (week number and the last two digits of the year number) [DC].
14. Transfer order number in SAP Transfer order number used in warehouse processes.
15. Date and time of label printing Date of creation of the warehouse order.
16. Recipient country symbol (Client) Two-letter country abbreviation according to ISO, e.g., DE.
17. Client number TME recorded in SAP Number assigned by the system at the time of Client registration in the system.
18. Lot number from the batch Information for the Client about the Manufacturer's batch number.
19. Country of origin of the product Information for the Client about the product's origin.
20. DATA MATRIX CODE for the Client Data encoded in the form of a MATRIX code – informational only for the Client. The description of the code is in the table - DATA MATRIX CODE Specification for the Client.
21. Last three digits from the Transfer Order Number that helps in order picking.
22. QR CODE for the Client QR code with marketing data. Link to the product page and data from barcodes. The description of the code is in the table - QR CODE Specification for the Client.

DATA MATRIX CODE Specification for the Client

LP. Description Marker DATA MATRIX Print empty value Parameter I Parameter II
1. Manufacturer/Supplier Symbol 1P
2. Country of Origin 4L
3. Client's Order Number K /
4. Client Symbol/Client Identifier P
5. Quantity Q
6. Start of Code &BE [)>
7. Start of Code &C1 06
8. End of Transmission &EN #04
9. Group Separator &FS #1D
10. Record Separator &RS #1E
11. Datacode (format YYWW) 10D X
12. Expiration Date 14D X
13. Manufacturer/Supplier Symbol 1P
14. Traceability Number 1T 8044
15. Manufacturer's Name 1V
16. Revision Number 2P -
17. Shipment ID 2S X
18. RoHS 30P Y|N
19. MSL 31P NA
20. Client's Order Position 4K 001001
21. Country of Origin 4L PL
22. Client Orders K
23. Client Symbol/Client Identifier P -
24. Quantity Q
25. BIN Number Z X

QR CODE Specification for the Client

LP. Description Data
1. Quantity QTY:200
2. TME Symbol PN:APE8865U5-18-HF-3T
3. Client Symbol CPN:123456789012345678901234567890WWWWW
4. Sales Order Number/Position PO:928004/1
5. Client's Order Number CPO:12345678901234567890123456789011111
6. Manufacturer MFR:APEC
7. Manufacturer Symbol MPN:APE8865U5-18-HF-3TR
8. Country of Origin CoO:PL
9. RoHS RoHS

Prefixes analogous to those in barcode codes.

Barcode Specification

LP. Description Data
1. Quantity QTY:200
2. TME Symbol PN:APE8865U5-18-HF-3T
3. Client Symbol CPN:123456789012345678901234567890WWWWW
4. Client's Order Number CPO:12345678901234567890123456789011111
5. Manufacturer Symbol MPN:APE8865U5-18-HF-3TR
6. Country of Origin CoO:PL
7. Datacode DC: 2250

All codes in the "Code 128B" standard.