+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Call us +48 42 645 54 44
09-06-2026
The AGH University of Science and Technology has launched the Advanced X-ray Laboratory, which provides an X-ray beam with parameters similar to those of large synchrotron facilities.
Nevomo's MagRail technology is designed to enable existing rail lines to be upgraded by adding electromagnetic Actuators and, in the future, magnetic levitation without building entirely new infrastructure.
The Lubelskie Voivodeship and Lublin universities have signed a memorandum of understanding to build a quantum computer to support research, administration and the development of modern computing technologies.
GW Instek introduces the GDS-2000HD/HG series of oscilloscopes, which combines 12-bit hardware resolution, compact design and analytical functions useful in laboratory, education and field testing.
MEAN WELL describes power solutions for data centres with AC and HVDC infrastructure, highlighting products for UPS, cooling and energy management systems.
Microchip is extending the dsPIC33CK family of controllers with the Value Line for cost-sensitive motor control, tactile measurement and precision signal processing applications.
MEAN WELL introduces W8 Isolated DC-DC Converters in 2 x 1 inch Enclosures, extending the family of 8:1 input modules with powers from 10 W to 50 W.
05-06-2026
AMPHENOL connectors and interconnect solutions for battery systems, e-mobility and energy storage will be on show at The Battery Show Europe at Messe Stuttgart from 9-11 June 2026 - stand 5-D30.
Thanks to its automated warehouses and digital material preparation, HELU reduces the lead time for cable assembly as early as the warehousing stage.
Designer Chris Haynes has unveiled Flapulator, a 3D-printed mechanical display calculator powered by a Raspberry Pi Pico.
Programmer Przemyslaw 'Psyho' Debiak was the only human to beat the OpenAI model in the heuristic path of the prestigious AtCoder competition, and points out areas where human intuition still has an advantage.
A consortium led by Selvita will receive PLN 91 million in funding from the National Centre for Research and Development to develop drug discovery methods and expand its Research and Development Centre.