Inductive Components

(23 433)

Rapid changes in electrical current are an extremely dangerous phenomenon that can damage the printed circuit board of an electronic system. In order to effectively protect the system against electrical current interference, suppression chokes are used. They are an extremely important component of electrotechnical and electronic systems, which should be known by every professional.

Choke design

Despite the crucial role of chokes, their design is extremely simple. A wire of appropriate thickness, formed into a spiral shape, is the basic element. The most common solution is to wind the spiral on a core made of ferromagnetic material with strong magnetic properties (e.g. cobalt, nickel or commonly used iron). Another, less commonly used design is the air-core choke, i.e. filling the coil with air. However, the disadvantage of the latter solution is that the coiled wire needs to be properly reinforced in order to prevent unwinding, as well as lower inductance in relation to chokes with cores (with the same number of coils). The use of core makes it possible to adjust choke inductance by changing its position in relation to the surrounding coils. Depending on operating conditions and application, we distinguish between designs equipped with a closed magnetic circuit, i.e. so-called shielded chokes, and those with an open magnetic circuit.

The application and installation method require using various types of passive elements with different shapes and types of wire winding. The most commonly used types of chokes are presented below:

  • SMD chokes;
  • THT chokes;
  • DMF current-compensated chokes.

How does the choke work?

A choke prevents sudden changes in current due to the magnetic field created around a live conductor. When the intensity of the flowing electric current changes abruptly, the magnetic field also changes, which nullifies the undesirable phenomenon by reverse currents. This so-called current throttling is also called self-induction and increases proportionally to the changes in the flowing current.

The most important parameter of a choke is its inductance, which in fact speaks about its ability to generate a magnetic field producing reverse current. In order to select the right choke, its resistance and allowable operating current must also be taken into account. Another parameter describing the properties of the coil is the Q factor. It determines the ability to throttle flows with frequencies deviating from its own resonant frequency.

The unit that characterizes a coil is Henry [H]. It tells you that a change in current of 1 ampere per second induces a voltage of 1 volt.

The increase in the inductance of a coil can be influenced by:

  • Increasing the number of coils and their surface area;
  • Selecting suitable material for the core structure, with high relative permeability;
  • Shortening coil length.

The use of chokes and their function

Devices that use the discussed induction elements surround us everywhere. Therefore, it is worth knowing where we can find them. Here are some examples:

  • Drive systems equipped with inverters – filtering of interference resulting from motor speed control with the use of a frequency converter;
  • All types of loudspeakers – a choke acting as an anti-interference device significantly improves the acoustic qualities of the generated sound;
  • Capacitive batteries – chokes as protective elements for capacitors

Standard coil versus choke – basic differences

Chokes are included in the group of inductors. For this reason, the terms choke and coil have been used interchangeably. At this point, however, it should be noted that not every coil is a choke. These elements are distinguished primarily by the way they are used in the electrical system. A coil is a choke only if its task is to prevent an undesirable change in current intensity. A different application of a coil (e.g. in electromagnets as a source of attracting metal elements) means that this element cannot be classified as a choke.

Power loss in the coils

The main reason for power loss in the coils is the resistance of the winding wire. Because of this, the coil heats up and the magnetic properties of the core change. It is especially dangerous in the case of high currents, as it may damage electronic components and, consequently, lead to a failure of the entire system.

Another important detail is precise workmanship. Careful winding of the wire or appropriate gaps between subsequent coils have a fundamental impact on the quality of the generated magnetic field. Its dispersion leads to a measurable loss of the choke's efficiency. It is worth mentioning that a poorly made coil may generate additional heat, which increases the risk of overheating the circuit as described above.

The quality of the core itself also has a huge impact on the power loss. Uneven implementation of the core can lead to generating large deviations of the actual parameters in relation to the nominal values.

Chokes – how to select the right one?

To sum up, chokes are used in devices that require suppression of sudden changes in currents, signal filtering or protection against overloads caused by harmonic currents. Due to the very wide application and parameters specific to each coil, special attention should be paid to selecting the appropriate circuit element. Only a choke with an appropriate inductance and designed to work with a specific current intensity can meet the requirements. Therefore, choosing such important elements of an electronic circuit should not be guided solely by economic aspects. It is worth relying on products from proven manufacturers that will meet the quality requirements and allow for long-term, failure-free operation.

Products: 23 433

Warehouse:

TME
External
All
Page 1
LBMF1608T100K | Inductor: wire; SMD; 0603; 10uH; 80mA; R: 360mΩ; ±10%; LB; 1.6x0.8mm
Inductor: wire; SMD; 0603; 10uH; 80mA; R: 360mΩ; ±10%; LB; 1.6x0.8mm
Manufacturer part number: LBMF1608T100K
Manufacturer: TAIYO YUDEN
Net price for quantities from 1 pcs - 0.22 USDGross price for quantities from 1 pcs - 0.22 USD
Net price for quantities from 10 pcs - 0.12 USDGross price for quantities from 10 pcs - 0.12 USD
Net price for quantities from 50 pcs - 0.08 USDGross price for quantities from 50 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.06 USDGross price for quantities from 100 pcs - 0.06 USD
Net price for quantities from 250 pcs - 0.05 USDGross price for quantities from 250 pcs - 0.05 USD
Net price for quantities from 500 pcs - 0.05 USDGross price for quantities from 500 pcs - 0.05 USD
Net price for quantities from 1000 pcs - 0.04 USDGross price for quantities from 1000 pcs - 0.04 USD
Net price for quantities from 3000 pcs - 0.03 USDGross price for quantities from 3000 pcs - 0.03 USD
Net price for quantities from 6000 pcs - 0.03 USDGross price for quantities from 6000 pcs - 0.03 USD
Net price for quantities from 9000 pcs - 0.03 USDGross price for quantities from 9000 pcs - 0.03 USD
80143 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
H1102NL | Transformer: LAN; SMD; -1.1dB; Network: Ethernet 10/100Mbps
Transformer: LAN; SMD; -1.1dB; Network: Ethernet 10/100Mbps
Manufacturer part number: H1102NL
Manufacturer: PULSE
Net price for quantities from 1 pcs - 1.93 USDGross price for quantities from 1 pcs - 1.93 USD
Net price for quantities from 10 pcs - 1.73 USDGross price for quantities from 10 pcs - 1.73 USD
Net price for quantities from 25 pcs - 1.50 USDGross price for quantities from 25 pcs - 1.50 USD
Net price for quantities from 40 pcs - 1.31 USDGross price for quantities from 40 pcs - 1.31 USD
Net price for quantities from 80 pcs - 1.01 USDGross price for quantities from 80 pcs - 1.01 USD
Net price for quantities from 120 pcs - 0.86 USDGross price for quantities from 120 pcs - 0.86 USD
Net price for quantities from 200 pcs - 0.71 USDGross price for quantities from 200 pcs - 0.71 USD
Net price for quantities from 240 pcs - 0.69 USDGross price for quantities from 240 pcs - 0.69 USD
Net price for quantities from 280 pcs - 0.66 USDGross price for quantities from 280 pcs - 0.66 USD
Net price for quantities from 520 pcs - 0.65 USDGross price for quantities from 520 pcs - 0.65 USD
4278 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
NRS4018T220MDGJ | Inductor: wire; SMD; 22uH; Ioper: 720mA; R: 290mΩ; ±20%; NRS; 4x4mm
Inductor: wire; SMD; 22uH; Ioper: 720mA; R: 290mΩ; ±20%; NRS; 4x4mm
Manufacturer part number: NRS4018T220MDGJ
Manufacturer: TAIYO YUDEN
Net price for quantities from 1 pcs - 0.33 USDGross price for quantities from 1 pcs - 0.33 USD
Net price for quantities from 10 pcs - 0.15 USDGross price for quantities from 10 pcs - 0.15 USD
Net price for quantities from 50 pcs - 0.08 USDGross price for quantities from 50 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.07 USDGross price for quantities from 100 pcs - 0.07 USD
Net price for quantities from 250 pcs - 0.07 USDGross price for quantities from 250 pcs - 0.07 USD
Net price for quantities from 500 pcs - 0.06 USDGross price for quantities from 500 pcs - 0.06 USD
Net price for quantities from 1000 pcs - 0.06 USDGross price for quantities from 1000 pcs - 0.06 USD
Net price for quantities from 3500 pcs - 0.06 USDGross price for quantities from 3500 pcs - 0.06 USD
Net price for quantities from 7000 pcs - 0.06 USDGross price for quantities from 7000 pcs - 0.06 USD
52842 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LQG15HN8N2J02D | Inductor: air coil; SMD; 0402; 8.2nH; 500mA; R: 0.25Ω; ±5%; LQG; 180mm
Inductor: air coil; SMD; 0402; 8.2nH; 500mA; R: 0.25Ω; ±5%; LQG; 180mm
Manufacturer part number: LQG15HN8N2J02D
Manufacturer: MURATA
Net price for quantities from 1 pcs - 0.09 USDGross price for quantities from 1 pcs - 0.09 USD
Net price for quantities from 10 pcs - 0.04 USDGross price for quantities from 10 pcs - 0.04 USD
Net price for quantities from 100 pcs - 0.03 USDGross price for quantities from 100 pcs - 0.03 USD
Net price for quantities from 1000 pcs - 0.02 USDGross price for quantities from 1000 pcs - 0.02 USD
Net price for quantities from 5000 pcs - 0.02 USDGross price for quantities from 5000 pcs - 0.02 USD
Net price for quantities from 10000 pcs - 0.01 USDGross price for quantities from 10000 pcs - 0.01 USD
Net price for quantities from 20000 pcs - 0.01 USDGross price for quantities from 20000 pcs - 0.01 USD
Net price for quantities from 30000 pcs - 0.01 USDGross price for quantities from 30000 pcs - 0.01 USD
Net price for quantities from 40000 pcs - 0.01 USDGross price for quantities from 40000 pcs - 0.01 USD
60694 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
B82790S0513N201 | Inductor: common mode; SMD; 51uH; 500mA; R: 140mΩ; ±30%; 7.1x6x5.2mm
Inductor: common mode; SMD; 51uH; 500mA; R: 140mΩ; ±30%; 7.1x6x5.2mm
Manufacturer part number: B82790S0513N201
Manufacturer: TDK
Net price for quantities from 1 pcs - 1.77 USDGross price for quantities from 1 pcs - 1.77 USD
Net price for quantities from 10 pcs - 1.66 USDGross price for quantities from 10 pcs - 1.66 USD
Net price for quantities from 25 pcs - 1.52 USDGross price for quantities from 25 pcs - 1.52 USD
Net price for quantities from 50 pcs - 1.37 USDGross price for quantities from 50 pcs - 1.37 USD
Net price for quantities from 100 pcs - 1.20 USDGross price for quantities from 100 pcs - 1.20 USD
Net price for quantities from 250 pcs - 1.00 USDGross price for quantities from 250 pcs - 1.00 USD
Net price for quantities from 500 pcs - 0.88 USDGross price for quantities from 500 pcs - 0.88 USD
Net price for quantities from 1000 pcs - 0.80 USDGross price for quantities from 1000 pcs - 0.80 USD
Net price for quantities from 1500 pcs - 0.77 USDGross price for quantities from 1500 pcs - 0.77 USD
Net price for quantities from 3000 pcs - 0.72 USDGross price for quantities from 3000 pcs - 0.72 USD
5530 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LM-NP-1001-B1L | Transformer: audio; Z: 600Ω; Rpri.wind: 66Ω; Rsec.winding: 66Ω
Transformer: audio; Z: 600Ω; Rpri.wind: 66Ω; Rsec.winding: 66Ω
Manufacturer part number: LM-NP-1001-B1L
Manufacturer: BOURNS
Net price for quantities from 1 pcs - 2.32 USDGross price for quantities from 1 pcs - 2.32 USD
Net price for quantities from 10 pcs - 2.17 USDGross price for quantities from 10 pcs - 2.17 USD
Net price for quantities from 28 pcs - 1.91 USDGross price for quantities from 28 pcs - 1.91 USD
Net price for quantities from 112 pcs - 1.81 USDGross price for quantities from 112 pcs - 1.81 USD
407 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
IHLP2525CZER4R7M01 | Inductor: wire; SMD; 4.7uH; 5.5A; R: 37mΩ; ±20%; IHLP; 6.47x6.47x3mm
Inductor: wire; SMD; 4.7uH; 5.5A; R: 37mΩ; ±20%; IHLP; 6.47x6.47x3mm
Manufacturer part number: IHLP2525CZER4R7M01
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.55 USDGross price for quantities from 1 pcs - 0.55 USD
Net price for quantities from 1000 pcs - 0.37 USDGross price for quantities from 1000 pcs - 0.37 USD
Net price for quantities from 2000 pcs - 0.34 USDGross price for quantities from 2000 pcs - 0.34 USD
Net price for quantities from 10000 pcs - 0.32 USDGross price for quantities from 10000 pcs - 0.32 USD
6883 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LQG15HN5N6S02D | Inductor: air coil; SMD; 0402; 5.6nH; 600mA; R: 0.18Ω; LQG; 180mm
Inductor: air coil; SMD; 0402; 5.6nH; 600mA; R: 0.18Ω; LQG; 180mm
Manufacturer part number: LQG15HN5N6S02D
Manufacturer: MURATA
Net price for quantities from 1 pcs - 0.09 USDGross price for quantities from 1 pcs - 0.09 USD
Net price for quantities from 10 pcs - 0.04 USDGross price for quantities from 10 pcs - 0.04 USD
Net price for quantities from 100 pcs - 0.03 USDGross price for quantities from 100 pcs - 0.03 USD
Net price for quantities from 1000 pcs - 0.02 USDGross price for quantities from 1000 pcs - 0.02 USD
Net price for quantities from 5000 pcs - 0.02 USDGross price for quantities from 5000 pcs - 0.02 USD
Net price for quantities from 10000 pcs - 0.02 USDGross price for quantities from 10000 pcs - 0.02 USD
Net price for quantities from 20000 pcs - 0.01 USDGross price for quantities from 20000 pcs - 0.01 USD
Net price for quantities from 30000 pcs - 0.01 USDGross price for quantities from 30000 pcs - 0.01 USD
Net price for quantities from 40000 pcs - 0.01 USDGross price for quantities from 40000 pcs - 0.01 USD
Net price for quantities from 100000 pcs - 0.01 USDGross price for quantities from 100000 pcs - 0.01 USD
53273 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LQM18DN100M70L | Inductor: multilayer; SMD; 0603; 10uH; 300mA; R: 1.365Ω; ±20%; LQM
Inductor: multilayer; SMD; 0603; 10uH; 300mA; R: 1.365Ω; ±20%; LQM
Manufacturer part number: LQM18DN100M70L
Manufacturer: MURATA
Net price for quantities from 1 pcs - 0.10 USDGross price for quantities from 1 pcs - 0.10 USD
Net price for quantities from 10 pcs - 0.08 USDGross price for quantities from 10 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.07 USDGross price for quantities from 100 pcs - 0.07 USD
Net price for quantities from 500 pcs - 0.06 USDGross price for quantities from 500 pcs - 0.06 USD
Net price for quantities from 1000 pcs - 0.05 USDGross price for quantities from 1000 pcs - 0.05 USD
Net price for quantities from 2500 pcs - 0.05 USDGross price for quantities from 2500 pcs - 0.05 USD
Net price for quantities from 4000 pcs - 0.05 USDGross price for quantities from 4000 pcs - 0.05 USD
Net price for quantities from 8000 pcs - 0.04 USDGross price for quantities from 8000 pcs - 0.04 USD
Net price for quantities from 12000 pcs - 0.04 USDGross price for quantities from 12000 pcs - 0.04 USD
730 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
NRS4018T100MDGJ | Inductor: wire; SMD; 10uH; Ioper: 1.2A; R: 150mΩ; ±20%; NRS; 4x4mm
Inductor: wire; SMD; 10uH; Ioper: 1.2A; R: 150mΩ; ±20%; NRS; 4x4mm
Manufacturer part number: NRS4018T100MDGJ
Manufacturer: TAIYO YUDEN
Net price for quantities from 1 pcs - 0.33 USDGross price for quantities from 1 pcs - 0.33 USD
Net price for quantities from 10 pcs - 0.17 USDGross price for quantities from 10 pcs - 0.17 USD
Net price for quantities from 50 pcs - 0.09 USDGross price for quantities from 50 pcs - 0.09 USD
Net price for quantities from 100 pcs - 0.07 USDGross price for quantities from 100 pcs - 0.07 USD
Net price for quantities from 500 pcs - 0.07 USDGross price for quantities from 500 pcs - 0.07 USD
Net price for quantities from 1000 pcs - 0.06 USDGross price for quantities from 1000 pcs - 0.06 USD
Net price for quantities from 3500 pcs - 0.06 USDGross price for quantities from 3500 pcs - 0.06 USD
Net price for quantities from 7000 pcs - 0.06 USDGross price for quantities from 7000 pcs - 0.06 USD
Net price for quantities from 10500 pcs - 0.06 USDGross price for quantities from 10500 pcs - 0.06 USD
34981 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
IHLP2525CZER100M01 | Inductor: wire; SMD; 10uH; 7A; R: 102mΩ; ±20%; IHLP; 6.47x6.47x3mm
Inductor: wire; SMD; 10uH; 7A; R: 102mΩ; ±20%; IHLP; 6.47x6.47x3mm
Manufacturer part number: IHLP2525CZER100M01
Manufacturer: VISHAY
Net price for quantities from 1 pcs - 0.67 USDGross price for quantities from 1 pcs - 0.67 USD
Net price for quantities from 50 pcs - 0.62 USDGross price for quantities from 50 pcs - 0.62 USD
Net price for quantities from 100 pcs - 0.59 USDGross price for quantities from 100 pcs - 0.59 USD
Net price for quantities from 250 pcs - 0.54 USDGross price for quantities from 250 pcs - 0.54 USD
Net price for quantities from 500 pcs - 0.48 USDGross price for quantities from 500 pcs - 0.48 USD
Net price for quantities from 1000 pcs - 0.42 USDGross price for quantities from 1000 pcs - 0.42 USD
Net price for quantities from 2000 pcs - 0.36 USDGross price for quantities from 2000 pcs - 0.36 USD
Net price for quantities from 4000 pcs - 0.34 USDGross price for quantities from 4000 pcs - 0.34 USD
10777 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
MLZ2012M100WT000 | Inductor: ferrite; SMD; 0805; 10uH; 350mA; R: 470mΩ; ±20%; -55÷125°C
Inductor: ferrite; SMD; 0805; 10uH; 350mA; R: 470mΩ; ±20%; -55÷125°C
Manufacturer part number: MLZ2012M100WT000
Manufacturer: TDK
Net price for quantities from 1 pcs - 0.06 USDGross price for quantities from 1 pcs - 0.06 USD
Net price for quantities from 10 pcs - 0.05 USDGross price for quantities from 10 pcs - 0.05 USD
Net price for quantities from 30 pcs - 0.04 USDGross price for quantities from 30 pcs - 0.04 USD
Net price for quantities from 50 pcs - 0.04 USDGross price for quantities from 50 pcs - 0.04 USD
Net price for quantities from 100 pcs - 0.04 USDGross price for quantities from 100 pcs - 0.04 USD
Net price for quantities from 200 pcs - 0.03 USDGross price for quantities from 200 pcs - 0.03 USD
Net price for quantities from 500 pcs - 0.03 USDGross price for quantities from 500 pcs - 0.03 USD
Net price for quantities from 1000 pcs - 0.03 USDGross price for quantities from 1000 pcs - 0.03 USD
7943 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
DLA10-N | Inductor: axial; THT; 10uH; 370mA; R: 720mΩ; Ø3x8mm; Ø: 3mm; H: 8mm
Inductor: axial; THT; 10uH; 370mA; R: 720mΩ; Ø3x8mm; Ø: 3mm; H: 8mm
Manufacturer part number: DLA10-N
Manufacturer: FERROCORE
Net price for quantities from 10 pcs - 0.13 USDGross price for quantities from 10 pcs - 0.13 USD
Net price for quantities from 50 pcs - 0.11 USDGross price for quantities from 50 pcs - 0.11 USD
Net price for quantities from 100 pcs - 0.05 USDGross price for quantities from 100 pcs - 0.05 USD
Net price for quantities from 500 pcs - 0.04 USDGross price for quantities from 500 pcs - 0.04 USD
Net price for quantities from 2000 pcs - 0.04 USDGross price for quantities from 2000 pcs - 0.04 USD
8810 in TME stock
No. of pieces (Multiple of: 10)
Minimum order quantity: 10.
Multiple of: 10.
LQG15HN9N1J02D | Inductor: air coil; SMD; 0402; 9.1nH; 500mA; R: 0.27Ω; ±5%; LQG; 180mm
Inductor: air coil; SMD; 0402; 9.1nH; 500mA; R: 0.27Ω; ±5%; LQG; 180mm
Manufacturer part number: LQG15HN9N1J02D
Manufacturer: MURATA
Net price for quantities from 1 pcs - 0.09 USDGross price for quantities from 1 pcs - 0.09 USD
Net price for quantities from 10 pcs - 0.04 USDGross price for quantities from 10 pcs - 0.04 USD
Net price for quantities from 100 pcs - 0.03 USDGross price for quantities from 100 pcs - 0.03 USD
Net price for quantities from 250 pcs - 0.03 USDGross price for quantities from 250 pcs - 0.03 USD
Net price for quantities from 1000 pcs - 0.02 USDGross price for quantities from 1000 pcs - 0.02 USD
Net price for quantities from 5000 pcs - 0.02 USDGross price for quantities from 5000 pcs - 0.02 USD
Net price for quantities from 10000 pcs - 0.01 USDGross price for quantities from 10000 pcs - 0.01 USD
Net price for quantities from 20000 pcs - 0.01 USDGross price for quantities from 20000 pcs - 0.01 USD
Net price for quantities from 30000 pcs - 0.01 USDGross price for quantities from 30000 pcs - 0.01 USD
Net price for quantities from 50000 pcs - 0.01 USDGross price for quantities from 50000 pcs - 0.01 USD
43229 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
RLB0914-101KL | Inductor: wire; THT; 100uH; 1A; R: 0.28Ω; ±10%; Ø8.7x12mm; vertical
Inductor: wire; THT; 100uH; 1A; R: 0.28Ω; ±10%; Ø8.7x12mm; vertical
Manufacturer part number: RLB0914-101KL
Manufacturer: BOURNS
Net price for quantities from 1 pcs - 0.35 USDGross price for quantities from 1 pcs - 0.35 USD
Net price for quantities from 7 pcs - 0.31 USDGross price for quantities from 7 pcs - 0.31 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 25 pcs - 0.27 USDGross price for quantities from 25 pcs - 0.27 USD
Net price for quantities from 50 pcs - 0.25 USDGross price for quantities from 50 pcs - 0.25 USD
Net price for quantities from 100 pcs - 0.23 USDGross price for quantities from 100 pcs - 0.23 USD
Net price for quantities from 200 pcs - 0.21 USDGross price for quantities from 200 pcs - 0.21 USD
Net price for quantities from 600 pcs - 0.19 USDGross price for quantities from 600 pcs - 0.19 USD
Net price for quantities from 1000 pcs - 0.18 USDGross price for quantities from 1000 pcs - 0.18 USD
Net price for quantities from 2600 pcs - 0.17 USDGross price for quantities from 2600 pcs - 0.17 USD
3382 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
NRS5040T4R7NMGK | Inductor: wire; SMD; 4.7uH; Ioper: 3.1A; R: 29mΩ; ±20%; NRS; 4.9x4.9mm
Inductor: wire; SMD; 4.7uH; Ioper: 3.1A; R: 29mΩ; ±20%; NRS; 4.9x4.9mm
Manufacturer part number: NRS5040T4R7NMGK
Manufacturer: TAIYO YUDEN
Net price for quantities from 1 pcs - 0.25 USDGross price for quantities from 1 pcs - 0.25 USD
Net price for quantities from 10 pcs - 0.17 USDGross price for quantities from 10 pcs - 0.17 USD
Net price for quantities from 25 pcs - 0.12 USDGross price for quantities from 25 pcs - 0.12 USD
Net price for quantities from 100 pcs - 0.11 USDGross price for quantities from 100 pcs - 0.11 USD
Net price for quantities from 1500 pcs - 0.10 USDGross price for quantities from 1500 pcs - 0.10 USD
Net price for quantities from 4500 pcs - 0.09 USDGross price for quantities from 4500 pcs - 0.09 USD
Net price for quantities from 9000 pcs - 0.09 USDGross price for quantities from 9000 pcs - 0.09 USD
21111 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
SM-LP-5001E | Transformer: LAN; 600Ω; Trans: 1: 1
Transformer: LAN; 600Ω; Trans: 1: 1
Manufacturer part number: SM-LP-5001E
Manufacturer: BOURNS
Net price for quantities from 1 pcs - 2.50 USDGross price for quantities from 1 pcs - 2.50 USD
Net price for quantities from 10 pcs - 2.00 USDGross price for quantities from 10 pcs - 2.00 USD
Net price for quantities from 25 pcs - 1.87 USDGross price for quantities from 25 pcs - 1.87 USD
Net price for quantities from 50 pcs - 1.80 USDGross price for quantities from 50 pcs - 1.80 USD
Net price for quantities from 100 pcs - 1.75 USDGross price for quantities from 100 pcs - 1.75 USD
Net price for quantities from 200 pcs - 1.73 USDGross price for quantities from 200 pcs - 1.73 USD
Net price for quantities from 400 pcs - 1.68 USDGross price for quantities from 400 pcs - 1.68 USD
Net price for quantities from 800 pcs - 1.66 USDGross price for quantities from 800 pcs - 1.66 USD
Net price for quantities from 1200 pcs - 1.64 USDGross price for quantities from 1200 pcs - 1.64 USD
Net price for quantities from 2000 pcs - 1.63 USDGross price for quantities from 2000 pcs - 1.63 USD
5467 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
DE1207-100 | Inductor: wire; SMD; 100uH; 2.1A; R: 151mΩ; ±20%; 12x12x8mm; -40÷85°C
Inductor: wire; SMD; 100uH; 2.1A; R: 151mΩ; ±20%; 12x12x8mm; -40÷85°C
Manufacturer part number: DE1207-100
Manufacturer: FERROCORE
Net price for quantities from 1 pcs - 0.37 USDGross price for quantities from 1 pcs - 0.37 USD
Net price for quantities from 25 pcs - 0.30 USDGross price for quantities from 25 pcs - 0.30 USD
Net price for quantities from 100 pcs - 0.26 USDGross price for quantities from 100 pcs - 0.26 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 2000 pcs - 0.22 USDGross price for quantities from 2000 pcs - 0.22 USD
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
4997 | Inductor: air coil; 0.22mH; 0.54Ω; Ø: 25mm; H: 12mm; Øcore: 0.6mm
Inductor: air coil; 0.22mH; 0.54Ω; Ø: 25mm; H: 12mm; Øcore: 0.6mm
Manufacturer part number: 4997
Manufacturer: VISATON
Net price for quantities from 1 pcs - 4.13 USDGross price for quantities from 1 pcs - 4.13 USD
Net price for quantities from 2 pcs - 3.71 USDGross price for quantities from 2 pcs - 3.71 USD
Net price for quantities from 5 pcs - 3.30 USDGross price for quantities from 5 pcs - 3.30 USD
Net price for quantities from 10 pcs - 3.09 USDGross price for quantities from 10 pcs - 3.09 USD
42 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LQW15AN4N7B00D | Inductor: wire; SMD; 0402; 4.7nH; 750mA; R: 0.07Ω; LQW; 180mm; ±0,1nH
Inductor: wire; SMD; 0402; 4.7nH; 750mA; R: 0.07Ω; LQW; 180mm; ±0,1nH
Manufacturer part number: LQW15AN4N7B00D
Manufacturer: MURATA
Net price for quantities from 1 pcs - 0.11 USDGross price for quantities from 1 pcs - 0.11 USD
Net price for quantities from 10 pcs - 0.08 USDGross price for quantities from 10 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.07 USDGross price for quantities from 100 pcs - 0.07 USD
Net price for quantities from 1000 pcs - 0.06 USDGross price for quantities from 1000 pcs - 0.06 USD
Net price for quantities from 2500 pcs - 0.05 USDGross price for quantities from 2500 pcs - 0.05 USD
Net price for quantities from 5000 pcs - 0.05 USDGross price for quantities from 5000 pcs - 0.05 USD
Net price for quantities from 10000 pcs - 0.04 USDGross price for quantities from 10000 pcs - 0.04 USD
Net price for quantities from 20000 pcs - 0.04 USDGross price for quantities from 20000 pcs - 0.04 USD
4794 in TME stock