+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

SMD LEDs

(7 595)

SMD LEDs (i.e. diodes intended for surface mounting) are among the most popular optical electronic components. They are used in backlighting and indicator components, for making large and complex arrays in LED light bulbs, tubes, strips, and more. The great advantage of SMD LEDs is their small size, thanks to which they can be used in mobile devices (flash lamps and torches in mobile phones are good examples here). Moreover, SMD diodes are also parts of LCDs, where they backlight the screen.

The SMD LEDs often have similar, if not identical, parameters to the THT components. These features also make them very popular. Nevertheless, small optoelectronic components can get overheated – especially in applications that involve illuminating objects. Therefore, as a designer and installer you should always take into consideration proper cooling of LEDs (ensure an adequate airflow or adhesion to the surface of a heat dissipation element, such as a copper heatsink or aluminium mounting strip).

In DIY projects or prototype development, using SMD LEDs may be more complicated. Luckily, you can choose to use THT components in the circuit in the designing phase, and then replace them with smaller equivalents in the final version of the device.

What are typical applications of colour SMD LEDs?

The SMD LED category has three product groups: white and coloured components and light pipes (light guides). Colour SMD LEDs are typical indicator components. SMD LEDs are often chosen for two main reasons: to minimise the PCB footprint occupied by optoelectronic components and to avoid drilling holes in the board. If the entire circuit was made using the SMD technology, a THT component would be a suboptimal choice. However, compact light sources have their shortcomings, too. Above all, they are positioned in parallel to the PCB surface and have a relatively small face area. To overcome these, one can use special light pipes for LEDs. They are transparent optical components which transfer light to the desired spot. The light pipes are designed for mounting on PCBs, and their light output is perpendicular to the input site. Due to this, LEDs may be mounted on the motherboard of the device, and the emitted light is visible to the user (e.g. at the front panel).

Colour LEDs category also comprises multicolour components, including RGBs. They emit mixed red, green and blue light, which (depending on relative intensity) may produce any light colour. To control such components, PWM signals are used. In order to achieve a uniformly coloured light, one may use light-diffusing components. There is also a special variant of multicolour components, namely RGBW devices, which can also emit white light.

Advantages of SMD LEDs emitting white light

Unlike the colour LEDs, white SMD LEDs are usually used as light sources. Of course, they may also be used as indicator lights – for example, in electronic and household equipment. Moreover, TME also offers LEDs with relatively high power (up to 1 W), intended for use in illumination systems, light sources and special effect installations. Due to their excellent energy efficiency, such components are often applied in battery-powered devices: low-power white SMD LEDs are used, for example, to illuminate keyboards in laptops, while brighter components are installed in torches or power tools. It is worth emphasising here that LEDs intended for interior lighting i.e. power LEDs, are listed as a separate TME catalogue category.

White light is characterised by one crucial parameter, namely its colour temperature. Even a tiny difference in the wavelength of the emitted light translates into the human perception of light as “warm” or “cold”. The value is expressed in K (kelvins). White light in the colour temperature of 5000–8000 K is similar to daylight. Below 5000 K, light becomes yellowish (1000 K is the colour temperature of a fire flame), and above 8000 K, light becomes blueish.

When power light sources are used, the produced heat must be dissipated to avoid overheating the system. A single SMD LED (even a very small one) may produce light with the intensity of over 135 lm. It is brighter than a traditional 10 W lightbulb. An LED consumes considerably less power than a standard lightbulb (e.g. 1 W), but due to its tiny dimensions, the component may heat up considerably, and its temperature may be harmful to the human body and deform plastic parts.

Crucial parameters and markings of SMD LEDs

The selection process for SMD LEDs is identical to that for components enclosed in other types of casings.. The only significant difference is the coding scheme, which is typical for other SMDs. According to the scheme, a four-digit symbol describes the size: the two first digits denote the length, and the two last ones – the width of the component. The unit is 0.01 in. An alternative, metric system for SMD markings is analogous to the former, but the unit is 0.1 mm. The majority of optoelectronic components are manufactured in standard sizes. There are, however, some exceptions to this rule.

The remaining parameters of the LEDs are consistent, regardless of the scheme. The operating voltage and current describe the LEDs electrical characteristics and also facilitate the selection of a current-limiting resistor. Power describes the energy consumed by the component. Viewing angle describes the lens used: depending on the application, the designer may decide to use an LED with a narrow viewing angle (10–20°) or a very wide one (up to 180°) so that the light can be seen along a line that is almost parallel to the PCB surface. LED colour may be defined in two ways: in general (by the name, “red”, “green”, etc.) or by referring to the specific wavelength of the emitted light. For white LEDs, an important parameter is luminosity, denoted in lumens (lm) and sometimes millilumens (especially in the case of indicator components).

Products: 7 595

Warehouse:

TME
External
All
Page 1
LTST-C190KGKT | LED; green; SMD; 0603; 18÷71mcd; 1.9÷2.4VDC; 1.6x0.8x0.8mm; 130°
LED; green; SMD; 0603; 18÷71mcd; 1.9÷2.4VDC; 1.6x0.8x0.8mm; 130°
Manufacturer part number: LTST-C190KGKT
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.10 USDGross price for quantities from 1 pcs - 0.10 USD
Net price for quantities from 10 pcs - 0.08 USDGross price for quantities from 10 pcs - 0.08 USD
Net price for quantities from 50 pcs - 0.05 USDGross price for quantities from 50 pcs - 0.05 USD
Net price for quantities from 100 pcs - 0.04 USDGross price for quantities from 100 pcs - 0.04 USD
Net price for quantities from 500 pcs - 0.03 USDGross price for quantities from 500 pcs - 0.03 USD
Net price for quantities from 1000 pcs - 0.02 USDGross price for quantities from 1000 pcs - 0.02 USD
Net price for quantities from 2000 pcs - 0.02 USDGross price for quantities from 2000 pcs - 0.02 USD
Net price for quantities from 4000 pcs - 0.02 USDGross price for quantities from 4000 pcs - 0.02 USD
Net price for quantities from 8000 pcs - 0.02 USDGross price for quantities from 8000 pcs - 0.02 USD
26140 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
OF-SMD2012G | LED; green; SMD; 0805; 50÷100mcd; 1.8÷2VDC; 2x1.25x0.68mm; 120°
LED; green; SMD; 0805; 50÷100mcd; 1.8÷2VDC; 2x1.25x0.68mm; 120°
Manufacturer part number: OF-SMD2012G
Manufacturer: OPTOFLASH
Net price for quantities from 10 pcs - 0.07 USDGross price for quantities from 10 pcs - 0.07 USD
Net price for quantities from 50 pcs - 0.06 USDGross price for quantities from 50 pcs - 0.06 USD
Net price for quantities from 250 pcs - 0.05 USDGross price for quantities from 250 pcs - 0.05 USD
Net price for quantities from 1000 pcs - 0.04 USDGross price for quantities from 1000 pcs - 0.04 USD
Net price for quantities from 3000 pcs - 0.04 USDGross price for quantities from 3000 pcs - 0.04 USD
Net price for quantities from 12000 pcs - 0.03 USDGross price for quantities from 12000 pcs - 0.03 USD
Net price for quantities from 24000 pcs - 0.02 USDGross price for quantities from 24000 pcs - 0.02 USD
Net price for quantities from 72000 pcs - 0.02 USDGross price for quantities from 72000 pcs - 0.02 USD
136603 in TME stock
No. of pieces (Multiple of: 10)
Minimum order quantity: 10.
Multiple of: 10.
LTST-C191KGKT | LED; green; SMD; 0603; 18÷71mcd; 1.9÷2.4VDC; 1.6x0.8x0.55mm; 130°
LED; green; SMD; 0603; 18÷71mcd; 1.9÷2.4VDC; 1.6x0.8x0.55mm; 130°
Manufacturer part number: LTST-C191KGKT
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.06 USDGross price for quantities from 1 pcs - 0.06 USD
Net price for quantities from 50 pcs - 0.06 USDGross price for quantities from 50 pcs - 0.06 USD
Net price for quantities from 100 pcs - 0.05 USDGross price for quantities from 100 pcs - 0.05 USD
Net price for quantities from 500 pcs - 0.04 USDGross price for quantities from 500 pcs - 0.04 USD
Net price for quantities from 1000 pcs - 0.03 USDGross price for quantities from 1000 pcs - 0.03 USD
Net price for quantities from 2000 pcs - 0.02 USDGross price for quantities from 2000 pcs - 0.02 USD
Net price for quantities from 2500 pcs - 0.02 USDGross price for quantities from 2500 pcs - 0.02 USD
Net price for quantities from 5000 pcs - 0.02 USDGross price for quantities from 5000 pcs - 0.02 USD
Net price for quantities from 10000 pcs - 0.02 USDGross price for quantities from 10000 pcs - 0.02 USD
Net price for quantities from 25000 pcs - 0.02 USDGross price for quantities from 25000 pcs - 0.02 USD
40220 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LY G6SP-CBEB-36-3B5A | LED; yellow; SMD; 3550÷11200mcd; 2.05÷2.65VDC; 3.5x3.2x2.1mm; 120°
LED; yellow; SMD; 3550÷11200mcd; 2.05÷2.65VDC; 3.5x3.2x2.1mm; 120°
Manufacturer part number: LY G6SP-CBEB-36-3B5A
Manufacturer: ams OSRAM
Net price for quantities from 2 pcs - 0.49 USDGross price for quantities from 2 pcs - 0.49 USD
Net price for quantities from 10 pcs - 0.43 USDGross price for quantities from 10 pcs - 0.43 USD
Net price for quantities from 100 pcs - 0.31 USDGross price for quantities from 100 pcs - 0.31 USD
Net price for quantities from 500 pcs - 0.26 USDGross price for quantities from 500 pcs - 0.26 USD
Net price for quantities from 1000 pcs - 0.23 USDGross price for quantities from 1000 pcs - 0.23 USD
Net price for quantities from 2000 pcs - 0.22 USDGross price for quantities from 2000 pcs - 0.22 USD
Net price for quantities from 5000 pcs - 0.21 USDGross price for quantities from 5000 pcs - 0.21 USD
Net price for quantities from 10000 pcs - 0.18 USDGross price for quantities from 10000 pcs - 0.18 USD
Net price for quantities from 20000 pcs - 0.18 USDGross price for quantities from 20000 pcs - 0.18 USD
74967 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 2.
Multiple of: 1.
OF-SMD2012R | LED; red; SMD; 0805; 90÷120mcd; 1.6÷1.9VDC; 2x1.25x0.68mm; 120°
LED; red; SMD; 0805; 90÷120mcd; 1.6÷1.9VDC; 2x1.25x0.68mm; 120°
Manufacturer part number: OF-SMD2012R
Manufacturer: OPTOFLASH
Net price for quantities from 10 pcs - 0.06 USDGross price for quantities from 10 pcs - 0.06 USD
Net price for quantities from 50 pcs - 0.05 USDGross price for quantities from 50 pcs - 0.05 USD
Net price for quantities from 250 pcs - 0.04 USDGross price for quantities from 250 pcs - 0.04 USD
Net price for quantities from 1000 pcs - 0.03 USDGross price for quantities from 1000 pcs - 0.03 USD
Net price for quantities from 2000 pcs - 0.03 USDGross price for quantities from 2000 pcs - 0.03 USD
Net price for quantities from 4000 pcs - 0.03 USDGross price for quantities from 4000 pcs - 0.03 USD
Net price for quantities from 8000 pcs - 0.03 USDGross price for quantities from 8000 pcs - 0.03 USD
Net price for quantities from 12000 pcs - 0.03 USDGross price for quantities from 12000 pcs - 0.03 USD
Net price for quantities from 24000 pcs - 0.02 USDGross price for quantities from 24000 pcs - 0.02 USD
100332 in TME stock
No. of pieces (Multiple of: 10)
Minimum order quantity: 10.
Multiple of: 10.
OF-SMD3216R | LED; red; SMD; 1206; 290÷500mcd; 1.8÷2.4VDC; 3.2x1.6x0.68mm; 120°
LED; red; SMD; 1206; 290÷500mcd; 1.8÷2.4VDC; 3.2x1.6x0.68mm; 120°
Manufacturer part number: OF-SMD3216R
Manufacturer: OPTOFLASH
Net price for quantities from 5 pcs - 0.11 USDGross price for quantities from 5 pcs - 0.11 USD
Net price for quantities from 25 pcs - 0.08 USDGross price for quantities from 25 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.06 USDGross price for quantities from 100 pcs - 0.06 USD
Net price for quantities from 500 pcs - 0.05 USDGross price for quantities from 500 pcs - 0.05 USD
Net price for quantities from 3000 pcs - 0.05 USDGross price for quantities from 3000 pcs - 0.05 USD
152385 in TME stock
No. of pieces (Multiple of: 5)
Minimum order quantity: 5.
Multiple of: 5.
WS2812B-2020-V6 | Programmable LED; RGB; SMD; 3.3÷5.3VDC; 2x2x0.84mm; 2kHz
Programmable LED; RGB; SMD; 3.3÷5.3VDC; 2x2x0.84mm; 2kHz
Manufacturer part number: WS2812B-2020-V6
Manufacturer: WORLDSEMI
Net price for quantities from 1 pcs - 0.31 USDGross price for quantities from 1 pcs - 0.31 USD
Net price for quantities from 10 pcs - 0.16 USDGross price for quantities from 10 pcs - 0.16 USD
Net price for quantities from 100 pcs - 0.11 USDGross price for quantities from 100 pcs - 0.11 USD
Net price for quantities from 500 pcs - 0.09 USDGross price for quantities from 500 pcs - 0.09 USD
Net price for quantities from 1000 pcs - 0.09 USDGross price for quantities from 1000 pcs - 0.09 USD
Net price for quantities from 2000 pcs - 0.08 USDGross price for quantities from 2000 pcs - 0.08 USD
Net price for quantities from 4500 pcs - 0.08 USDGross price for quantities from 4500 pcs - 0.08 USD
27588 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LTST-C190KRKT | LED; red; SMD; 0603; 18÷180mcd; 1.6÷2.4VDC; 1.6x0.8x0.8mm; 130°
LED; red; SMD; 0603; 18÷180mcd; 1.6÷2.4VDC; 1.6x0.8x0.8mm; 130°
Manufacturer part number: LTST-C190KRKT
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.12 USDGross price for quantities from 1 pcs - 0.12 USD
Net price for quantities from 100 pcs - 0.04 USDGross price for quantities from 100 pcs - 0.04 USD
Net price for quantities from 500 pcs - 0.03 USDGross price for quantities from 500 pcs - 0.03 USD
Net price for quantities from 1000 pcs - 0.03 USDGross price for quantities from 1000 pcs - 0.03 USD
Net price for quantities from 2000 pcs - 0.03 USDGross price for quantities from 2000 pcs - 0.03 USD
Net price for quantities from 4000 pcs - 0.02 USDGross price for quantities from 4000 pcs - 0.02 USD
Net price for quantities from 8000 pcs - 0.02 USDGross price for quantities from 8000 pcs - 0.02 USD
Net price for quantities from 12000 pcs - 0.02 USDGross price for quantities from 12000 pcs - 0.02 USD
Net price for quantities from 20000 pcs - 0.02 USDGross price for quantities from 20000 pcs - 0.02 USD
Net price for quantities from 28000 pcs - 0.02 USDGross price for quantities from 28000 pcs - 0.02 USD
59633 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LYE6SF-ABDA-363B5A | LED; yellow; SMD; PLCC4; 4.8÷15.15lm; 1400÷5600mcd; 2.05÷2.65VDC
LED; yellow; SMD; PLCC4; 4.8÷15.15lm; 1400÷5600mcd; 2.05÷2.65VDC
Manufacturer part number: LYE6SF-ABDA-363B5A
Manufacturer: ams OSRAM
Net price for quantities from 5 pcs - 0.31 USDGross price for quantities from 5 pcs - 0.31 USD
Net price for quantities from 25 pcs - 0.19 USDGross price for quantities from 25 pcs - 0.19 USD
Net price for quantities from 100 pcs - 0.17 USDGross price for quantities from 100 pcs - 0.17 USD
Net price for quantities from 500 pcs - 0.16 USDGross price for quantities from 500 pcs - 0.16 USD
Net price for quantities from 1000 pcs - 0.14 USDGross price for quantities from 1000 pcs - 0.14 USD
Net price for quantities from 2000 pcs - 0.13 USDGross price for quantities from 2000 pcs - 0.13 USD
Net price for quantities from 4000 pcs - 0.13 USDGross price for quantities from 4000 pcs - 0.13 USD
Net price for quantities from 10000 pcs - 0.12 USDGross price for quantities from 10000 pcs - 0.12 USD
Net price for quantities from 20000 pcs - 0.11 USDGross price for quantities from 20000 pcs - 0.11 USD
97755 in TME stock
No. of pieces (Multiple of: 5)
Minimum order quantity: 5.
Multiple of: 5.
HSMG-C170 | LED; green; SMD; 0805; 4.5÷15mcd; 2.2÷2.6VDC; 2x1.25x0.8mm; 170°
LED; green; SMD; 0805; 4.5÷15mcd; 2.2÷2.6VDC; 2x1.25x0.8mm; 170°
Manufacturer part number: HSMG-C170
Manufacturer: BROADCOM (AVAGO)
Net price for quantities from 1 pcs - 0.28 USDGross price for quantities from 1 pcs - 0.28 USD
Net price for quantities from 5 pcs - 0.23 USDGross price for quantities from 5 pcs - 0.23 USD
Net price for quantities from 10 pcs - 0.20 USDGross price for quantities from 10 pcs - 0.20 USD
Net price for quantities from 50 pcs - 0.12 USDGross price for quantities from 50 pcs - 0.12 USD
Net price for quantities from 100 pcs - 0.09 USDGross price for quantities from 100 pcs - 0.09 USD
Net price for quantities from 150 pcs - 0.08 USDGross price for quantities from 150 pcs - 0.08 USD
Net price for quantities from 250 pcs - 0.07 USDGross price for quantities from 250 pcs - 0.07 USD
Net price for quantities from 500 pcs - 0.07 USDGross price for quantities from 500 pcs - 0.07 USD
Net price for quantities from 1000 pcs - 0.06 USDGross price for quantities from 1000 pcs - 0.06 USD
Net price for quantities from 4000 pcs - 0.06 USDGross price for quantities from 4000 pcs - 0.06 USD
89914 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LY E67F-ABBB-46-1 | LED; yellow; SMD; PLCC4; 1400÷2800mcd; 2.05÷2.65VDC; 3.4x3x2.1mm
LED; yellow; SMD; PLCC4; 1400÷2800mcd; 2.05÷2.65VDC; 3.4x3x2.1mm
Manufacturer part number: LY E67F-ABBB-46-1
Manufacturer: ams OSRAM
Net price for quantities from 5 pcs - 0.23 USDGross price for quantities from 5 pcs - 0.23 USD
Net price for quantities from 100 pcs - 0.14 USDGross price for quantities from 100 pcs - 0.14 USD
Net price for quantities from 500 pcs - 0.13 USDGross price for quantities from 500 pcs - 0.13 USD
Net price for quantities from 1000 pcs - 0.12 USDGross price for quantities from 1000 pcs - 0.12 USD
Net price for quantities from 2000 pcs - 0.09 USDGross price for quantities from 2000 pcs - 0.09 USD
Net price for quantities from 4000 pcs - 0.09 USDGross price for quantities from 4000 pcs - 0.09 USD
Net price for quantities from 10000 pcs - 0.09 USDGross price for quantities from 10000 pcs - 0.09 USD
Net price for quantities from 20000 pcs - 0.08 USDGross price for quantities from 20000 pcs - 0.08 USD
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 5.
Multiple of: 1.
LTST-C191KRKT | LED; red; SMD; 0603; 18÷54mcd; 2÷2.4VDC; 1.6x0.8x0.55mm; 130°; 20mA
LED; red; SMD; 0603; 18÷54mcd; 2÷2.4VDC; 1.6x0.8x0.55mm; 130°; 20mA
Manufacturer part number: LTST-C191KRKT
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.14 USDGross price for quantities from 1 pcs - 0.14 USD
Net price for quantities from 10 pcs - 0.04 USDGross price for quantities from 10 pcs - 0.04 USD
Net price for quantities from 100 pcs - 0.03 USDGross price for quantities from 100 pcs - 0.03 USD
Net price for quantities from 500 pcs - 0.02 USDGross price for quantities from 500 pcs - 0.02 USD
Net price for quantities from 1000 pcs - 0.02 USDGross price for quantities from 1000 pcs - 0.02 USD
Net price for quantities from 3000 pcs - 0.02 USDGross price for quantities from 3000 pcs - 0.02 USD
Net price for quantities from 5000 pcs - 0.02 USDGross price for quantities from 5000 pcs - 0.02 USD
Net price for quantities from 10000 pcs - 0.02 USDGross price for quantities from 10000 pcs - 0.02 USD
Net price for quantities from 15000 pcs - 0.01 USDGross price for quantities from 15000 pcs - 0.01 USD
Net price for quantities from 25000 pcs - 0.01 USDGross price for quantities from 25000 pcs - 0.01 USD
52335 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
RF-W2SA50TS-A39R | LED; RGB; SMD; PLCC6; 1.8÷2.4/2.8÷3.6/2.8÷3.6VDC; 5.4x4.95x1.6mm
LED; RGB; SMD; PLCC6; 1.8÷2.4/2.8÷3.6/2.8÷3.6VDC; 5.4x4.95x1.6mm
Manufacturer part number: RF-W2SA50TS-A39R
Manufacturer: REFOND
Net price for quantities from 10 pcs - 0.11 USDGross price for quantities from 10 pcs - 0.11 USD
Net price for quantities from 50 pcs - 0.09 USDGross price for quantities from 50 pcs - 0.09 USD
Net price for quantities from 200 pcs - 0.08 USDGross price for quantities from 200 pcs - 0.08 USD
Net price for quantities from 500 pcs - 0.07 USDGross price for quantities from 500 pcs - 0.07 USD
Net price for quantities from 1000 pcs - 0.07 USDGross price for quantities from 1000 pcs - 0.07 USD
Net price for quantities from 2000 pcs - 0.06 USDGross price for quantities from 2000 pcs - 0.06 USD
Net price for quantities from 5000 pcs - 0.05 USDGross price for quantities from 5000 pcs - 0.05 USD
180940 in TME stock
No. of pieces (Multiple of: 10)
Minimum order quantity: 10.
Multiple of: 10.
WS2812B-V5 | Programmable LED; RGB; SMD; PLCC4; 3.7÷5.3VDC; 5x5x1.57mm
Programmable LED; RGB; SMD; PLCC4; 3.7÷5.3VDC; 5x5x1.57mm
Manufacturer part number: WS2812B-V5
Manufacturer: WORLDSEMI
Net price for quantities from 2 pcs - 0.39 USDGross price for quantities from 2 pcs - 0.39 USD
Net price for quantities from 10 pcs - 0.20 USDGross price for quantities from 10 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.13 USDGross price for quantities from 100 pcs - 0.13 USD
Net price for quantities from 500 pcs - 0.12 USDGross price for quantities from 500 pcs - 0.12 USD
Net price for quantities from 1000 pcs - 0.11 USDGross price for quantities from 1000 pcs - 0.11 USD
Net price for quantities from 2000 pcs - 0.11 USDGross price for quantities from 2000 pcs - 0.11 USD
Net price for quantities from 5000 pcs - 0.10 USDGross price for quantities from 5000 pcs - 0.10 USD
1 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 2.
Multiple of: 1.
Product available till the stock lasts
KP-1608SGC | LED; green; SMD; 0603; 4÷15mcd; 2.2÷2.5VDC; 1.6x0.8x1.1mm; 120°
LED; green; SMD; 0603; 4÷15mcd; 2.2÷2.5VDC; 1.6x0.8x1.1mm; 120°
Manufacturer part number: KP-1608SGC
Manufacturer: KINGBRIGHT ELECTRONIC
Net price for quantities from 1 pcs - 0.08 USDGross price for quantities from 1 pcs - 0.08 USD
Net price for quantities from 10 pcs - 0.06 USDGross price for quantities from 10 pcs - 0.06 USD
Net price for quantities from 100 pcs - 0.06 USDGross price for quantities from 100 pcs - 0.06 USD
Net price for quantities from 2000 pcs - 0.05 USDGross price for quantities from 2000 pcs - 0.05 USD
Net price for quantities from 12000 pcs - 0.05 USDGross price for quantities from 12000 pcs - 0.05 USD
103838 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
KP-2012SGC | LED; green; SMD; 0805; 4÷15mcd; 2.2÷2.5VDC; 2x1.25x1.1mm; 120°; 20mA
LED; green; SMD; 0805; 4÷15mcd; 2.2÷2.5VDC; 2x1.25x1.1mm; 120°; 20mA
Manufacturer part number: KP-2012SGC
Manufacturer: KINGBRIGHT ELECTRONIC
Net price for quantities from 1 pcs - 0.08 USDGross price for quantities from 1 pcs - 0.08 USD
Net price for quantities from 10 pcs - 0.08 USDGross price for quantities from 10 pcs - 0.08 USD
Net price for quantities from 50 pcs - 0.07 USDGross price for quantities from 50 pcs - 0.07 USD
Net price for quantities from 100 pcs - 0.06 USDGross price for quantities from 100 pcs - 0.06 USD
Net price for quantities from 500 pcs - 0.05 USDGross price for quantities from 500 pcs - 0.05 USD
Net price for quantities from 2000 pcs - 0.05 USDGross price for quantities from 2000 pcs - 0.05 USD
Net price for quantities from 4000 pcs - 0.05 USDGross price for quantities from 4000 pcs - 0.05 USD
69547 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LTST-C150KGKT | LED; green; SMD; 1206; 18÷71mcd; 2VDC; 3.2x1.6x1.1mm; 130°; 20mA
LED; green; SMD; 1206; 18÷71mcd; 2VDC; 3.2x1.6x1.1mm; 130°; 20mA
Manufacturer part number: LTST-C150KGKT
Manufacturer: LITEON
Net price for quantities from 1 pcs - 0.17 USDGross price for quantities from 1 pcs - 0.17 USD
Net price for quantities from 10 pcs - 0.08 USDGross price for quantities from 10 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.05 USDGross price for quantities from 100 pcs - 0.05 USD
Net price for quantities from 500 pcs - 0.04 USDGross price for quantities from 500 pcs - 0.04 USD
Net price for quantities from 1000 pcs - 0.03 USDGross price for quantities from 1000 pcs - 0.03 USD
Net price for quantities from 3000 pcs - 0.03 USDGross price for quantities from 3000 pcs - 0.03 USD
Net price for quantities from 6000 pcs - 0.02 USDGross price for quantities from 6000 pcs - 0.02 USD
9740 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
OF-SMD2012HR | LED; red; SMD; 0805; 460÷700mcd; 1.8÷2.4VDC; 2x1.25x0.68mm; 120°
LED; red; SMD; 0805; 460÷700mcd; 1.8÷2.4VDC; 2x1.25x0.68mm; 120°
Manufacturer part number: OF-SMD2012HR
Manufacturer: OPTOFLASH
Net price for quantities from 5 pcs - 0.16 USDGross price for quantities from 5 pcs - 0.16 USD
Net price for quantities from 25 pcs - 0.12 USDGross price for quantities from 25 pcs - 0.12 USD
Net price for quantities from 100 pcs - 0.10 USDGross price for quantities from 100 pcs - 0.10 USD
Net price for quantities from 1000 pcs - 0.09 USDGross price for quantities from 1000 pcs - 0.09 USD
Net price for quantities from 2000 pcs - 0.09 USDGross price for quantities from 2000 pcs - 0.09 USD
Net price for quantities from 4000 pcs - 0.08 USDGross price for quantities from 4000 pcs - 0.08 USD
Net price for quantities from 8000 pcs - 0.08 USDGross price for quantities from 8000 pcs - 0.08 USD
Net price for quantities from 12000 pcs - 0.07 USDGross price for quantities from 12000 pcs - 0.07 USD
Net price for quantities from 24000 pcs - 0.07 USDGross price for quantities from 24000 pcs - 0.07 USD
150005 in TME stock
No. of pieces (Multiple of: 5)
Minimum order quantity: 5.
Multiple of: 5.
OF-SMD3528WN | LED; white cold; SMD; PLCC2; Case (mm): 3528; 2100÷2400mcd; 6000K
LED; white cold; SMD; PLCC2; Case (mm): 3528; 2100÷2400mcd; 6000K
Manufacturer part number: OF-SMD3528WN
Manufacturer: OPTOFLASH
Net price for quantities from 5 pcs - 0.16 USDGross price for quantities from 5 pcs - 0.16 USD
Net price for quantities from 25 pcs - 0.08 USDGross price for quantities from 25 pcs - 0.08 USD
Net price for quantities from 100 pcs - 0.06 USDGross price for quantities from 100 pcs - 0.06 USD
Net price for quantities from 500 pcs - 0.05 USDGross price for quantities from 500 pcs - 0.05 USD
Net price for quantities from 2000 pcs - 0.04 USDGross price for quantities from 2000 pcs - 0.04 USD
63498 in TME stock
No. of pieces (Multiple of: 5)
Minimum order quantity: 5.
Multiple of: 5.
OF-SMD2012B | LED; blue; SMD; 0805; 150÷200mcd; 3÷3.2VDC; 2x1.25x0.68mm; 120°
LED; blue; SMD; 0805; 150÷200mcd; 3÷3.2VDC; 2x1.25x0.68mm; 120°
Manufacturer part number: OF-SMD2012B
Manufacturer: OPTOFLASH
Net price for quantities from 10 pcs - 0.07 USDGross price for quantities from 10 pcs - 0.07 USD
Net price for quantities from 50 pcs - 0.05 USDGross price for quantities from 50 pcs - 0.05 USD
Net price for quantities from 250 pcs - 0.04 USDGross price for quantities from 250 pcs - 0.04 USD
Net price for quantities from 1000 pcs - 0.04 USDGross price for quantities from 1000 pcs - 0.04 USD
Net price for quantities from 2000 pcs - 0.04 USDGross price for quantities from 2000 pcs - 0.04 USD
Net price for quantities from 4000 pcs - 0.03 USDGross price for quantities from 4000 pcs - 0.03 USD
Net price for quantities from 8000 pcs - 0.03 USDGross price for quantities from 8000 pcs - 0.03 USD
Net price for quantities from 12000 pcs - 0.03 USDGross price for quantities from 12000 pcs - 0.03 USD
Net price for quantities from 24000 pcs - 0.03 USDGross price for quantities from 24000 pcs - 0.03 USD
30051 in TME stock
No. of pieces (Multiple of: 10)
Minimum order quantity: 10.
Multiple of: 10.