+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Java - definition

Java is a high-level, object-oriented programming language and development platform, originally developed by Sun Microsystems and now being developed by Oracle Corporation. It was designed with portability, reliability and security in mind, following the principle of "write once, run anywhere" - meaning that a programme written in Java can be run on any device equipped with the Java Virtual Machine (JVM) execution environment, regardless of the operating system.

Source code in Java is compiled into bytecode, an intermediate format executed by the JVM, which allows it to remain independent of the hardware architecture. The JVM manages memory, supports multithreading, provides security mechanisms and error handling, making Java programmes more robust and easier to maintain. The language has an extensive standard library (Java API), including functionality for data handling, networking, Interfaces graphics, cryptography, databases and much more.

Java supports the object-oriented programming paradigm, in which classes, inheritance, polymorphism and encapsulation play a central role. This enables the construction of complex, modular systems that are easy to test and extend. At the same time, the language offers a readable syntax, similar to C and C++, which makes it easy to learn for those with structural programming experience.

The use of Java covers a wide range of areas - from desktop and server applications, to mobile applications (especially for Android), to embedded systems and enterprise solutions. The technology underpins many business environments, with solutions such as Java EE (Enterprise Edition) providing a set of tools for building scalable web applications. Java's development is supported by a community and a system of cyclic updates and standardisation, ensuring its stability and compliance with modern requirements software engineering.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.