+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Distributed computing - definition

Distributed computing is a paradigm of data processing, in which computing tasks are performed in parallel on multiple independent computing units networked together, acting as a coherent logical system. Unlike traditional centralised systems, distributed computing does not rely on a single central computer, but rather on the interaction of multiple nodes, each of which may have its own memory, operating system and processing resources.

This model allows problems requiring high computing power, high availability or scalability to be solved efficiently. Computations are broken down into smaller tasks that are distributed to the individual units, and the partial results are then aggregated. A key feature of this approach is concurrency and independent processing with the need for synchronisation and communication between nodes. This requires special algorithms for distributed data management, coordination and fault tolerance.

Distributed computing is the basis of many modern technologies such as cloud computing, grid computing, cluster systems or peer-to-peer networks. They are used in large-scale data analysis, modelling of physical phenomena, 3D graphics rendering, scientific computing, cryptography and stream processing systems.

A significant challenge in distributed systems is ensuring data integrity, reliability, transmission security and optimal resource allocation. Due to the lack of a central control point, distributed architectures require robustness to unit errors and mechanisms to detect and correct them. Designing such systems requires knowledge of network communication theory, concurrent algorithms and synchronisation and fault-tolerance issues.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.