+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Processor (CPU) - definition

The CPU (Central Processing Unit) is the central computing unit of a computer system, responsible for performing arithmetic operations, logical operations and controlling the flow of data and instructions in a digital circuit. Its architecture is based on a set of registers, execution units and communication buses that perform sequential processing of instructions according to the instruction cycle model, which includes fetching, decoding and executing operations according to the Instruction Set Architecture (ISA).

The basic element of the CPU is the arithmetic logic unit (ALU), responsible for mathematical operations and logical comparisons, and the control unit (CU), coordinating the data flow between the operational memory, registers and input-output circuits. Modern processors use superscalar architectures and parallel instruction execution mechanisms such as pipelining and hardware multithreading (Hyper-Threading, SMT) to increase processing efficiency and optimise the use of computing resources.

Complex memory management systems, including hierarchical cache systems (L1, L2, L3), jump prediction controllers and address translation buffers (TLBs), minimise data access latency and optimise performance under intensive processing conditions. Modern CPUs also integrate dedicated accelerators such as SIMD (Single Instruction, Multiple Data) units, which improve vector calculations used in algorithms computer graphics, data analysis and artificial intelligence.

Multi-core processors, in which the physical cores operate independently or share cache resources and communication buses, enable the simultaneous execution of multiple processing threads, which significantly increases operational throughput and enables efficient execution of multitasking workloads. Heterogeneous architectures use CPU-GPUs as well as solutions with dedicated neural processing units (NPUs) and FPGAs to support tasks that require high computational parallelism.

Advanced semiconductor manufacturing technologies allow the implementation of multilayer transistor structures with high integration density, based on FinFET and GAAFET technologies, leading to reduced power consumption and increased operational efficiency. Dynamic power management mechanisms, such as DVFS (Dynamic Voltage and Frequency Scaling) and Turbo Boost, enable adaptive adjustment of the processor's operating parameters to current loads, resulting in optimised energy balance and reduced thermal losses.

Modern CPUs are designed with hardware security in mind, including memory isolation technologies, protection mechanisms against speculative attacks and cryptographic instructions that enhance the security of processing operations. Server and computing systems use processors with enhanced RAS (Reliability, Availability, Serviceability) functionality, providing ECC error correction, anomaly detection and dynamic resource switching to minimise operational downtime.

CPU architectures are evolving towards increasing specialisation of computing units, implementation of advanced parallelism mechanisms and integration with co-processor chips, enabling efficient processing of tasks with high computational complexity in a wide range of applications, from embedded systems to supercomputers.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.