+1 300 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Date of publication: 06-05-2025 🕒 6 min read
Imagine a touchscreen that can "respond" – with a subtle click, a rough texture, or a sensation of resistance. This is how haptics works, a technology that allows electronic devices to simulate the sense of touch. Thanks to it, our interactions with equipment become more natural, intuitive, and multidimensional. Haptics is no longer just the vibration of a phone during a call – it also includes realistic sensations in video games, feedback in VR gloves, and even the simulation of scalpel pressure in robotic surgery. Increasingly, touch complements image and sound in digital interfaces, enhancing the message and engaging the user on a new level.
In this article, we will explore what haptics is and why it is becoming a key element of modern electronics. We will answer questions: What technologies allow the "feeling" of virtual objects? In which fields – from smartphones, through medicine, to automotive – is haptics used today? And what else might await us in the future when touch becomes as digital as the screen?
Haptics is a field of technology that deals with replicating tactile sensations, such as pressure, vibration, or resistance, in human interaction with electronic devices. The key here is the use of the sense of touch as an information channel – alongside sight and hearing – which significantly enriches content reception and increases the precision of actions. Haptic sensations are divided into two basic types. The tactile component comes from the skin surface – we feel roughness, temperature, or vibrations through it. The kinesthetic component includes information from muscles and joints, allowing, for example, to feel the weight of an object or resistance during movement. Both components are processed by specialized mechanoreceptors located in the skin and deep tissues. These receptors react to various stimuli: Meissner's corpuscles to light touch and vibrations, Pacini's to rapid vibrations, Merkel's to steady pressure, and Ruffini's to stretching.
In electronic devices, tactile sensations are artificially generated – through feedback, which means transmitting a tactile stimulus in response to a user's action. For example, touching a button on a smartphone screen can be reciprocated with a short vibration that mimics a "click". This gives the user physical confirmation of the action, improving ergonomics and reducing errors.
The history of haptics dates back to the mid-20th century when the first experiments with devices transmitting tactile information appeared. A breakthrough occurred in the 1990s, with the emergence of interfaces such as PHANToM – a device with a robotic arm that allowed "touching" virtual objects. At the same time, technology began to enter entertainment – in 1997, the DualShock controller for the PlayStation console introduced vibrations as a standard element of games. In subsequent years, further innovations appeared, such as Apple's precise Taptic Engine system, used today in iPhones and Apple Watches. It is worth adding that video games and aviation were pioneers in the adoption of haptics – from control sticks with resistance to controllers with vibrations signaling dangers or collisions.
Haptics has evolved from simple, mechanical solutions to advanced digital simulations of the sense of touch. Currently, it forms the foundation of modern user interfaces, and its potential continues to grow with the development of electronics, materials, and artificial intelligence.
Modern electronics offer many ways to deliver tactile sensations. Device designers now have a range of haptic technologies at their disposal, which differ in principle of operation, precision, cost, and possible applications. From simple vibration motors, through high-precision piezoelectric modules, to ultrasonic "touch in the air" – each of these technologies finds its place in user interfaces.
The most common form of haptics in consumer electronics is mechanical vibrations generated by miniature motors. There are two main types: ERM (Eccentric Rotating Mass) and LRA (Linear Resonant Actuator). The ERM motor works by rotating an unbalanced mass, which causes the entire device to vibrate. In contrast, the LRA uses a mass mounted on a spring, electromagnetically stimulated to move in one direction, allowing for more precise and rapid effects.
ERM motors dominated in older mobile phones and classic console pads. They were cheap and effective but reacted slowly and offered only basic vibrations. Newer designs, such as modern smartphones or PlayStation and Nintendo controllers, increasingly use LRA. This allows for more varied haptic effects – from a short "tap" to long pulsations. These vibrations are used to confirm touch on the screen, inform about notifications, and in games – to increase immersion.
See vibration motors in the TME offer
Piezoelectric technology allows for much greater precision of operation. In this case, materials that deform under the influence of electrical voltage are used. Piezo actuators can generate very fast and subtle movements, making them ideal for advanced applications – for example, in laptop touchpads, where they simulate a click without using a mechanical button, or in medical devices, where accuracy and speed of response are crucial.
Due to their properties, piezoelectrics allow not only for vibrations but also for replicating various textures or clicks of different strengths. Although they are more expensive and require higher supply voltages, their use is growing where precision and compact dimensions are essential.
One of the more advanced and impressive technologies is electrostatic haptics, also known as electrovibration. Instead of physical movement, it uses a variable electrostatic field that increases friction between the finger and the screen surface. The user can thus feel roughness, slipperiness, or bumps on smooth glass.
This technology does not require moving parts, only a transparent electrode on the screen and appropriate voltage control. Practical applications include solutions such as TanvasTouch or Senseg, presented at technology fairs. They enable, for example, tactile exploration of material texture during online shopping or operation of buttons without looking at the screen – which finds application in automotive, among others.
An even more futuristic approach is ultrasonic haptics. This technology uses focused sound waves at high frequencies, which – despite the lack of physical contact – create a noticeable pressure on the skin. In practice, this means the possibility of "feeling" an object floating in the air, such as a button or surface.
Solutions of this type are being developed, for example, by the company Ultraleap, which combines haptics with a hand-tracking system. The technology finds application in touchless interfaces – for example, in VR/AR, where the user does not need a glove to feel a virtual object, or in car panels, where buttons can be operated "in the air" without the risk of dirtying the screen. This is also an example of haptics that enhances hygiene and safety in public spaces.
The most innovative approaches use smart materials that change their shape or properties in response to stimuli – voltage, temperature, or magnetic field. This group includes, among others, electroactive polymers (EAP) and shape memory alloys (SMA), such as nitinol.
Solutions based on these materials are lightweight, flexible, and can be almost invisible – ideal for wearable devices (wearables), interactive clothing, or thin layers applied to screens. Examples include thin vibrating films, flexible straps in VR gloves, or micro actuators in medicine. Although this technology is still developing in laboratories, it already shows the potential for creating a new generation of haptic interfaces – lightweight, quiet, and almost imperceptible, but full of tactile possibilities.
Haptics is not just advanced technology – it is primarily a tool that improves the quality of user interaction with devices. Its presence in modern interfaces directly affects the way we perceive technology: it makes it more understandable, predictable, and engaging. Touch introduces a physical feedback element that strengthens system responses and reduces uncertainty in operation, which is particularly important in the context of touch screens or virtual environments.
One of the main advantages of haptics is its intuitiveness. Well-designed tactile effects lead the user almost "by feel", without the need for additional visual messages. This makes device operation more natural – especially where sight or hearing are already occupied, such as while driving or training.
Haptics also improves the precision and engagement of the user. Even subtle vibration can help confirm a button press, reducing errors and enhancing the comfort of interface use. In games or VR applications, tactile sensations increase immersion, making the user better "immerse" in the environment. Additionally, more and more systems offer personalization of tactile experiences – users can adjust the strength of vibrations, the duration of impulses, or even assign different effects to specific actions.
Despite numerous benefits, haptics is not without challenges. One of the basic limitations is the cost of components – precise actuators, such as piezoelectric or ultrasonic, are more expensive than classic motors, which may limit their use in cheaper devices. Another aspect is energy consumption. Vibrations, especially strong or prolonged ones, can significantly burden the battery, forcing design compromises – especially in mobile devices.
Designing haptic interfaces also requires considering the needs of people with disabilities. For some users, strong vibration may be helpful, for others – too intense or difficult to interpret. Therefore, it is necessary to create flexible and configurable solutions that allow adjusting the strength, frequency, and type of stimulus to individual preferences. Haptics can be a huge support for people with sensory limitations, but only if it is designed with accessibility in mind.
The market shows clear trends that define the future development of the industry. One of them is miniaturization – smaller and more efficient components allow for the use of haptics even in very compact devices, such as headphones, rings, or bands. Another direction is integration with AI, which enables dynamic adjustment of tactile effects to user behaviors and preferences. Wearable devices are also becoming an increasingly important segment – wearables, which thanks to haptics become more interactive, informative, and comfortable to use.
Looking to the future, haptics has enormous potential for development in entirely new fields. Wearable touch interfaces can revolutionize everyday communication, warning of dangers, or even assist blind people in spatial orientation. There is also growing interest in using haptics in art and emotional communication – experiments with haptic music, digital sculpture, or conveying emotions through vibrations show that this technology goes beyond utilitarian frames and becomes a means of expression.
In the perspective of a few years, touch may become the new language of digital interaction. Just as image and sound changed the way we communicate with machines, now comes the era in which tactile sensations will not only inform but also engage, lead, and emotionally enrich the user experience. Haptics is no longer just an addition – it becomes an integral part of the digital world.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,300,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.