You are browsing the website for customers from: Slovenia. Based on location data, the suggested version of the page for you is USA / US

+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

How to calculate the required power of an LED power supply?

Date of publication: 09-10-2025 🕒 6 min read

Have you ever wondered which LED power supply would be the best solution for your project? Proper selection of the power supply is crucial for the performance and longevity of the LED strip, which is important for hobbyists, students, and consumers who want to maximize the potential of such lighting. In this article, we will thoroughly explain how to calculate the required power for an LED power supply and why it is so important.

Key information in brief

  • The power of the LED power supply is calculated by multiplying the length of the strip by the nominal power (W/m).
  • It is recommended to add a 20–30% power margin to avoid overload.
  • When choosing a power supply, consider the supply voltage of the LED strip (most often 12V or 24V).
  • LED power supplies should have overload, short-circuit, and overvoltage protection.
  • When connecting the power supply, it is important to maintain the correct polarity of the wires (red "+" and black "−").
  • If you are unsure about the installation correctness, it is worth consulting a specialist.

We will start with basic information about LED power supplies and then proceed to key aspects that will help make the right choice. In the article, we will show how to calculate the power of the power supply, taking into account the length of the strip and its nominal power. We will also discuss the importance of adding a power margin to minimize the risk of power supply overload.

How to calculate the power of the power supply

Calculating the power of the LED power supply is a crucial step that enables proper powering of the LED strip and ensures its longevity. To get the right power, you should use a simple formula:

Length of the strip (m) x Strip power (W/m).

For example, if you have 3 meters of LED strip with a power of 4.8W/m, the calculation is as follows: 3m x 4.8W/m = 14.4 W. This result gives us an idea of the minimum power the power supply must have to power the strip.

However, you should not forget to add a power margin, which is extremely important to avoid overloading the power supply. It is recommended to add 20–30% power margin to the calculated value. In our case, adding 20% to 14.4 W gives: 14.4 W x 120% = 17.28 W. This means a power supply of at least 18W is needed for proper operation. This approach protects the power supply from damage and the LED strip from potential operational problems, which is essential for anyone who wants to fully utilize the potential of their lighting.

How to choose a power supply?

Choosing the right power supply is key for the proper functioning of the LED lighting system. The most common types of power supplies are 12V and 24V, which adapt the mains voltage to that required by the LED diodes. When choosing a power supply, pay attention to technical parameters such as maximum power, type of supply (DC or AC), and additional protections against overload, short circuit, or overheating.

When planning to connect multiple light sources, you must carefully calculate their total power. For example, if you have six LED points, each with 6W power, calculate: 6W x 6 = 36W. Adding a power margin recommended at 20% gives: 36W + 20% = 43.2W. When choosing a power supply, select a model with a power of at least 45W to ensure stable power.

Examples of power supply power calculations

Calculating power supply power is crucial to ensure the stability and efficiency of the LED lighting system. To convert Amperes to Watts, you can use a simple formula:

Voltage x Current.

For example, for a power supply with 12V voltage and 1.25A current, power can be calculated as 1.25A x 12V = 15W. In another case, for a 12V power supply with 2.1A current, calculations are: 2.1A x 12V = 25W. Such conversions are essential when choosing the right power supply.

When considering different lengths of LED strips, appropriate calculations must also be done. For example, for a strip with 15W/m power and a length of 5m, calculate: 5m x 15W/m = 75W. Adding a 20% margin gives 75W + 20% = 90W (recommended power supply 90W). Similarly, for a 10m strip with 10W/m power, calculations are: 10m x 10W/m = 100W, and adding the margin gives 100W + 20% = 120W (power supply 120W). For a 15m strip with 13W/m power, calculate: 15m x 13W/m = 195W, which after adding a 20% margin gives 195W + 20% = 234W (power supply 295W). These kinds of calculations help choose a power supply capable of efficiently powering the entire LED system.

How to connect the power supply to the LED strip?

Connecting the power supply to the LED strip is a critical step affecting the efficiency and safety of the entire installation. To connect the power supply correctly, it is worth starting by understanding its schematic. First, ensure the power is turned off. Power supplies have two markings: INPUT (power input 230V) and OUTPUT (LED strip output). When connecting the power supply, pay special attention to polarity: the red wire corresponds to (+), and the black wire to (−). Incorrect connection of these wires can lead to damage to both the power supply and the LED strip.

Regarding safety, ensure the power supply has adequate power to handle the entire installation. A power supply that is too weak can lead to overheating and device damage. Therefore, adding a power margin is necessary. Also, remember the need to connect the wires precisely — incorrect connection may cause short circuits or other problems.

What protections do LED power supplies have?

Protections in LED power supplies play a key role in ensuring system stability and safety. Thanks to various forms of protection, such as overvoltage, short-circuit, and overload protection, these power supplies maintain voltage at a constant level, which is crucial for the proper functioning of LED diodes. These protections help avoid damage both in the power supply and the LED strips themselves, significantly extending their lifespan.

The MTBF (Mean Time Between Failures) parameter, which means the average time between failures, is also an important durability indicator for power supplies. The higher the MTBF value, the better the build quality and reliability of the device. High-quality LED power supplies, often offered by reputable brands, have a long MTBF, meaning they are more resistant to damage and will operate for a longer time without requiring replacement. When choosing a power supply, it is worth paying attention to these parameters to ensure effective and safe lighting.

Summary

Choosing the right power supply for an LED strip is crucial for ensuring proper operation and the longevity of the lighting installation. Remember a few important points: first of all, select a power supply power that should be 20% higher than the total power of the LED strip to provide a proper margin. It is also important to match the voltage of the power supply to the strip requirements, most often choosing 12V or 24V models. Do not forget about the type of power supply, which should be suitable for the conditions it will be used in—for example, for outdoor applications, a power supply with appropriate moisture and dirt protection rating is necessary.

Can I use one power supply for several different LED strips?

Yes, you can use one power supply for multiple LED strips, but they must all have the same supply voltage (e.g., all 12V). It is also necessary to calculate the total power consumption of all connected strips and add a recommended power reserve (20–30%) to prevent overloading the power supply.

Which type of power supply should I choose – constant voltage or constant current?

Constant voltage power supplies work best with flexible LED strips and decorative lighting, while constant current power supplies are recommended for high-power LEDs that require precise current control.

Does the cable length matter when choosing an LED power supply?

Yes, the cable length affects voltage drops, which can result in reduced brightness at the end of the LED strip. For longer cable runs, it is advisable to use a power supply with slightly higher power output or cables with a larger cross-section to minimize energy losses.

Are LED power supplies energy-efficient?

Yes, most modern LED power supplies have an energy efficiency of 80–90%. Higher efficiency means less energy wasted as heat, resulting in lower operating costs and longer device lifespan.

Can an LED power supply be installed outdoors?

Yes, but only power supplies specifically designed for outdoor use (with an IP67 or higher protection rating) can be installed in environments exposed to moisture, rain, or dust. Standard indoor power supplies should not be used outdoors.

Do all LED power supplies support dimming?

No, not all LED power supplies support dimming. If you want brightness control, make sure the selected model supports dimming standards such as 0–10V, DALI, or PWM.

How often should I maintain an LED power supply?

It is recommended to perform maintenance at least every 6–12 months. Maintenance mainly involves cleaning the power supply housing from dust, checking the condition of cables and connectors, and inspecting the sealing in outdoor installations.

Does an LED power supply need grounding?

It depends on the protection class of the power supply. Class I power supplies require a protective ground connection, while Class II or III units do not, as they feature reinforced insulation or operate at safe extra-low voltage (SELV).

Can I plug an LED power supply into a regular outlet?

Yes, most LED power supplies are designed for standard mains voltage (e.g., 230V). However, ensure that the power supply’s technical specifications match the mains voltage and that the installation complies with applicable safety standards.

What are the most common causes of LED power supply failures?

The most common causes of LED power supply failures are overloading (insufficient power capacity), poor ventilation (overheating), installation errors (e.g., incorrect wire polarity), and environmental factors such as moisture, dust, or high temperatures.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

rightColumnPicture rightColumnPicture

READ ALSO