+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

PLC (Programmable Logic Controller) - definition

PLC (Programmable Logic Controller) is a specialized microprocessor-based device designed for automatic control of industrial processes, machinery, and technological systems. Its primary function is to continuously monitor input signals from sensors, buttons, or other detection elements, process them according to programmed logic, and generate appropriate output signals to control actuators, relays, valves, or other execution elements.

A PLC is built to operate in harsh industrial environments characterized by electromagnetic interference, vibration, moisture, or extreme temperatures. Its robust design ensures high reliability and resistance to environmental factors, allowing long-term operation without the need for frequent maintenance or calibration. One of the key advantages of a PLC is its modular architecture, which allows system expansion with additional inputs, outputs, communication interfaces, or specialized modules.

Programmable logic controllers use programming languages compliant with the IEC 61131-3 standard, such as Ladder Diagram (LD), Instruction List (IL), Structured Text (ST), and Function Block Diagram (FBD). These languages allow the development of complex control algorithms that can be easily modified and adapted to changing process conditions without hardware intervention. Programming is typically performed on a computer using dedicated software and a communication interface.

PLCs play a critical role in production automation, transport systems, infrastructure management, and any application requiring sequential or conditional control with high precision and reliability. Compared to traditional relay-based systems, PLCs offer significantly greater flexibility, real-time system monitoring, and easier fault diagnostics. Integration with industrial networks and SCADA systems enables remote management, visualization, and optimization of technological processes.

PLC drivers

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.