+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Programming language - definition

A Programming Language is a formal instructional writing system by which a programmer defines algorithms, operations and data structures to create computer programmes. The language bridges the gap between the logic of a machine and the way a human thinks, enabling the precise formulation of commands that can be interpreted or compiled by a computer. Programming languages have a defined syntax (rules of notation) and semantics (meaning of instructions) that make it possible to create complex digital systems, utility applications and computational solutions.

Depending on the level of abstraction, programming languages are divided into low-level languages, which are close to the hardware structure, and high-level languages, which are oriented towards operational logic and code readability. High-level languages such as Python, Java, C++ or Rust provide mechanisms for data abstraction, flow control, modularity and error handling, which greatly facilitate the design and maintenance of large programming projects. There are also specialised languages targeting specific domains, such as e.g. MATLAB in numerical analysis or VHDL in digital circuit design.

The programming language also determines the paradigm in which code development takes place - it can be imperative, object-oriented, functional, declarative or a combination of these approaches. The choice of language depends on the nature of the problem, the Tools available and the execution environment. Each language has its own compiler or interpreter, which converts source code into a form executable by processor or virtual machine.

The importance of programming languages is central to the entire process of software engineering - from requirements analysis, implementation and testing to optimisation and maintenance. The language defines the ability to express algorithms, how memory is managed, how concurrency is handled and the availability of libraries and tools to support application development. Modern languages are evolving towards greater type safety, code readability, portability and execution efficiency.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.