مراوح المكتب

(1)

As a piece of office equipment, office fans can play a crucial role in building the productivity and well-being of your employees. This kind of device can help maintain proper air circulation and temperature by distributing heat or cold around the room evenly. Also, it helps remove air contamination such as, for example, smoke.

All these factors show that a fan can have a positive impact on the comfort, productivity and well-being of those working in the office.

How a desk fan works

A fan is a device which forces the air to move in a room. It usually has got 3 or 4 blades, which spin around the axis of a shaft and push the air in a particular direction. A desk fan can be powered from the mains, by a battery or a USB port. Such a device usually offers a few operating modes and speed adjustment, so that it can satisfy the user’s actual needs best.

Fans are used for many different purposes, e.g. to cool down a room or to remove unwanted odours. They are very useful in offices, where they help maintain appropriate temperature and provide better air circulation. All of this may positively influence the employees’ well-being and productivity.

Office fans – what are they for?

An office fan is a device which helps circulate air in an office. There are different kinds of fans available, and the choice depends on the user’s preferences and needs. Below, you can see some examples of office fans:

A table/desk fan is rather small and can be set, for example, on an employee’s desk. It is available in different sizes and colours. Also, some models offer speed adjustment and oscillation features.

Floor/pedestal fans are bigger than table fans and often have additional features, such as: oscillation, height adjustment, speed adjustment as well as an auto off option, which helps save energy. A large office fan is perfect for those who need intensive air flow in a room, for example, when it is very hot or when they work in a room without air conditioning. It can also be useful in rooms in which there is a need to distribute the air very fast, such as a kitchen or a bathroom.

Wall fans are designed to be wall-mounted and often offer the oscillation feature. They are perfect for small offices or conference rooms, where there is not enough space to set a floor/pedestal fan.

While choosing an office fan, you need to pay attention to the level of noise and energy consumption as well as the device performance parameters. You should also remember to clean the fan regularly in order to avoid the accumulation of dust and other dirt.

Office fans available at TME

In our catalogue, you can browse through the available fans and sort them according to many categories.

Type, power and voltage of a fan

In the catalogue, there are fans powered by alternating current or direct current. You can also search for specific ranges of power or voltage values.

Power cord/adapter type

You can choose from 3 types:

You should also take into account the length of the power cord.

Other criteria for choosing an office fan

In terms of efficiency, it is worth considering the size and diameter of the fan head. If the appearance is important to you, pay attention to the housing colour.

منتجات: 1

المستودع:

TME
الكل
الصفحة 1
WIFIFNH10CBK | Fan: AC; 2kW; 220÷240V; Len: 1.7m; 190x565x190mm; Plug: angled 90°
Fan: AC; 2kW; 220÷240V; Len: 1.7m; 190x565x190mm; Plug: angled 90°
رمز الشركة المصنعة: WIFIFNH10CBK
السعر الصافي للكميات من 1 pcs - 99.30 EURالسعر الإجمالي للكميات من 1 pcs - 99.30 EUR