+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Capacitors

(17 504)

A capacitor is one of the basic passive electronic components. Its task is to store energy in the electric field. The amount of stored energy is described by the capacitance of the capacitor, which is expressed in farads (F). The capacitance measured in full farads is not very common. Typically, capacitors have the capacitance of micro- (µ), nano- (n), pico- (p) farads.
The second basic parameter of a capacitor, apart from its capacitance, is its maximum operating voltage. Due to its design, a capacitor is susceptible to the so-called breakdown. Therefore, each capacitor has a parameter that defines the maximum voltage that can appear between its terminals. After exceeding it, a breakdown may occur, resulting in a short-circuit of the capacitor.

Capacitor – design and principle of operation

Capacitors are made of two conductors (capacitor plates) separated from each other by a non-conductive dielectric material. It can be any insulating material such as: air, plastic, ceramics, paper. The operation of a capacitor is based on Coulomb's law. According to that law, the media on both plates of the capacitor interact with each other. Media with the same charge repel each other, while those with the opposite charge attract each other. The effect of such a phenomenon is the presence of opposite charges on the capacitor plates. Their number is equal on both sides. Thanks to the dielectric material contained between the plates, the flow of charges is impossible, and this results in the formation of an electric field.

Types of capacitors

There are many different types of capacitors available on the market, including customized designs for specific tasks. Some of the types of capacitors available at TME are described below. Ceramic capacitors and MLCCs – these are some of the most common electronic components. What is interesting, the number of such capacitors manufactured in a single year is about one trillion. Ceramic capacitors owe their name to the ceramics used as an insulating material. MLCCs (multi-layer ceramic capacitors) are a subtype of conventional ceramic capacitors. An MLCC is a ceramic capacitor made in a multi-layer process. Ceramic capacitors do not have a specific polarisation, so they can be used in AC circuits, they are also available in both THT (through-hole mounting) and SMD (surface mounting) versions.

Electrolytic capacitors – the second most common type of capacitors are electrolytic designs. Thanks to the use of electrolyte, they offer much larger capacitance than ceramic capacitors. Almost all of them require appropriate polarisation – incorrect incorporation of such a capacitor into a circuit may even result in its explosion. These capacitors are also available in THT and SMD versions.

Trimmer – it is a variable capacitor, also called a tuning capacitor or tuning condenser. As the name suggests, the capacitance of such a capacitor can be freely adjusted. Trimmers were used in older designs of radios. At TME, several modern SMD trimmers are available.

Supercapacitors – they are a type of electrolytic capacitors and are able to store huge amounts of energy. Thanks to a special design, their capacitance reaches up to 3kF. In practice, it can be said that supercapacitors combine features of conventional capacitors and rechargeable batteries. Charging speed is their great advantage.

Products: 17 504

Warehouse:

TME
All
Page 1
NEW
EEHZA1K470V | Capacitor: hybrid; H: 10.5mm; 47uF; 80VDC; 1.7A; SMD; ESR: 36mΩ; ZA
Capacitor: hybrid; H: 10.5mm; 47uF; 80VDC; 1.7A; SMD; ESR: 36mΩ; ZA
Manufacturer part number: EEHZA1K470V
Manufacturer: PANASONIC
Net price for quantities from 1 pcs - 2.18 EURGross price for quantities from 1 pcs - 2.18 EUR
Net price for quantities from 5 pcs - 1.85 EURGross price for quantities from 5 pcs - 1.85 EUR
Net price for quantities from 10 pcs - 1.66 EURGross price for quantities from 10 pcs - 1.66 EUR
Net price for quantities from 50 pcs - 1.24 EURGross price for quantities from 50 pcs - 1.24 EUR
Net price for quantities from 100 pcs - 1.13 EURGross price for quantities from 100 pcs - 1.13 EUR
Net price for quantities from 250 pcs - 0.99 EURGross price for quantities from 250 pcs - 0.99 EUR
Net price for quantities from 500 pcs - 0.92 EURGross price for quantities from 500 pcs - 0.92 EUR
Net price for quantities from 1000 pcs - 0.86 EURGross price for quantities from 1000 pcs - 0.86 EUR
Net price for quantities from 1500 pcs - 0.84 EURGross price for quantities from 1500 pcs - 0.84 EUR
Net price for quantities from 3500 pcs - 0.80 EURGross price for quantities from 3500 pcs - 0.80 EUR
28 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
HG2W687M35050HC | Capacitor: electrolytic; SNAP-IN; 680uF; 450VDC; Ø35x50mm; ±20%
Capacitor: electrolytic; SNAP-IN; 680uF; 450VDC; Ø35x50mm; ±20%
Manufacturer part number: HG2W687M35050HC
Manufacturer: SAMWHA
Net price for quantities from 1 pcs - 5.61 EURGross price for quantities from 1 pcs - 5.61 EUR
Net price for quantities from 5 pcs - 5.37 EURGross price for quantities from 5 pcs - 5.37 EUR
Net price for quantities from 10 pcs - 5.11 EURGross price for quantities from 10 pcs - 5.11 EUR
Net price for quantities from 25 pcs - 4.84 EURGross price for quantities from 25 pcs - 4.84 EUR
Net price for quantities from 50 pcs - 4.66 EURGross price for quantities from 50 pcs - 4.66 EUR
Net price for quantities from 100 pcs - 4.42 EURGross price for quantities from 100 pcs - 4.42 EUR
11 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
MSASU31LBB5106KTNA01 | Capacitor: ceramic; MLCC; 10uF; 50VDC; X5R; ±10%; SMD; 1206
Capacitor: ceramic; MLCC; 10uF; 50VDC; X5R; ±10%; SMD; 1206
Manufacturer part number: MSASU31LBB5106KTNA01
Manufacturer: TAIYO YUDEN
Net price for quantities from 1 pcs - 0.24 EURGross price for quantities from 1 pcs - 0.24 EUR
Net price for quantities from 10 pcs - 0.12 EURGross price for quantities from 10 pcs - 0.12 EUR
Net price for quantities from 50 pcs - 0.07 EURGross price for quantities from 50 pcs - 0.07 EUR
Net price for quantities from 100 pcs - 0.05 EURGross price for quantities from 100 pcs - 0.05 EUR
Net price for quantities from 250 pcs - 0.05 EURGross price for quantities from 250 pcs - 0.05 EUR
Net price for quantities from 500 pcs - 0.04 EURGross price for quantities from 500 pcs - 0.04 EUR
Net price for quantities from 1000 pcs - 0.04 EURGross price for quantities from 1000 pcs - 0.04 EUR
Net price for quantities from 2000 pcs - 0.04 EURGross price for quantities from 2000 pcs - 0.04 EUR
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
Hardly available product
NEW
NXH35VB220M3.5TP8X11.5 | Capacitor: electrolytic; low ESR; THT; 220uF; 35VDC; Pitch: 3.5mm
Capacitor: electrolytic; low ESR; THT; 220uF; 35VDC; Pitch: 3.5mm
Manufacturer part number: NXH35VB220M3.5TP8X11.5
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.08 EURGross price for quantities from 1 pcs - 0.08 EUR
Net price for quantities from 10 pcs - 0.07 EURGross price for quantities from 10 pcs - 0.07 EUR
Net price for quantities from 50 pcs - 0.06 EURGross price for quantities from 50 pcs - 0.06 EUR
Net price for quantities from 100 pcs - 0.06 EURGross price for quantities from 100 pcs - 0.06 EUR
Net price for quantities from 250 pcs - 0.05 EURGross price for quantities from 250 pcs - 0.05 EUR
Net price for quantities from 500 pcs - 0.05 EURGross price for quantities from 500 pcs - 0.05 EUR
Net price for quantities from 1000 pcs - 0.05 EURGross price for quantities from 1000 pcs - 0.05 EUR
1156 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
RD1C108M10016PA | Capacitor: electrolytic; THT; 1000uF; 16VDC; 10x16mm; ±20%; 2000h
Capacitor: electrolytic; THT; 1000uF; 16VDC; 10x16mm; ±20%; 2000h
Manufacturer part number: RD1C108M10016PA
Manufacturer: SAMWHA
Net price for quantities from 1 pcs - 0.08 EURGross price for quantities from 1 pcs - 0.08 EUR
Net price for quantities from 10 pcs - 0.07 EURGross price for quantities from 10 pcs - 0.07 EUR
Net price for quantities from 50 pcs - 0.07 EURGross price for quantities from 50 pcs - 0.07 EUR
Net price for quantities from 100 pcs - 0.06 EURGross price for quantities from 100 pcs - 0.06 EUR
Net price for quantities from 250 pcs - 0.06 EURGross price for quantities from 250 pcs - 0.06 EUR
Net price for quantities from 500 pcs - 0.06 EURGross price for quantities from 500 pcs - 0.06 EUR
Net price for quantities from 1000 pcs - 0.06 EURGross price for quantities from 1000 pcs - 0.06 EUR
Net price for quantities from 1500 pcs - 0.05 EURGross price for quantities from 1500 pcs - 0.05 EUR
Net price for quantities from 3000 pcs - 0.05 EURGross price for quantities from 3000 pcs - 0.05 EUR
Net price for quantities from 6000 pcs - 0.05 EURGross price for quantities from 6000 pcs - 0.05 EUR
2 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
NXH50VB470M10X20 | Capacitor: electrolytic; low ESR; THT; 470uF; 50VDC; Pitch: 5mm
Capacitor: electrolytic; low ESR; THT; 470uF; 50VDC; Pitch: 5mm
Manufacturer part number: NXH50VB470M10X20
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.22 EURGross price for quantities from 1 pcs - 0.22 EUR
Net price for quantities from 10 pcs - 0.18 EURGross price for quantities from 10 pcs - 0.18 EUR
Net price for quantities from 25 pcs - 0.16 EURGross price for quantities from 25 pcs - 0.16 EUR
Net price for quantities from 50 pcs - 0.14 EURGross price for quantities from 50 pcs - 0.14 EUR
Net price for quantities from 100 pcs - 0.13 EURGross price for quantities from 100 pcs - 0.13 EUR
85 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
SD2A106M05011PC | Capacitor: electrolytic; THT; 10uF; 100VDC; 5x11mm; ±20%; 2000h
Capacitor: electrolytic; THT; 10uF; 100VDC; 5x11mm; ±20%; 2000h
Manufacturer part number: SD2A106M05011PC
Manufacturer: SAMWHA
Net price for quantities from 1 pcs - 0.08 EURGross price for quantities from 1 pcs - 0.08 EUR
Net price for quantities from 10 pcs - 0.04 EURGross price for quantities from 10 pcs - 0.04 EUR
Net price for quantities from 100 pcs - 0.02 EURGross price for quantities from 100 pcs - 0.02 EUR
Net price for quantities from 500 pcs - 0.02 EURGross price for quantities from 500 pcs - 0.02 EUR
Net price for quantities from 1000 pcs - 0.02 EURGross price for quantities from 1000 pcs - 0.02 EUR
Net price for quantities from 2000 pcs - 0.02 EURGross price for quantities from 2000 pcs - 0.02 EUR
Net price for quantities from 4000 pcs - 0.02 EURGross price for quantities from 4000 pcs - 0.02 EUR
Net price for quantities from 6000 pcs - 0.01 EURGross price for quantities from 6000 pcs - 0.01 EUR
Net price for quantities from 10000 pcs - 0.01 EURGross price for quantities from 10000 pcs - 0.01 EUR
3836 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
NXH35VB470M10X16 | Capacitor: electrolytic; low ESR; THT; 470uF; 35VDC; Pitch: 5mm
Capacitor: electrolytic; low ESR; THT; 470uF; 35VDC; Pitch: 5mm
Manufacturer part number: NXH35VB470M10X16
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.12 EURGross price for quantities from 1 pcs - 0.12 EUR
Net price for quantities from 10 pcs - 0.11 EURGross price for quantities from 10 pcs - 0.11 EUR
Net price for quantities from 25 pcs - 0.09 EURGross price for quantities from 25 pcs - 0.09 EUR
Net price for quantities from 50 pcs - 0.08 EURGross price for quantities from 50 pcs - 0.08 EUR
Net price for quantities from 100 pcs - 0.08 EURGross price for quantities from 100 pcs - 0.08 EUR
65 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
RD1V477M10016PA | Capacitor: electrolytic; THT; 470uF; 35VDC; 10x16mm; ±20%; 2000h
Capacitor: electrolytic; THT; 470uF; 35VDC; 10x16mm; ±20%; 2000h
Manufacturer part number: RD1V477M10016PA
Manufacturer: SAMWHA
Net price for quantities from 1 pcs - 0.25 EURGross price for quantities from 1 pcs - 0.25 EUR
Net price for quantities from 10 pcs - 0.15 EURGross price for quantities from 10 pcs - 0.15 EUR
Net price for quantities from 50 pcs - 0.10 EURGross price for quantities from 50 pcs - 0.10 EUR
Net price for quantities from 100 pcs - 0.09 EURGross price for quantities from 100 pcs - 0.09 EUR
Net price for quantities from 250 pcs - 0.08 EURGross price for quantities from 250 pcs - 0.08 EUR
Net price for quantities from 500 pcs - 0.08 EURGross price for quantities from 500 pcs - 0.08 EUR
Net price for quantities from 1000 pcs - 0.07 EURGross price for quantities from 1000 pcs - 0.07 EUR
Net price for quantities from 2000 pcs - 0.07 EURGross price for quantities from 2000 pcs - 0.07 EUR
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
NXH35VB100M6.3X11 | Capacitor: electrolytic; low ESR; THT; 100uF; 35VDC; Pitch: 2.5mm
Capacitor: electrolytic; low ESR; THT; 100uF; 35VDC; Pitch: 2.5mm
Manufacturer part number: NXH35VB100M6.3X11
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.11 EURGross price for quantities from 1 pcs - 0.11 EUR
Net price for quantities from 10 pcs - 0.07 EURGross price for quantities from 10 pcs - 0.07 EUR
Net price for quantities from 25 pcs - 0.05 EURGross price for quantities from 25 pcs - 0.05 EUR
Net price for quantities from 50 pcs - 0.04 EURGross price for quantities from 50 pcs - 0.04 EUR
Net price for quantities from 100 pcs - 0.04 EURGross price for quantities from 100 pcs - 0.04 EUR
Net price for quantities from 200 pcs - 0.04 EURGross price for quantities from 200 pcs - 0.04 EUR
Net price for quantities from 400 pcs - 0.04 EURGross price for quantities from 400 pcs - 0.04 EUR
395 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
NXH25VB1000M5.0TP10X25 | Capacitor: electrolytic; low ESR; THT; 1000uF; 25VDC; Pitch: 5mm
Capacitor: electrolytic; low ESR; THT; 1000uF; 25VDC; Pitch: 5mm
Manufacturer part number: NXH25VB1000M5.0TP10X25
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.26 EURGross price for quantities from 1 pcs - 0.26 EUR
Net price for quantities from 10 pcs - 0.22 EURGross price for quantities from 10 pcs - 0.22 EUR
Net price for quantities from 50 pcs - 0.20 EURGross price for quantities from 50 pcs - 0.20 EUR
Net price for quantities from 100 pcs - 0.19 EURGross price for quantities from 100 pcs - 0.19 EUR
Net price for quantities from 250 pcs - 0.18 EURGross price for quantities from 250 pcs - 0.18 EUR
Net price for quantities from 500 pcs - 0.16 EURGross price for quantities from 500 pcs - 0.16 EUR
75 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
NXA25VB100M2.5TP6.3X11 | Capacitor: electrolytic; low ESR; THT; 100uF; 25VDC; Pitch: 2.5mm
Capacitor: electrolytic; low ESR; THT; 100uF; 25VDC; Pitch: 2.5mm
Manufacturer part number: NXA25VB100M2.5TP6.3X11
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.08 EURGross price for quantities from 1 pcs - 0.08 EUR
Net price for quantities from 10 pcs - 0.04 EURGross price for quantities from 10 pcs - 0.04 EUR
Net price for quantities from 50 pcs - 0.04 EURGross price for quantities from 50 pcs - 0.04 EUR
Net price for quantities from 100 pcs - 0.04 EURGross price for quantities from 100 pcs - 0.04 EUR
Net price for quantities from 250 pcs - 0.04 EURGross price for quantities from 250 pcs - 0.04 EUR
Net price for quantities from 500 pcs - 0.03 EURGross price for quantities from 500 pcs - 0.03 EUR
Net price for quantities from 1000 pcs - 0.03 EURGross price for quantities from 1000 pcs - 0.03 EUR
Net price for quantities from 1500 pcs - 0.03 EURGross price for quantities from 1500 pcs - 0.03 EUR
1047 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
SS1J106M05007PC | Capacitor: electrolytic; THT; 10uF; 63VDC; 5x7mm; ±20%; 2000h; SS
Capacitor: electrolytic; THT; 10uF; 63VDC; 5x7mm; ±20%; 2000h; SS
Manufacturer part number: SS1J106M05007PC
Manufacturer: SAMWHA
Net price for quantities from 10 pcs - 0.06 EURGross price for quantities from 10 pcs - 0.06 EUR
Net price for quantities from 50 pcs - 0.03 EURGross price for quantities from 50 pcs - 0.03 EUR
Net price for quantities from 100 pcs - 0.03 EURGross price for quantities from 100 pcs - 0.03 EUR
Net price for quantities from 200 pcs - 0.03 EURGross price for quantities from 200 pcs - 0.03 EUR
Net price for quantities from 400 pcs - 0.02 EURGross price for quantities from 400 pcs - 0.02 EUR
Net price for quantities from 1000 pcs - 0.02 EURGross price for quantities from 1000 pcs - 0.02 EUR
Net price for quantities from 2000 pcs - 0.02 EURGross price for quantities from 2000 pcs - 0.02 EUR
1950 in TME stock
No. of pieces (Multiplicity: 10)
Minimum order quantity: 10.
Multiplicity: 10.
NEW
MKS2D022201A00KSSD | Capacitor: polyester; 22nF; 63VDC,100VDC; 5mm; ±10%; 2.5x6.5x7.2mm
Capacitor: polyester; 22nF; 63VDC,100VDC; 5mm; ±10%; 2.5x6.5x7.2mm
Manufacturer part number: MKS2D022201A00KSSD
Manufacturer: WIMA
Net price for quantities from 10000 pcs - 0.12 EURGross price for quantities from 10000 pcs - 0.12 EUR
0 in TME stock
No. of pieces (Multiplicity: 10 000)
Minimum order quantity: 10 000.
Multiplicity: 10 000.
NEW
NXH35VB47M5X11 | Capacitor: electrolytic; low ESR; THT; 47uF; 35VDC; Pitch: 2mm; ±20%
Capacitor: electrolytic; low ESR; THT; 47uF; 35VDC; Pitch: 2mm; ±20%
Manufacturer part number: NXH35VB47M5X11
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.09 EURGross price for quantities from 1 pcs - 0.09 EUR
Net price for quantities from 10 pcs - 0.05 EURGross price for quantities from 10 pcs - 0.05 EUR
Net price for quantities from 25 pcs - 0.04 EURGross price for quantities from 25 pcs - 0.04 EUR
Net price for quantities from 50 pcs - 0.04 EURGross price for quantities from 50 pcs - 0.04 EUR
Net price for quantities from 100 pcs - 0.04 EURGross price for quantities from 100 pcs - 0.04 EUR
Net price for quantities from 200 pcs - 0.04 EURGross price for quantities from 200 pcs - 0.04 EUR
203 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
MSAST21GBB5106MTNA01 | Capacitor: ceramic; MLCC; 10uF; 25VDC; X5R; ±20%; SMD; 0805
Capacitor: ceramic; MLCC; 10uF; 25VDC; X5R; ±20%; SMD; 0805
Manufacturer part number: MSAST21GBB5106MTNA01
Manufacturer: TAIYO YUDEN
Net price for quantities from 1 pcs - 0.10 EURGross price for quantities from 1 pcs - 0.10 EUR
Net price for quantities from 10 pcs - 0.07 EURGross price for quantities from 10 pcs - 0.07 EUR
Net price for quantities from 100 pcs - 0.04 EURGross price for quantities from 100 pcs - 0.04 EUR
Net price for quantities from 500 pcs - 0.03 EURGross price for quantities from 500 pcs - 0.03 EUR
Net price for quantities from 1500 pcs - 0.03 EURGross price for quantities from 1500 pcs - 0.03 EUR
Net price for quantities from 3000 pcs - 0.03 EURGross price for quantities from 3000 pcs - 0.03 EUR
2 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
Hardly available product
NEW
WB1V108M12025PL | Capacitor: electrolytic; THT; 1000uF; 35VDC; 12.5x25mm; ±20%; 5000h
Capacitor: electrolytic; THT; 1000uF; 35VDC; 12.5x25mm; ±20%; 5000h
Manufacturer part number: WB1V108M12025PL
Manufacturer: SAMWHA
Net price for quantities from 1 pcs - 0.34 EURGross price for quantities from 1 pcs - 0.34 EUR
Net price for quantities from 10 pcs - 0.30 EURGross price for quantities from 10 pcs - 0.30 EUR
Net price for quantities from 50 pcs - 0.29 EURGross price for quantities from 50 pcs - 0.29 EUR
Net price for quantities from 100 pcs - 0.27 EURGross price for quantities from 100 pcs - 0.27 EUR
Net price for quantities from 200 pcs - 0.26 EURGross price for quantities from 200 pcs - 0.26 EUR
Net price for quantities from 400 pcs - 0.25 EURGross price for quantities from 400 pcs - 0.25 EUR
Net price for quantities from 800 pcs - 0.24 EURGross price for quantities from 800 pcs - 0.24 EUR
Net price for quantities from 1600 pcs - 0.23 EURGross price for quantities from 1600 pcs - 0.23 EUR
1242 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
NBC400VB10M10X16 | Capacitor: electrolytic; THT; 10uF; 400VDC; Pitch: 5mm; ±20%; 10000h
Capacitor: electrolytic; THT; 10uF; 400VDC; Pitch: 5mm; ±20%; 10000h
Manufacturer part number: NBC400VB10M10X16
Manufacturer: SAMYOUNG
Net price for quantities from 1 pcs - 0.31 EURGross price for quantities from 1 pcs - 0.31 EUR
Net price for quantities from 10 pcs - 0.22 EURGross price for quantities from 10 pcs - 0.22 EUR
Net price for quantities from 25 pcs - 0.19 EURGross price for quantities from 25 pcs - 0.19 EUR
Net price for quantities from 50 pcs - 0.17 EURGross price for quantities from 50 pcs - 0.17 EUR
Net price for quantities from 100 pcs - 0.16 EURGross price for quantities from 100 pcs - 0.16 EUR
14 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CC0402JRNPO9BN101 | Capacitor: ceramic; MLCC; 100pF; 50V; C0G (NP0); ±5%; SMD; 0402
Capacitor: ceramic; MLCC; 100pF; 50V; C0G (NP0); ±5%; SMD; 0402
Manufacturer part number: CC0402JRNPO9BN101
Manufacturer: YAGEO
Net price for quantities from 1 pcs - 0.02 EURGross price for quantities from 1 pcs - 0.02 EUR
Net price for quantities from 10000 pcs - 0.00 EURGross price for quantities from 10000 pcs - 0.00 EUR
Net price for quantities from 20000 pcs - 0.00 EURGross price for quantities from 20000 pcs - 0.00 EUR
Net price for quantities from 30000 pcs - 0.00 EURGross price for quantities from 30000 pcs - 0.00 EUR
Net price for quantities from 50000 pcs - 0.00 EURGross price for quantities from 50000 pcs - 0.00 EUR
Net price for quantities from 70000 pcs - 0.00 EURGross price for quantities from 70000 pcs - 0.00 EUR
Net price for quantities from 100000 pcs - 0.00 EURGross price for quantities from 100000 pcs - 0.00 EUR
Net price for quantities from 200000 pcs - 0.00 EURGross price for quantities from 200000 pcs - 0.00 EUR
Net price for quantities from 400000 pcs - 0.00 EURGross price for quantities from 400000 pcs - 0.00 EUR
Net price for quantities from 500000 pcs - 0.00 EURGross price for quantities from 500000 pcs - 0.00 EUR
60742 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
Hardly available product
NEW
CS3216X5R107M100NRI | Capacitor: ceramic; MLCC; 100uF; 10V; X5R; ±20%; SMD; 1206
Capacitor: ceramic; MLCC; 100uF; 10V; X5R; ±20%; SMD; 1206
Manufacturer part number: CS3216X5R107M100NRI
Manufacturer: SAMWHA
Net price for quantities from 1 pcs - 0.28 EURGross price for quantities from 1 pcs - 0.28 EUR
Net price for quantities from 10 pcs - 0.25 EURGross price for quantities from 10 pcs - 0.25 EUR
Net price for quantities from 100 pcs - 0.24 EURGross price for quantities from 100 pcs - 0.24 EUR
Net price for quantities from 500 pcs - 0.23 EURGross price for quantities from 500 pcs - 0.23 EUR
Net price for quantities from 1000 pcs - 0.21 EURGross price for quantities from 1000 pcs - 0.21 EUR
Net price for quantities from 2000 pcs - 0.20 EURGross price for quantities from 2000 pcs - 0.20 EUR
Net price for quantities from 4000 pcs - 0.19 EURGross price for quantities from 4000 pcs - 0.19 EUR
Net price for quantities from 10000 pcs - 0.18 EURGross price for quantities from 10000 pcs - 0.18 EUR
7699 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
Hardly available product