+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

IGBT transistors

(1 502)

IGBTs (insulated-gate bipolar transistors) belong to the group of semiconductor electronic components. They are used to control high-power currents, i.e. high voltages and/or amperages. Due to their much needed characteristics, IGBTs are used, for example, in inverters, which are powered by direct current at the input and generate alternating current at the output. IGBTs are also used in other power devices (e.g. converters, rectifiers, welders) and also in audio amplifiers and electric cars. The examples listed here are just some of the possible applications of these extremely useful electronic components.

The structure and characteristics of IGBTs

Insulated-gate bipolar transistors are electronic components with three leads. Similarly to ordinary bipolar transistors, they have a collector and an emitter, but instead of a base, IGBTs have a gate – a terminal identical to that in unipolar transistors, e.g. MOSFETs. In order to understand easily how they work, look at the equivalent circuit model of the component, i.e. its internal diagram. It shows the connected transistors: a bipolar PNP transistor and a unipolar MOSFET with an N-channel. MOSFET’s drain is connected to the bipolar transistor’s base, and the unipolar transistor’s gate and the collector and emitter of the bipolar transistor end with the outside leads.

The structure of an IGBT combines the advantages of unipolar and bipolar transistors. The first one is the simple control by applying the gate input voltage that is adequate for the emitter (approx. 4–8 V). Another advantage is its ability to conduct high-amperage currents. IGBTs have very high rated collector-emitter voltage, up to 6 kV. They are also suitable for controlling high-amperage currents, up to hundreds of amperes.

Despite their significant advantages, those components require their controlling devices to have a relatively high output current. It is connected with the need for rapid re-charging of the IGBT gate’s capacitance during high-frequency switching. The peak current may reach several amperes. However, it is a lower value than that necessary for controlling bipolar transistors with similar parameters. The IGBT current switching frequency (with proper controlling) may be as high as 30 kHz.

One of the advantages of IGBTs over widely used MOSFETs is a much lower forward voltage drop. In the case of MOSFETs the drop is small anyway, so they are often used for controlling various power receivers, e.g. LED strips. However, while conducting high-amperage currents, their internal resistance may cause high voltage drops and significant heating. IGBT voltage drops are much lower because the flowing current is bipolar.

IGBTs provide relatively prompt switching on of current circuits; however, compared to MOSFETs, switching off the current flowing through the component takes longer. Lowering voltage on an IGBT’s gate does not immediately switch it off. This phenomenon is sometimes called “the current tail”. It also limits the operating frequency of the component in the electronic circuit.

Like other electronic components, IGBTs are available as SMD (surface-mounted) or THT (through-hole technology) devices. They may also be sold as modules, i.e. systems of several IGBTs connected in parallel with additional electronic components (resistors, diodes etc.).

How to choose an IGBT for your application?

IGBT transistors have virtually identical parameters as other types of transistors. Take for instance the rated collector-emitter voltage, which specifies how high a potential difference can be applied between these leads without a breakdown and permanent damage to the semiconductor component. This parameter is expressed in volts [V]. The collector-emitter voltages for IGBTs may reach from ca. 300 V to as much as 5 kV.

Another important parameter is the collector current, i.e. the maximum average current flowing through the transistor. It is expressed in amperes [A]. Widely available IGBTs can handle currents from 1 A to 400 A. This parameter is connected to another one, known as power dissipation, expressed in watts [W], which may reach from 10 W to 2 kW. The higher the flowing current is, the higher power is dissipated as heat through the outer case. Components with bigger housings may reach higher values of dissipated power due to better heat dissipation. To increase its efficiency, passive cooling is often used. It is applied by affixing a radiator to the transistor (screwed or glued with heat-transfer glues). Another solution is an active cooling system, which is an airflow forced by a fan.

In addition to a rated collector current, manufacturers specify a peak collector current, which defines the maximum transient current that may flow through the component without causing its immediate thermal damage. IGBTs may handle up to 1 kA of peak currents.

Depending on the chosen controlling system, you should take into consideration the maximum permissible gate-emitter voltage (usually between 10 V and 30 V). In order to obtain information on the switching threshold of the selected transistor and the forward current achievable for the given conditions, you should read the specific component’s documentation. Among other things, it contains the characteristics of the relationship between the collector current and the collector-emitter voltage and gate-emitter voltage.

For adjusting a driver, an IGBT transistor’s gate charge, expressed in coulombs [C], is an important detail. Its value may vary from 6 nC to 1180 nC. It is a key parameter in terms of choosing a controlling device, which must have an adequate output current to optimally power and discharge the gate. This parameter is particularly important for high switching frequencies of the transistor.

Documentation also often contains transistors’ turn-on and turn-off delay times, which are significant for designing electronic circuits of certain types.

Products: 1 502

Warehouse:

TME
External
All
Page 1
FGH40N60SMD | Transistor: IGBT; 600V; 40A; 174W; TO247-3
Transistor: IGBT; 600V; 40A; 174W; TO247-3
Manufacturer part number: FGH40N60SMD
Manufacturer: ONSEMI
Net price for quantities from 1 pcs - 4.95 USDGross price for quantities from 1 pcs - 4.95 USD
Net price for quantities from 3 pcs - 4.21 USDGross price for quantities from 3 pcs - 4.21 USD
Net price for quantities from 10 pcs - 3.55 USDGross price for quantities from 10 pcs - 3.55 USD
Net price for quantities from 30 pcs - 3.06 USDGross price for quantities from 30 pcs - 3.06 USD
Net price for quantities from 60 pcs - 2.90 USDGross price for quantities from 60 pcs - 2.90 USD
Net price for quantities from 120 pcs - 2.81 USDGross price for quantities from 120 pcs - 2.81 USD
169 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
AOK60B65H2AL | Transistor: IGBT; 650V; 60A; 166W; TO247; Eoff: 1.17mJ; Eon: 2.36mJ
Transistor: IGBT; 650V; 60A; 166W; TO247; Eoff: 1.17mJ; Eon: 2.36mJ
Manufacturer part number: AOK60B65H2AL
Net price for quantities from 1 pcs - 2.94 USDGross price for quantities from 1 pcs - 2.94 USD
Net price for quantities from 3 pcs - 2.65 USDGross price for quantities from 3 pcs - 2.65 USD
Net price for quantities from 10 pcs - 2.33 USDGross price for quantities from 10 pcs - 2.33 USD
Net price for quantities from 90 pcs - 2.11 USDGross price for quantities from 90 pcs - 2.11 USD
Net price for quantities from 240 pcs - 1.96 USDGross price for quantities from 240 pcs - 1.96 USD
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
IKW40N120H3FKSA1 | Transistor: IGBT; 1.2kV; 80A; 483W; TO247-3; H3
Transistor: IGBT; 1.2kV; 80A; 483W; TO247-3; H3
Manufacturer part number: IKW40N120H3FKSA1
Manufacturer: INFINEON TECHNOLOGIES
Net price for quantities from 1 pcs - 6.83 USDGross price for quantities from 1 pcs - 6.83 USD
Net price for quantities from 5 pcs - 5.33 USDGross price for quantities from 5 pcs - 5.33 USD
Net price for quantities from 10 pcs - 4.78 USDGross price for quantities from 10 pcs - 4.78 USD
Net price for quantities from 30 pcs - 4.17 USDGross price for quantities from 30 pcs - 4.17 USD
Net price for quantities from 60 pcs - 4.02 USDGross price for quantities from 60 pcs - 4.02 USD
313 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
STGW40H65DFB | Transistor: IGBT; 650V; 40A; 283W; TO247-3
Transistor: IGBT; 650V; 40A; 283W; TO247-3
Manufacturer part number: STGW40H65DFB
Manufacturer: STMicroelectronics
Net price for quantities from 1 pcs - 3.10 USDGross price for quantities from 1 pcs - 3.10 USD
Net price for quantities from 2 pcs - 2.65 USDGross price for quantities from 2 pcs - 2.65 USD
Net price for quantities from 10 pcs - 2.06 USDGross price for quantities from 10 pcs - 2.06 USD
Net price for quantities from 30 pcs - 1.81 USDGross price for quantities from 30 pcs - 1.81 USD
Net price for quantities from 120 pcs - 1.72 USDGross price for quantities from 120 pcs - 1.72 USD
192 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
STGP10NC60KD | Transistor: IGBT; 600V; 10A; 65W; TO220AB
Transistor: IGBT; 600V; 10A; 65W; TO220AB
Manufacturer part number: STGP10NC60KD
Manufacturer: STMicroelectronics
Net price for quantities from 1 pcs - 1.97 USDGross price for quantities from 1 pcs - 1.97 USD
Net price for quantities from 5 pcs - 1.51 USDGross price for quantities from 5 pcs - 1.51 USD
Net price for quantities from 10 pcs - 1.32 USDGross price for quantities from 10 pcs - 1.32 USD
Net price for quantities from 25 pcs - 1.10 USDGross price for quantities from 25 pcs - 1.10 USD
Net price for quantities from 50 pcs - 0.97 USDGross price for quantities from 50 pcs - 0.97 USD
Net price for quantities from 100 pcs - 0.91 USDGross price for quantities from 100 pcs - 0.91 USD
Net price for quantities from 500 pcs - 0.87 USDGross price for quantities from 500 pcs - 0.87 USD
169 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
STGW20NC60VD | Transistor: IGBT; 600V; 30A; 200W; TO247-3
Transistor: IGBT; 600V; 30A; 200W; TO247-3
Manufacturer part number: STGW20NC60VD
Manufacturer: STMicroelectronics
Net price for quantities from 1 pcs - 3.11 USDGross price for quantities from 1 pcs - 3.11 USD
Net price for quantities from 5 pcs - 2.74 USDGross price for quantities from 5 pcs - 2.74 USD
Net price for quantities from 10 pcs - 2.56 USDGross price for quantities from 10 pcs - 2.56 USD
Net price for quantities from 15 pcs - 2.45 USDGross price for quantities from 15 pcs - 2.45 USD
Net price for quantities from 30 pcs - 2.25 USDGross price for quantities from 30 pcs - 2.25 USD
Net price for quantities from 60 pcs - 2.05 USDGross price for quantities from 60 pcs - 2.05 USD
Net price for quantities from 90 pcs - 1.98 USDGross price for quantities from 90 pcs - 1.98 USD
Net price for quantities from 120 pcs - 1.92 USDGross price for quantities from 120 pcs - 1.92 USD
Net price for quantities from 150 pcs - 1.90 USDGross price for quantities from 150 pcs - 1.90 USD
Net price for quantities from 1020 pcs - 1.77 USDGross price for quantities from 1020 pcs - 1.77 USD
2085 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
IHW30N160R5XKSA1 | Transistor: IGBT; 1.6kV; 39A; 131.5W; TO247-3
Transistor: IGBT; 1.6kV; 39A; 131.5W; TO247-3
Manufacturer part number: IHW30N160R5XKSA1
Manufacturer: INFINEON TECHNOLOGIES
Net price for quantities from 1 pcs - 3.15 USDGross price for quantities from 1 pcs - 3.15 USD
Net price for quantities from 10 pcs - 2.63 USDGross price for quantities from 10 pcs - 2.63 USD
Net price for quantities from 30 pcs - 2.45 USDGross price for quantities from 30 pcs - 2.45 USD
Net price for quantities from 120 pcs - 2.28 USDGross price for quantities from 120 pcs - 2.28 USD
96 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
SGB02N120ATMA1 | Transistor: IGBT; NPT; 1.2kV; 6.2A; 62W; D2PAK
Transistor: IGBT; NPT; 1.2kV; 6.2A; 62W; D2PAK
Manufacturer part number: SGB02N120ATMA1
Manufacturer: INFINEON TECHNOLOGIES
Net price for quantities from 1000 pcs - 1.11 USDGross price for quantities from 1000 pcs - 1.11 USD
47000 in an external stock
No. of pieces (Multiplicity: 1 000)
Minimum order quantity: 1 000.
Multiplicity: 1 000.
The offer is available for business customers only
FGH60N60SMD | Transistor: IGBT; 600V; 60A; 300W; TO247-3
Transistor: IGBT; 600V; 60A; 300W; TO247-3
Manufacturer part number: FGH60N60SMD
Manufacturer: ONSEMI
Net price for quantities from 1 pcs - 6.78 USDGross price for quantities from 1 pcs - 6.78 USD
Net price for quantities from 10 pcs - 4.49 USDGross price for quantities from 10 pcs - 4.49 USD
Net price for quantities from 30 pcs - 4.04 USDGross price for quantities from 30 pcs - 4.04 USD
Net price for quantities from 60 pcs - 3.91 USDGross price for quantities from 60 pcs - 3.91 USD
281 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
IHW30N135R5XKSA1 | Transistor: IGBT; 1.35kV; 30A; 165W; TO247-3
Transistor: IGBT; 1.35kV; 30A; 165W; TO247-3
Manufacturer part number: IHW30N135R5XKSA1
Manufacturer: INFINEON TECHNOLOGIES
Net price for quantities from 1 pcs - 4.66 USDGross price for quantities from 1 pcs - 4.66 USD
Net price for quantities from 5 pcs - 2.51 USDGross price for quantities from 5 pcs - 2.51 USD
Net price for quantities from 10 pcs - 2.38 USDGross price for quantities from 10 pcs - 2.38 USD
Net price for quantities from 30 pcs - 2.22 USDGross price for quantities from 30 pcs - 2.22 USD
Net price for quantities from 60 pcs - 2.16 USDGross price for quantities from 60 pcs - 2.16 USD
Net price for quantities from 120 pcs - 2.07 USDGross price for quantities from 120 pcs - 2.07 USD
Net price for quantities from 150 pcs - 2.05 USDGross price for quantities from 150 pcs - 2.05 USD
Net price for quantities from 300 pcs - 1.97 USDGross price for quantities from 300 pcs - 1.97 USD
520 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
AOD5B60D | Transistor: IGBT; 600V; 5A; 21.7W; TO252; Eoff: 0.04mJ; Eon: 0.14mJ
Transistor: IGBT; 600V; 5A; 21.7W; TO252; Eoff: 0.04mJ; Eon: 0.14mJ
Manufacturer part number: AOD5B60D
Net price for quantities from 1 pcs - 0.71 USDGross price for quantities from 1 pcs - 0.71 USD
Net price for quantities from 5 pcs - 0.69 USDGross price for quantities from 5 pcs - 0.69 USD
Net price for quantities from 25 pcs - 0.67 USDGross price for quantities from 25 pcs - 0.67 USD
Net price for quantities from 100 pcs - 0.64 USDGross price for quantities from 100 pcs - 0.64 USD
Net price for quantities from 500 pcs - 0.62 USDGross price for quantities from 500 pcs - 0.62 USD
4569 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
STGW60H65DFB | Transistor: IGBT; 650V; 60A; 375W; TO247-3
Transistor: IGBT; 650V; 60A; 375W; TO247-3
Manufacturer part number: STGW60H65DFB
Manufacturer: STMicroelectronics
Net price for quantities from 1 pcs - 5.14 USDGross price for quantities from 1 pcs - 5.14 USD
Net price for quantities from 3 pcs - 4.55 USDGross price for quantities from 3 pcs - 4.55 USD
Net price for quantities from 5 pcs - 4.17 USDGross price for quantities from 5 pcs - 4.17 USD
Net price for quantities from 10 pcs - 3.66 USDGross price for quantities from 10 pcs - 3.66 USD
Net price for quantities from 15 pcs - 3.37 USDGross price for quantities from 15 pcs - 3.37 USD
Net price for quantities from 30 pcs - 2.95 USDGross price for quantities from 30 pcs - 2.95 USD
Net price for quantities from 60 pcs - 2.82 USDGross price for quantities from 60 pcs - 2.82 USD
393 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
IHW30N120R5XKSA1 | Transistor: IGBT; TRENCHSTOP™ RC; 1.2kV; 30A; 165W; TO247-3
Transistor: IGBT; TRENCHSTOP™ RC; 1.2kV; 30A; 165W; TO247-3
Manufacturer part number: IHW30N120R5XKSA1
Manufacturer: INFINEON TECHNOLOGIES
Net price for quantities from 1 pcs - 3.71 USDGross price for quantities from 1 pcs - 3.71 USD
Net price for quantities from 5 pcs - 2.56 USDGross price for quantities from 5 pcs - 2.56 USD
Net price for quantities from 10 pcs - 2.31 USDGross price for quantities from 10 pcs - 2.31 USD
Net price for quantities from 30 pcs - 2.07 USDGross price for quantities from 30 pcs - 2.07 USD
Net price for quantities from 120 pcs - 1.97 USDGross price for quantities from 120 pcs - 1.97 USD
153 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
IKW50N60DTPXKSA1 | Transistor: IGBT; 600V; 61A; 159.6W; TO247-3
Transistor: IGBT; 600V; 61A; 159.6W; TO247-3
Manufacturer part number: IKW50N60DTPXKSA1
Manufacturer: INFINEON TECHNOLOGIES
Net price for quantities from 1 pcs - 3.51 USDGross price for quantities from 1 pcs - 3.51 USD
Net price for quantities from 10 pcs - 2.42 USDGross price for quantities from 10 pcs - 2.42 USD
Net price for quantities from 30 pcs - 2.04 USDGross price for quantities from 30 pcs - 2.04 USD
Net price for quantities from 120 pcs - 1.70 USDGross price for quantities from 120 pcs - 1.70 USD
Net price for quantities from 150 pcs - 1.68 USDGross price for quantities from 150 pcs - 1.68 USD
774 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
FGH40N60UFDTU | Transistor: IGBT; 600V; 40A; 116W; TO247-3
Transistor: IGBT; 600V; 40A; 116W; TO247-3
Manufacturer part number: FGH40N60UFDTU
Manufacturer: ONSEMI
Net price for quantities from 1 pcs - 3.86 USDGross price for quantities from 1 pcs - 3.86 USD
Net price for quantities from 10 pcs - 2.52 USDGross price for quantities from 10 pcs - 2.52 USD
Net price for quantities from 30 pcs - 2.16 USDGross price for quantities from 30 pcs - 2.16 USD
Net price for quantities from 120 pcs - 2.04 USDGross price for quantities from 120 pcs - 2.04 USD
75 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
STGW40V60DF | Transistor: IGBT; 600V; 80A; 283W; TO247-3
Transistor: IGBT; 600V; 80A; 283W; TO247-3
Manufacturer part number: STGW40V60DF
Manufacturer: STMicroelectronics
Net price for quantities from 1 pcs - 3.95 USDGross price for quantities from 1 pcs - 3.95 USD
Net price for quantities from 5 pcs - 2.67 USDGross price for quantities from 5 pcs - 2.67 USD
Net price for quantities from 10 pcs - 2.47 USDGross price for quantities from 10 pcs - 2.47 USD
Net price for quantities from 30 pcs - 2.25 USDGross price for quantities from 30 pcs - 2.25 USD
Net price for quantities from 120 pcs - 2.14 USDGross price for quantities from 120 pcs - 2.14 USD
399 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
IGW50N60H3FKSA1 | Transistor: IGBT; 600V; 50A; 333W; TO247-3; H3
Transistor: IGBT; 600V; 50A; 333W; TO247-3; H3
Manufacturer part number: IGW50N60H3FKSA1
Manufacturer: INFINEON TECHNOLOGIES
Net price for quantities from 1 pcs - 3.27 USDGross price for quantities from 1 pcs - 3.27 USD
Net price for quantities from 5 pcs - 2.98 USDGross price for quantities from 5 pcs - 2.98 USD
Net price for quantities from 10 pcs - 2.81 USDGross price for quantities from 10 pcs - 2.81 USD
Net price for quantities from 30 pcs - 2.52 USDGross price for quantities from 30 pcs - 2.52 USD
Net price for quantities from 120 pcs - 2.21 USDGross price for quantities from 120 pcs - 2.21 USD
Net price for quantities from 150 pcs - 2.16 USDGross price for quantities from 150 pcs - 2.16 USD
Net price for quantities from 300 pcs - 2.00 USDGross price for quantities from 300 pcs - 2.00 USD
Net price for quantities from 510 pcs - 1.91 USDGross price for quantities from 510 pcs - 1.91 USD
Net price for quantities from 1020 pcs - 1.84 USDGross price for quantities from 1020 pcs - 1.84 USD
14 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
FGD5T120SH | Transistor: IGBT; 1.2kV; 5A; 28W; DPAK; Features: logic level; ESD
Transistor: IGBT; 1.2kV; 5A; 28W; DPAK; Features: logic level; ESD
Manufacturer part number: FGD5T120SH
Manufacturer: ONSEMI
Net price for quantities from 1 pcs - 2.23 USDGross price for quantities from 1 pcs - 2.23 USD
Net price for quantities from 10 pcs - 1.43 USDGross price for quantities from 10 pcs - 1.43 USD
Net price for quantities from 100 pcs - 0.99 USDGross price for quantities from 100 pcs - 0.99 USD
Net price for quantities from 250 pcs - 0.95 USDGross price for quantities from 250 pcs - 0.95 USD
2485 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
FGA60N65SMD | Transistor: IGBT; 650V; 60A; 300W; TO3PN
Transistor: IGBT; 650V; 60A; 300W; TO3PN
Manufacturer part number: FGA60N65SMD
Manufacturer: ONSEMI
Net price for quantities from 1 pcs - 5.64 USDGross price for quantities from 1 pcs - 5.64 USD
Net price for quantities from 3 pcs - 5.13 USDGross price for quantities from 3 pcs - 5.13 USD
Net price for quantities from 10 pcs - 4.35 USDGross price for quantities from 10 pcs - 4.35 USD
Net price for quantities from 30 pcs - 3.67 USDGross price for quantities from 30 pcs - 3.67 USD
Net price for quantities from 60 pcs - 3.55 USDGross price for quantities from 60 pcs - 3.55 USD
58 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
FGH40N60SFDTU | Transistor: IGBT; 600V; 40A; 116W; TO247-3
Transistor: IGBT; 600V; 40A; 116W; TO247-3
Manufacturer part number: FGH40N60SFDTU
Manufacturer: ONSEMI
Net price for quantities from 1 pcs - 4.79 USDGross price for quantities from 1 pcs - 4.79 USD
Net price for quantities from 3 pcs - 4.28 USDGross price for quantities from 3 pcs - 4.28 USD
Net price for quantities from 10 pcs - 3.48 USDGross price for quantities from 10 pcs - 3.48 USD
Net price for quantities from 30 pcs - 2.80 USDGross price for quantities from 30 pcs - 2.80 USD
Net price for quantities from 60 pcs - 2.71 USDGross price for quantities from 60 pcs - 2.71 USD
119 in TME stock