+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Ring ferrites

(677)

Ring ferrites belong to the family of ferrite filters, also known as ferrite cores. These filters come in a variety of sizes and shapes, such as cylinders with a hole along their axis of rotation, or the previously mentioned rings. They are often found at the ends of various types of cables and wires, e.g. computer mice, switching power supplies, or USB cables, sometimes even on both sides, near the plugs, and thus close to the input and output ‘to’ and ‘from’ a particular device.

How do ring ferrites work?

Ferrite filters, in the simplest of terms, serve to supress, in both directions, high-frequency interference. Their operation does not differ much from commonly used chokes or inductors. In their applications, ferrites are characterised primarily by impedance, but indirectly they can introduce a kind of capacitance and also resistance into the circuit. Applied to both DC and AC conductors, they act as a low-pass filters, suppressing interference at higher frequencies, and in fact dissipating their energy by converting it into thermal energy, which is then given off to the environment. Interference can be the result of e.g. electromagnetic influence of another device or electronic circuit located near the output signal. Such a situation is typical e.g. for switching-mode power supplies, due to the specific nature of their operation and switching currents at high frequency. This interference is referred to as electromagnetic interference, the so-called EMI or RFI (radio-frequency interference) noise. A current flowing through a conductor, according to Ampère's law, creates a magnetic field around it. In the case of current interference, this field is not constant and is subject to fluctuations, which then interact with the ferrite filter. This, in turn, suppresses the electrical signal interference that arises in the conductor.

In simple terms, as the interference frequency increases, the impedance of the conductor on which the ferrite core is embedded increases. However, this is only half true. Ferrites have frequency characteristics that show for which oscillating voltage frequency values they have the highest impedance. After passing a certain frequency value, however, their impedance begins to decrease again. When selecting a suitable ring ferrite, it is extremely important to choose one whose impedance value is the highest for the interference frequencies of our system. To find them, and at the same time to choose a suitable filter, experiments and tests can be carried out, e.g. by using frequency analysis, otherwise known as spectrum analysis.

Choosing ring ferrites – what to look for?

When designing an electronic circuit in which we want to use a ring ferrite, its heating must be taken into account. It is therefore necessary to provide adequate passive or active cooling using forced air circulation, e.g. by a fan. High current values and large interference at high frequencies will not only cause a significant amount of heat to be emitted, but may also lead to the saturation of the ferrite core, i.e. a drop in its inductance by as much as 90%.

Ring ferrites application

Ferrite cores are a simple and inexpensive way to apply low-pass filtering to an already existing cable infrastructure, for example by creating a choke, or in other words, an inductor. In the case of ring ferrites it is sufficient to wrap a conductor several (typically 5 to 7) times through the centre around the ring to provide adequate filtering against high-frequency interference.

Ring ferrites can be found in outdoor cabling, but ferrite filters are just as often found inside various types of equipment, e.g. in the form of ferrite beads or chokes, as filters for incoming power, but also to filter signals directly on PCBs, near transistors, microprocessors and other integrated circuits, as well as connectors.

The application of ferrite filters is also useful in the case of devices that may emit radio frequency energy, because in such a case the cable may behave like an antenna, so the signal transmitted through will be distorted. Such a phenomenon may lead to unpredictable behaviour of powered devices. The same may occur for signal cables, which can cause distortions in communication between integrated circuits.

When selecting a ring ferrite, you should pay attention to several factors, depending on the specific application, currents flowing through the conductor, as well as the space available, e.g. in the housing of a given device. The dimensions of the filter can be taken into account, including the internal opening, which should allow for winding a wire of a given diameter through its centre several times, the material of the core, which will translate into its frequency characteristics, and the inductance factor. Before selecting a ferrite core, it is also worth reading its detailed technical documentation provided by the manufacturer, which will contain all the most important information, along with the aforementioned characteristics.

Products: 677

Warehouse:

TME
External
All
Page 1
B64290L0618X830 | Ferrite: toroidal; L: 10mm; Øint: 14.8mm; Øout: 25.3mm; N30; 4620nH
Ferrite: toroidal; L: 10mm; Øint: 14.8mm; Øout: 25.3mm; N30; 4620nH
Manufacturer part number: B64290L0618X830
Manufacturer: TDK
Net price for quantities from 1 pcs - 1.50 EURGross price for quantities from 1 pcs - 1.50 EUR
Net price for quantities from 5 pcs - 1.21 EURGross price for quantities from 5 pcs - 1.21 EUR
Net price for quantities from 10 pcs - 1.08 EURGross price for quantities from 10 pcs - 1.08 EUR
Net price for quantities from 25 pcs - 0.91 EURGross price for quantities from 25 pcs - 0.91 EUR
Net price for quantities from 50 pcs - 0.78 EURGross price for quantities from 50 pcs - 0.78 EUR
Net price for quantities from 100 pcs - 0.67 EURGross price for quantities from 100 pcs - 0.67 EUR
Net price for quantities from 250 pcs - 0.52 EURGross price for quantities from 250 pcs - 0.52 EUR
Net price for quantities from 500 pcs - 0.42 EURGross price for quantities from 500 pcs - 0.42 EUR
Net price for quantities from 1000 pcs - 0.34 EURGross price for quantities from 1000 pcs - 0.34 EUR
Net price for quantities from 2000 pcs - 0.33 EURGross price for quantities from 2000 pcs - 0.33 EUR
2348 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
5943002701 | Ferrite: toroidal; 43; -55÷90°C; 885nH; 35.5x23x12.7mm
Ferrite: toroidal; 43; -55÷90°C; 885nH; 35.5x23x12.7mm
Manufacturer part number: 5943002701
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 3.16 EURGross price for quantities from 1 pcs - 3.16 EUR
Net price for quantities from 5 pcs - 2.55 EURGross price for quantities from 5 pcs - 2.55 EUR
Net price for quantities from 10 pcs - 2.37 EURGross price for quantities from 10 pcs - 2.37 EUR
Net price for quantities from 25 pcs - 2.10 EURGross price for quantities from 25 pcs - 2.10 EUR
Net price for quantities from 53 pcs - 1.91 EURGross price for quantities from 53 pcs - 1.91 EUR
Net price for quantities from 106 pcs - 1.78 EURGross price for quantities from 106 pcs - 1.78 EUR
499 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T130-2 | Ferrite: toroidal; L: 11.1mm; Øint: 19.8mm; Øout: 33mm; iron powder
Ferrite: toroidal; L: 11.1mm; Øint: 19.8mm; Øout: 33mm; iron powder
Manufacturer part number: T130-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 2.66 EURGross price for quantities from 1 pcs - 2.66 EUR
Net price for quantities from 5 pcs - 2.20 EURGross price for quantities from 5 pcs - 2.20 EUR
Net price for quantities from 25 pcs - 1.91 EURGross price for quantities from 25 pcs - 1.91 EUR
Net price for quantities from 50 pcs - 1.84 EURGross price for quantities from 50 pcs - 1.84 EUR
Net price for quantities from 100 pcs - 1.79 EURGross price for quantities from 100 pcs - 1.79 EUR
Net price for quantities from 250 pcs - 1.76 EURGross price for quantities from 250 pcs - 1.76 EUR
Net price for quantities from 500 pcs - 1.74 EURGross price for quantities from 500 pcs - 1.74 EUR
Net price for quantities from 1000 pcs - 1.71 EURGross price for quantities from 1000 pcs - 1.71 EUR
125 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T106-2 | Ferrite: toroidal; L: 11.1mm; Øint: 14.5mm; Øout: 26.9mm; 13.5nH
Ferrite: toroidal; L: 11.1mm; Øint: 14.5mm; Øout: 26.9mm; 13.5nH
Manufacturer part number: T106-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 2.08 EURGross price for quantities from 1 pcs - 2.08 EUR
Net price for quantities from 5 pcs - 1.63 EURGross price for quantities from 5 pcs - 1.63 EUR
Net price for quantities from 25 pcs - 1.38 EURGross price for quantities from 25 pcs - 1.38 EUR
Net price for quantities from 140 pcs - 1.25 EURGross price for quantities from 140 pcs - 1.25 EUR
1418 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
B64290L0048X830 | Ferrite: toroidal; L: 12.5mm; Øint: 20.5mm; Øout: 34mm; N30; 5460nH
Ferrite: toroidal; L: 12.5mm; Øint: 20.5mm; Øout: 34mm; N30; 5460nH
Manufacturer part number: B64290L0048X830
Manufacturer: TDK
Net price for quantities from 1 pcs - 3.03 EURGross price for quantities from 1 pcs - 3.03 EUR
Net price for quantities from 10 pcs - 2.62 EURGross price for quantities from 10 pcs - 2.62 EUR
Net price for quantities from 25 pcs - 2.27 EURGross price for quantities from 25 pcs - 2.27 EUR
Net price for quantities from 40 pcs - 2.08 EURGross price for quantities from 40 pcs - 2.08 EUR
Net price for quantities from 50 pcs - 2.00 EURGross price for quantities from 50 pcs - 2.00 EUR
Net price for quantities from 100 pcs - 1.80 EURGross price for quantities from 100 pcs - 1.80 EUR
Net price for quantities from 200 pcs - 1.65 EURGross price for quantities from 200 pcs - 1.65 EUR
Net price for quantities from 300 pcs - 1.58 EURGross price for quantities from 300 pcs - 1.58 EUR
Net price for quantities from 500 pcs - 1.52 EURGross price for quantities from 500 pcs - 1.52 EUR
Net price for quantities from 800 pcs - 1.48 EURGross price for quantities from 800 pcs - 1.48 EUR
1611 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T184-26 | Ferrite: toroidal; L: 18mm; Øint: 24.1mm; Øout: 46.7mm; iron powder
Ferrite: toroidal; L: 18mm; Øint: 24.1mm; Øout: 46.7mm; iron powder
Manufacturer part number: T184-26
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 3.79 EURGross price for quantities from 1 pcs - 3.79 EUR
Net price for quantities from 5 pcs - 3.15 EURGross price for quantities from 5 pcs - 3.15 EUR
Net price for quantities from 10 pcs - 2.92 EURGross price for quantities from 10 pcs - 2.92 EUR
Net price for quantities from 20 pcs - 2.81 EURGross price for quantities from 20 pcs - 2.81 EUR
Net price for quantities from 40 pcs - 2.74 EURGross price for quantities from 40 pcs - 2.74 EUR
Net price for quantities from 60 pcs - 2.70 EURGross price for quantities from 60 pcs - 2.70 EUR
Net price for quantities from 100 pcs - 2.65 EURGross price for quantities from 100 pcs - 2.65 EUR
Net price for quantities from 200 pcs - 2.63 EURGross price for quantities from 200 pcs - 2.63 EUR
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T106-26 | Ferrite: toroidal; L: 11.1mm; Øint: 14.5mm; Øout: 26.9mm; 93nH
Ferrite: toroidal; L: 11.1mm; Øint: 14.5mm; Øout: 26.9mm; 93nH
Manufacturer part number: T106-26
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 1.38 EURGross price for quantities from 1 pcs - 1.38 EUR
Net price for quantities from 5 pcs - 1.16 EURGross price for quantities from 5 pcs - 1.16 EUR
Net price for quantities from 10 pcs - 1.06 EURGross price for quantities from 10 pcs - 1.06 EUR
Net price for quantities from 25 pcs - 1.00 EURGross price for quantities from 25 pcs - 1.00 EUR
Net price for quantities from 70 pcs - 0.95 EURGross price for quantities from 70 pcs - 0.95 EUR
Net price for quantities from 140 pcs - 0.93 EURGross price for quantities from 140 pcs - 0.93 EUR
Net price for quantities from 420 pcs - 0.92 EURGross price for quantities from 420 pcs - 0.92 EUR
1278 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
5943003801 | Ferrite: toroidal; 43; -55÷90°C; 1075nH; 61x35.55x12.7mm
Ferrite: toroidal; 43; -55÷90°C; 1075nH; 61x35.55x12.7mm
Manufacturer part number: 5943003801
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 9.94 EURGross price for quantities from 1 pcs - 9.94 EUR
Net price for quantities from 20 pcs - 8.32 EURGross price for quantities from 20 pcs - 8.32 EUR
Net price for quantities from 40 pcs - 7.49 EURGross price for quantities from 40 pcs - 7.49 EUR
Net price for quantities from 60 pcs - 6.66 EURGross price for quantities from 60 pcs - 6.66 EUR
Net price for quantities from 80 pcs - 5.82 EURGross price for quantities from 80 pcs - 5.82 EUR
Net price for quantities from 100 pcs - 5.49 EURGross price for quantities from 100 pcs - 5.49 EUR
20 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T50-2 | Ferrite: toroidal; L: 4.83mm; Øint: 7.7mm; Øout: 12.7mm; iron powder
Ferrite: toroidal; L: 4.83mm; Øint: 7.7mm; Øout: 12.7mm; iron powder
Manufacturer part number: T50-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 0.78 EURGross price for quantities from 1 pcs - 0.78 EUR
Net price for quantities from 10 pcs - 0.51 EURGross price for quantities from 10 pcs - 0.51 EUR
Net price for quantities from 50 pcs - 0.47 EURGross price for quantities from 50 pcs - 0.47 EUR
Net price for quantities from 100 pcs - 0.43 EURGross price for quantities from 100 pcs - 0.43 EUR
Net price for quantities from 500 pcs - 0.41 EURGross price for quantities from 500 pcs - 0.41 EUR
Net price for quantities from 1000 pcs - 0.40 EURGross price for quantities from 1000 pcs - 0.40 EUR
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T130-26 | Ferrite: toroidal; L: 11.1mm; Øint: 19.8mm; Øout: 33mm; iron powder
Ferrite: toroidal; L: 11.1mm; Øint: 19.8mm; Øout: 33mm; iron powder
Manufacturer part number: T130-26
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 1.47 EURGross price for quantities from 1 pcs - 1.47 EUR
Net price for quantities from 5 pcs - 1.28 EURGross price for quantities from 5 pcs - 1.28 EUR
Net price for quantities from 25 pcs - 1.13 EURGross price for quantities from 25 pcs - 1.13 EUR
Net price for quantities from 100 pcs - 1.04 EURGross price for quantities from 100 pcs - 1.04 EUR
323 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T106-52 | Ferrite: toroidal; L: 11.1mm; Øint: 14.5mm; Øout: 26.9mm; 95nH
Ferrite: toroidal; L: 11.1mm; Øint: 14.5mm; Øout: 26.9mm; 95nH
Manufacturer part number: T106-52
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 1.28 EURGross price for quantities from 1 pcs - 1.28 EUR
Net price for quantities from 5 pcs - 1.06 EURGross price for quantities from 5 pcs - 1.06 EUR
Net price for quantities from 10 pcs - 1.00 EURGross price for quantities from 10 pcs - 1.00 EUR
Net price for quantities from 30 pcs - 0.94 EURGross price for quantities from 30 pcs - 0.94 EUR
Net price for quantities from 70 pcs - 0.91 EURGross price for quantities from 70 pcs - 0.91 EUR
Net price for quantities from 140 pcs - 0.90 EURGross price for quantities from 140 pcs - 0.90 EUR
Net price for quantities from 280 pcs - 0.89 EURGross price for quantities from 280 pcs - 0.89 EUR
90 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T157-2 | Ferrite: toroidal; L: 14.5mm; Øint: 24.1mm; Øout: 39.9mm; 14nH
Ferrite: toroidal; L: 14.5mm; Øint: 24.1mm; Øout: 39.9mm; 14nH
Manufacturer part number: T157-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 4.88 EURGross price for quantities from 1 pcs - 4.88 EUR
Net price for quantities from 5 pcs - 4.19 EURGross price for quantities from 5 pcs - 4.19 EUR
Net price for quantities from 10 pcs - 3.84 EURGross price for quantities from 10 pcs - 3.84 EUR
Net price for quantities from 30 pcs - 3.61 EURGross price for quantities from 30 pcs - 3.61 EUR
Net price for quantities from 60 pcs - 3.53 EURGross price for quantities from 60 pcs - 3.53 EUR
Net price for quantities from 120 pcs - 3.48 EURGross price for quantities from 120 pcs - 3.48 EUR
Net price for quantities from 240 pcs - 3.44 EURGross price for quantities from 240 pcs - 3.44 EUR
192 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
MS-157060-2 | Ferrite: toroidal; L: 15mm; Øint: 24mm; Øout: 40mm; sendust; 81nH
Ferrite: toroidal; L: 15mm; Øint: 24mm; Øout: 40mm; sendust; 81nH
Manufacturer part number: MS-157060-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 2.25 EURGross price for quantities from 1 pcs - 2.25 EUR
Net price for quantities from 5 pcs - 1.94 EURGross price for quantities from 5 pcs - 1.94 EUR
Net price for quantities from 10 pcs - 1.78 EURGross price for quantities from 10 pcs - 1.78 EUR
Net price for quantities from 36 pcs - 1.63 EURGross price for quantities from 36 pcs - 1.63 EUR
Net price for quantities from 72 pcs - 1.57 EURGross price for quantities from 72 pcs - 1.57 EUR
Net price for quantities from 108 pcs - 1.55 EURGross price for quantities from 108 pcs - 1.55 EUR
Net price for quantities from 216 pcs - 1.54 EURGross price for quantities from 216 pcs - 1.54 EUR
Net price for quantities from 432 pcs - 1.53 EURGross price for quantities from 432 pcs - 1.53 EUR
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
B64290L0618X087 | Ferrite: toroidal; L: 10mm; Øint: 14.8mm; Øout: 25.3mm; N87; 2360nH
Ferrite: toroidal; L: 10mm; Øint: 14.8mm; Øout: 25.3mm; N87; 2360nH
Manufacturer part number: B64290L0618X087
Manufacturer: TDK
Net price for quantities from 1 pcs - 1.76 EURGross price for quantities from 1 pcs - 1.76 EUR
Net price for quantities from 10 pcs - 1.39 EURGross price for quantities from 10 pcs - 1.39 EUR
Net price for quantities from 25 pcs - 1.07 EURGross price for quantities from 25 pcs - 1.07 EUR
Net price for quantities from 50 pcs - 0.86 EURGross price for quantities from 50 pcs - 0.86 EUR
Net price for quantities from 100 pcs - 0.79 EURGross price for quantities from 100 pcs - 0.79 EUR
Net price for quantities from 500 pcs - 0.75 EURGross price for quantities from 500 pcs - 0.75 EUR
194 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
TX36/23/15-3E25 | Ferrite: toroidal; Øint: 22.7mm; Øout: 36.2mm; 3E25; 7390nH; H: 14mm
Ferrite: toroidal; Øint: 22.7mm; Øout: 36.2mm; 3E25; 7390nH; H: 14mm
Manufacturer part number: TX36/23/15-3E25
Manufacturer: FERROXCUBE
Net price for quantities from 1 pcs - 2.99 EURGross price for quantities from 1 pcs - 2.99 EUR
Net price for quantities from 10 pcs - 2.01 EURGross price for quantities from 10 pcs - 2.01 EUR
Net price for quantities from 50 pcs - 1.72 EURGross price for quantities from 50 pcs - 1.72 EUR
Net price for quantities from 140 pcs - 1.61 EURGross price for quantities from 140 pcs - 1.61 EUR
Net price for quantities from 560 pcs - 1.50 EURGross price for quantities from 560 pcs - 1.50 EUR
233 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T25X12X15 | Ferrite: toroidal; L: 12mm; Øint: 15mm; Øout: 25mm; TF
Ferrite: toroidal; L: 12mm; Øint: 15mm; Øout: 25mm; TF
Manufacturer part number: T25X12X15
Manufacturer: FERROCORE
Net price for quantities from 5 pcs - 0.78 EURGross price for quantities from 5 pcs - 0.78 EUR
Net price for quantities from 25 pcs - 0.63 EURGross price for quantities from 25 pcs - 0.63 EUR
Net price for quantities from 100 pcs - 0.48 EURGross price for quantities from 100 pcs - 0.48 EUR
Net price for quantities from 500 pcs - 0.35 EURGross price for quantities from 500 pcs - 0.35 EUR
Net price for quantities from 2000 pcs - 0.32 EURGross price for quantities from 2000 pcs - 0.32 EUR
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 5.
Multiple of: 1.
RT-310-190-70 | Ferrite: toroidal; L: 7mm; Øint: 19mm; Øout: 31mm; K5B; 35Ω
Ferrite: toroidal; L: 7mm; Øint: 19mm; Øout: 31mm; K5B; 35Ω
Manufacturer part number: RT-310-190-70
Manufacturer: RICHCO
Net price for quantities from 1 pcs - 1.46 EURGross price for quantities from 1 pcs - 1.46 EUR
Net price for quantities from 5 pcs - 1.01 EURGross price for quantities from 5 pcs - 1.01 EUR
Net price for quantities from 25 pcs - 0.87 EURGross price for quantities from 25 pcs - 0.87 EUR
Net price for quantities from 40 pcs - 0.82 EURGross price for quantities from 40 pcs - 0.82 EUR
2 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T41X15X27 | Ferrite: toroidal; L: 15mm; Øint: 27mm; Øout: 41mm; TF
Ferrite: toroidal; L: 15mm; Øint: 27mm; Øout: 41mm; TF
Manufacturer part number: T41X15X27
Manufacturer: FERROCORE
Net price for quantities from 1 pcs - 1.45 EURGross price for quantities from 1 pcs - 1.45 EUR
Net price for quantities from 5 pcs - 1.29 EURGross price for quantities from 5 pcs - 1.29 EUR
Net price for quantities from 25 pcs - 1.23 EURGross price for quantities from 25 pcs - 1.23 EUR
Net price for quantities from 100 pcs - 1.09 EURGross price for quantities from 100 pcs - 1.09 EUR
Net price for quantities from 500 pcs - 0.99 EURGross price for quantities from 500 pcs - 0.99 EUR
616 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
TX42/26/13-3E25 | Ferrite: toroidal; Øint: 25.9mm; Øout: 42.1mm; 3E25; 6425nH; H: 13mm
Ferrite: toroidal; Øint: 25.9mm; Øout: 42.1mm; 3E25; 6425nH; H: 13mm
Manufacturer part number: TX42/26/13-3E25
Manufacturer: FERROXCUBE
Net price for quantities from 1 pcs - 3.58 EURGross price for quantities from 1 pcs - 3.58 EUR
Net price for quantities from 5 pcs - 3.06 EURGross price for quantities from 5 pcs - 3.06 EUR
Net price for quantities from 28 pcs - 2.81 EURGross price for quantities from 28 pcs - 2.81 EUR
Net price for quantities from 140 pcs - 2.64 EURGross price for quantities from 140 pcs - 2.64 EUR
Net price for quantities from 280 pcs - 2.59 EURGross price for quantities from 280 pcs - 2.59 EUR
253 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
T31X16X19 | Ferrite: toroidal; L: 16mm; Øint: 19mm; Øout: 31mm; TF
Ferrite: toroidal; L: 16mm; Øint: 19mm; Øout: 31mm; TF
Manufacturer part number: T31X16X19
Manufacturer: FERROCORE
Net price for quantities from 1 pcs - 1.37 EURGross price for quantities from 1 pcs - 1.37 EUR
Net price for quantities from 5 pcs - 0.95 EURGross price for quantities from 5 pcs - 0.95 EUR
Net price for quantities from 10 pcs - 0.84 EURGross price for quantities from 10 pcs - 0.84 EUR
Net price for quantities from 40 pcs - 0.72 EURGross price for quantities from 40 pcs - 0.72 EUR
Net price for quantities from 80 pcs - 0.66 EURGross price for quantities from 80 pcs - 0.66 EUR
Net price for quantities from 120 pcs - 0.64 EURGross price for quantities from 120 pcs - 0.64 EUR
Net price for quantities from 200 pcs - 0.63 EURGross price for quantities from 200 pcs - 0.63 EUR
Net price for quantities from 320 pcs - 0.61 EURGross price for quantities from 320 pcs - 0.61 EUR
Net price for quantities from 640 pcs - 0.61 EURGross price for quantities from 640 pcs - 0.61 EUR
495 in TME stock