Mechanical components

60 986 products
Browse by

In the process of designing and manufacturing of electronic circuits, it is very important to use appropriate mechanical components in order to ensure that the individual elements fit one another, and the installation of a device in its designated place and its operation are easy and convenient. The use of safety components – both for the protection of user and of the circuit itself – is just as important. With properly selected mechanical parts, we can significantly improve the service life and functionality of the designed devices.

Mechanical components available from TME

There are over 15 thousand mechanical components available from TME, useful for the construction of various devices. Among them, you can find basic engineering components, such as bolts, screws, nuts, threaded washers and inserts. Various securing and fixing components, spacers, as well as guides, handles, and clamps can help stabilize the installation. Mounting in the target location will be easier with the use of such mechanical components as hinges and feet. The mobility of the whole device and its individual parts is guaranteed by the properly selected handles and wheels, and bearings, which prove indispensable in many applications. Seals will ensure tight connections, while end caps will protect spare openings and outlets. Knobs and clamping levers will ensure easy use of the device, while locks will limit access to authorised users only. The wide selection of mechanical components makes it possible to choose the appropriate equipment for various projects. Installation stability, as well as the ease and safety of use are factors that always have to be taken into account.