مكثفات

(128 839)

A capacitor is one of the basic passive electronic components. Its task is to store energy in the electric field. The amount of stored energy is described by the capacitance of the capacitor, which is expressed in farads (F). The capacitance measured in full farads is not very common. Typically, capacitors have the capacitance of micro- (µ), nano- (n), pico- (p) farads.
The second basic parameter of a capacitor, apart from its capacitance, is its maximum operating voltage. Due to its design, a capacitor is susceptible to the so-called breakdown. Therefore, each capacitor has a parameter that defines the maximum voltage that can appear between its terminals. After exceeding it, a breakdown may occur, resulting in a short-circuit of the capacitor.

Capacitor – design and principle of operation

Capacitors are made of two conductors (capacitor plates) separated from each other by a non-conductive dielectric material. It can be any insulating material such as: air, plastic, ceramics, paper. The operation of a capacitor is based on Coulomb's law. According to that law, the media on both plates of the capacitor interact with each other. Media with the same charge repel each other, while those with the opposite charge attract each other. The effect of such a phenomenon is the presence of opposite charges on the capacitor plates. Their number is equal on both sides. Thanks to the dielectric material contained between the plates, the flow of charges is impossible, and this results in the formation of an electric field.

Types of capacitors

There are many different types of capacitors available on the market, including customized designs for specific tasks. Some of the types of capacitors available at TME are described below. Ceramic capacitors and MLCCs – these are some of the most common electronic components. What is interesting, the number of such capacitors manufactured in a single year is about one trillion. Ceramic capacitors owe their name to the ceramics used as an insulating material. MLCCs (multi-layer ceramic capacitors) are a subtype of conventional ceramic capacitors. An MLCC is a ceramic capacitor made in a multi-layer process. Ceramic capacitors do not have a specific polarisation, so they can be used in AC circuits, they are also available in both THT (through-hole mounting) and SMD (surface mounting) versions.

Electrolytic capacitors – the second most common type of capacitors are electrolytic designs. Thanks to the use of electrolyte, they offer much larger capacitance than ceramic capacitors. Almost all of them require appropriate polarisation – incorrect incorporation of such a capacitor into a circuit may even result in its explosion. These capacitors are also available in THT and SMD versions.

Trimmer – it is a variable capacitor, also called a tuning capacitor or tuning condenser. As the name suggests, the capacitance of such a capacitor can be freely adjusted. Trimmers were used in older designs of radios. At TME, several modern SMD trimmers are available.

Supercapacitors – they are a type of electrolytic capacitors and are able to store huge amounts of energy. Thanks to a special design, their capacitance reaches up to 3kF. In practice, it can be said that supercapacitors combine features of conventional capacitors and rechargeable batteries. Charging speed is their great advantage.

منتجات: 128 839

المستودع:

TME
خارجي
الكل
الصفحة 1
JFX-3.3U/250 | Capacitor: polypropylene; 3.3uF; 250VDC; ±5%; Ø17.5x31.5mm; THT
Capacitor: polypropylene; 3.3uF; 250VDC; ±5%; Ø17.5x31.5mm; THT
رمز الشركة المصنعة: JFX-3.3U/250
الشركة المصنعة: Jb Capacitors
السعر الصافي للكميات من 1 pcs - 1.74 EURالسعر الإجمالي للكميات من 1 pcs - 1.74 EUR
السعر الصافي للكميات من 5 pcs - 1.61 EURالسعر الإجمالي للكميات من 5 pcs - 1.61 EUR
السعر الصافي للكميات من 25 pcs - 1.39 EURالسعر الإجمالي للكميات من 25 pcs - 1.39 EUR
السعر الصافي للكميات من 100 pcs - 1.24 EURالسعر الإجمالي للكميات من 100 pcs - 1.24 EUR
481 في مستودع TME
عدد القطع (المضاعف: 1)
0805B104K500CT | Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0805
Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0805
رمز الشركة المصنعة: 0805B104K500CT
الشركة المصنعة: WALSIN
السعر الصافي للكميات من 1 pcs - 0.09 EURالسعر الإجمالي للكميات من 1 pcs - 0.09 EUR
السعر الصافي للكميات من 10 pcs - 0.06 EURالسعر الإجمالي للكميات من 10 pcs - 0.06 EUR
السعر الصافي للكميات من 100 pcs - 0.03 EURالسعر الإجمالي للكميات من 100 pcs - 0.03 EUR
السعر الصافي للكميات من 1000 pcs - 0.01 EURالسعر الإجمالي للكميات من 1000 pcs - 0.01 EUR
السعر الصافي للكميات من 4000 pcs - 0.01 EURالسعر الإجمالي للكميات من 4000 pcs - 0.01 EUR
16887503 في مستودع TME
عدد القطع (المضاعف: 1)
المنتج قليل التوفر
JFX-2.2U/250 | Capacitor: polypropylene; 2.2uF; 250VDC; ±5%; Ø14.5x31.5mm; THT
Capacitor: polypropylene; 2.2uF; 250VDC; ±5%; Ø14.5x31.5mm; THT
رمز الشركة المصنعة: JFX-2.2U/250
الشركة المصنعة: Jb Capacitors
السعر الصافي للكميات من 1 pcs - 1.58 EURالسعر الإجمالي للكميات من 1 pcs - 1.58 EUR
السعر الصافي للكميات من 5 pcs - 1.46 EURالسعر الإجمالي للكميات من 5 pcs - 1.46 EUR
السعر الصافي للكميات من 25 pcs - 1.35 EURالسعر الإجمالي للكميات من 25 pcs - 1.35 EUR
السعر الصافي للكميات من 100 pcs - 1.21 EURالسعر الإجمالي للكميات من 100 pcs - 1.21 EUR
219 في مستودع TME
عدد القطع (المضاعف: 1)
UFW1H101MPD | Capacitor: electrolytic; THT; 100uF; 50VDC; Ø8x11.5mm; Pitch: 3.5mm
Capacitor: electrolytic; THT; 100uF; 50VDC; Ø8x11.5mm; Pitch: 3.5mm
رمز الشركة المصنعة: UFW1H101MPD
الشركة المصنعة: NICHICON
السعر الصافي للكميات من 1 pcs - 0.33 EURالسعر الإجمالي للكميات من 1 pcs - 0.33 EUR
السعر الصافي للكميات من 5 pcs - 0.27 EURالسعر الإجمالي للكميات من 5 pcs - 0.27 EUR
السعر الصافي للكميات من 10 pcs - 0.22 EURالسعر الإجمالي للكميات من 10 pcs - 0.22 EUR
السعر الصافي للكميات من 15 pcs - 0.19 EURالسعر الإجمالي للكميات من 15 pcs - 0.19 EUR
السعر الصافي للكميات من 50 pcs - 0.13 EURالسعر الإجمالي للكميات من 50 pcs - 0.13 EUR
السعر الصافي للكميات من 100 pcs - 0.12 EURالسعر الإجمالي للكميات من 100 pcs - 0.12 EUR
السعر الصافي للكميات من 200 pcs - 0.11 EURالسعر الإجمالي للكميات من 200 pcs - 0.11 EUR
876 في مستودع TME
عدد القطع (المضاعف: 1)
TAJB106K016RNJ | Capacitor: tantalum; 10uF; 16VDC; SMD; B; 1411; ±10%; -55÷125°C; TAJ
Capacitor: tantalum; 10uF; 16VDC; SMD; B; 1411; ±10%; -55÷125°C; TAJ
رمز الشركة المصنعة: TAJB106K016RNJ
الشركة المصنعة: KYOCERA AVX
السعر الصافي للكميات من 1 pcs - 0.46 EURالسعر الإجمالي للكميات من 1 pcs - 0.46 EUR
السعر الصافي للكميات من 10 pcs - 0.25 EURالسعر الإجمالي للكميات من 10 pcs - 0.25 EUR
السعر الصافي للكميات من 50 pcs - 0.16 EURالسعر الإجمالي للكميات من 50 pcs - 0.16 EUR
السعر الصافي للكميات من 100 pcs - 0.13 EURالسعر الإجمالي للكميات من 100 pcs - 0.13 EUR
السعر الصافي للكميات من 500 pcs - 0.10 EURالسعر الإجمالي للكميات من 500 pcs - 0.10 EUR
السعر الصافي للكميات من 1000 pcs - 0.09 EURالسعر الإجمالي للكميات من 1000 pcs - 0.09 EUR
السعر الصافي للكميات من 2000 pcs - 0.08 EURالسعر الإجمالي للكميات من 2000 pcs - 0.08 EUR
السعر الصافي للكميات من 4000 pcs - 0.08 EURالسعر الإجمالي للكميات من 4000 pcs - 0.08 EUR
السعر الصافي للكميات من 6000 pcs - 0.08 EURالسعر الإجمالي للكميات من 6000 pcs - 0.08 EUR
السعر الصافي للكميات من 10000 pcs - 0.08 EURالسعر الإجمالي للكميات من 10000 pcs - 0.08 EUR
104390 في مستودع TME
عدد القطع (المضاعف: 1)
TAJA106K016RNJ | Capacitor: tantalum; 10uF; 16VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ
Capacitor: tantalum; 10uF; 16VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ
رمز الشركة المصنعة: TAJA106K016RNJ
الشركة المصنعة: KYOCERA AVX
السعر الصافي للكميات من 1 pcs - 0.39 EURالسعر الإجمالي للكميات من 1 pcs - 0.39 EUR
السعر الصافي للكميات من 10 pcs - 0.14 EURالسعر الإجمالي للكميات من 10 pcs - 0.14 EUR
السعر الصافي للكميات من 50 pcs - 0.12 EURالسعر الإجمالي للكميات من 50 pcs - 0.12 EUR
السعر الصافي للكميات من 100 pcs - 0.11 EURالسعر الإجمالي للكميات من 100 pcs - 0.11 EUR
السعر الصافي للكميات من 500 pcs - 0.09 EURالسعر الإجمالي للكميات من 500 pcs - 0.09 EUR
السعر الصافي للكميات من 1000 pcs - 0.08 EURالسعر الإجمالي للكميات من 1000 pcs - 0.08 EUR
السعر الصافي للكميات من 2000 pcs - 0.08 EURالسعر الإجمالي للكميات من 2000 pcs - 0.08 EUR
السعر الصافي للكميات من 4000 pcs - 0.07 EURالسعر الإجمالي للكميات من 4000 pcs - 0.07 EUR
السعر الصافي للكميات من 6000 pcs - 0.07 EURالسعر الإجمالي للكميات من 6000 pcs - 0.07 EUR
السعر الصافي للكميات من 10000 pcs - 0.07 EURالسعر الإجمالي للكميات من 10000 pcs - 0.07 EUR
96876 في مستودع TME
عدد القطع (المضاعف: 1)
TAJD107K016RNJ | Capacitor: tantalum; 100uF; 16VDC; SMD; D; 2917; ±10%; -55÷125°C; TAJ
Capacitor: tantalum; 100uF; 16VDC; SMD; D; 2917; ±10%; -55÷125°C; TAJ
رمز الشركة المصنعة: TAJD107K016RNJ
الشركة المصنعة: KYOCERA AVX
السعر الصافي للكميات من 1 pcs - 0.97 EURالسعر الإجمالي للكميات من 1 pcs - 0.97 EUR
السعر الصافي للكميات من 10 pcs - 0.55 EURالسعر الإجمالي للكميات من 10 pcs - 0.55 EUR
السعر الصافي للكميات من 50 pcs - 0.46 EURالسعر الإجمالي للكميات من 50 pcs - 0.46 EUR
السعر الصافي للكميات من 100 pcs - 0.43 EURالسعر الإجمالي للكميات من 100 pcs - 0.43 EUR
السعر الصافي للكميات من 250 pcs - 0.40 EURالسعر الإجمالي للكميات من 250 pcs - 0.40 EUR
السعر الصافي للكميات من 500 pcs - 0.37 EURالسعر الإجمالي للكميات من 500 pcs - 0.37 EUR
السعر الصافي للكميات من 1000 pcs - 0.37 EURالسعر الإجمالي للكميات من 1000 pcs - 0.37 EUR
السعر الصافي للكميات من 2500 pcs - 0.36 EURالسعر الإجمالي للكميات من 2500 pcs - 0.36 EUR
السعر الصافي للكميات من 5000 pcs - 0.36 EURالسعر الإجمالي للكميات من 5000 pcs - 0.36 EUR
السعر الصافي للكميات من 10000 pcs - 0.35 EURالسعر الإجمالي للكميات من 10000 pcs - 0.35 EUR
0 في مستودع TME
عدد القطع (المضاعف: 1)
293D106X9010A2TE3 | Capacitor: tantalum; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C
Capacitor: tantalum; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C
رمز الشركة المصنعة: 293D106X9010A2TE3
الشركة المصنعة: VISHAY
السعر الصافي للكميات من 1 pcs - 0.32 EURالسعر الإجمالي للكميات من 1 pcs - 0.32 EUR
السعر الصافي للكميات من 10 pcs - 0.19 EURالسعر الإجمالي للكميات من 10 pcs - 0.19 EUR
السعر الصافي للكميات من 50 pcs - 0.14 EURالسعر الإجمالي للكميات من 50 pcs - 0.14 EUR
السعر الصافي للكميات من 100 pcs - 0.12 EURالسعر الإجمالي للكميات من 100 pcs - 0.12 EUR
السعر الصافي للكميات من 500 pcs - 0.09 EURالسعر الإجمالي للكميات من 500 pcs - 0.09 EUR
السعر الصافي للكميات من 1000 pcs - 0.09 EURالسعر الإجمالي للكميات من 1000 pcs - 0.09 EUR
السعر الصافي للكميات من 2000 pcs - 0.08 EURالسعر الإجمالي للكميات من 2000 pcs - 0.08 EUR
السعر الصافي للكميات من 4000 pcs - 0.08 EURالسعر الإجمالي للكميات من 4000 pcs - 0.08 EUR
السعر الصافي للكميات من 6000 pcs - 0.08 EURالسعر الإجمالي للكميات من 6000 pcs - 0.08 EUR
السعر الصافي للكميات من 10000 pcs - 0.08 EURالسعر الإجمالي للكميات من 10000 pcs - 0.08 EUR
93557 في مستودع TME
عدد القطع (المضاعف: 1)
R82DC3100DQ50K | Capacitor: polyester; 100nF; 40VAC; 63VDC; 5mm; ±10%; 2.5x6.5x7.2mm
Capacitor: polyester; 100nF; 40VAC; 63VDC; 5mm; ±10%; 2.5x6.5x7.2mm
رمز الشركة المصنعة: R82DC3100DQ50K
الشركة المصنعة: KEMET
السعر الصافي للكميات من 1 pcs - 0.33 EURالسعر الإجمالي للكميات من 1 pcs - 0.33 EUR
السعر الصافي للكميات من 10 pcs - 0.13 EURالسعر الإجمالي للكميات من 10 pcs - 0.13 EUR
السعر الصافي للكميات من 50 pcs - 0.12 EURالسعر الإجمالي للكميات من 50 pcs - 0.12 EUR
السعر الصافي للكميات من 100 pcs - 0.11 EURالسعر الإجمالي للكميات من 100 pcs - 0.11 EUR
السعر الصافي للكميات من 500 pcs - 0.09 EURالسعر الإجمالي للكميات من 500 pcs - 0.09 EUR
السعر الصافي للكميات من 1000 pcs - 0.08 EURالسعر الإجمالي للكميات من 1000 pcs - 0.08 EUR
السعر الصافي للكميات من 3500 pcs - 0.07 EURالسعر الإجمالي للكميات من 3500 pcs - 0.07 EUR
السعر الصافي للكميات من 7000 pcs - 0.06 EURالسعر الإجمالي للكميات من 7000 pcs - 0.06 EUR
السعر الصافي للكميات من 10500 pcs - 0.06 EURالسعر الإجمالي للكميات من 10500 pcs - 0.06 EUR
السعر الصافي للكميات من 21000 pcs - 0.05 EURالسعر الإجمالي للكميات من 21000 pcs - 0.05 EUR
54606 في مستودع TME
عدد القطع (المضاعف: 1)
0603B104K500CT | Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0603
Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0603
رمز الشركة المصنعة: 0603B104K500CT
الشركة المصنعة: WALSIN
السعر الصافي للكميات من 1 pcs - 0.17 EURالسعر الإجمالي للكميات من 1 pcs - 0.17 EUR
السعر الصافي للكميات من 10 pcs - 0.09 EURالسعر الإجمالي للكميات من 10 pcs - 0.09 EUR
السعر الصافي للكميات من 100 pcs - 0.03 EURالسعر الإجمالي للكميات من 100 pcs - 0.03 EUR
السعر الصافي للكميات من 1000 pcs - 0.01 EURالسعر الإجمالي للكميات من 1000 pcs - 0.01 EUR
السعر الصافي للكميات من 4000 pcs - 0.01 EURالسعر الإجمالي للكميات من 4000 pcs - 0.01 EUR
السعر الصافي للكميات من 12000 pcs - 0.01 EURالسعر الإجمالي للكميات من 12000 pcs - 0.01 EUR
السعر الصافي للكميات من 20000 pcs - 0.01 EURالسعر الإجمالي للكميات من 20000 pcs - 0.01 EUR
السعر الصافي للكميات من 40000 pcs - 0.01 EURالسعر الإجمالي للكميات من 40000 pcs - 0.01 EUR
السعر الصافي للكميات من 60000 pcs - 0.01 EURالسعر الإجمالي للكميات من 60000 pcs - 0.01 EUR
السعر الصافي للكميات من 100000 pcs - 0.01 EURالسعر الإجمالي للكميات من 100000 pcs - 0.01 EUR
19080974 في مستودع TME
عدد القطع (المضاعف: 1)
المنتج قليل التوفر
EWH1EV101E11OT | Capacitor: electrolytic; THT; 100uF; 25VDC; Ø6.3x11mm; Pitch: 2.5mm
Capacitor: electrolytic; THT; 100uF; 25VDC; Ø6.3x11mm; Pitch: 2.5mm
رمز الشركة المصنعة: EWH1EV101E11OT
الشركة المصنعة: AISHI
السعر الصافي للكميات من 20 pcs - 0.06 EURالسعر الإجمالي للكميات من 20 pcs - 0.06 EUR
السعر الصافي للكميات من 100 pcs - 0.03 EURالسعر الإجمالي للكميات من 100 pcs - 0.03 EUR
السعر الصافي للكميات من 500 pcs - 0.02 EURالسعر الإجمالي للكميات من 500 pcs - 0.02 EUR
السعر الصافي للكميات من 1000 pcs - 0.02 EURالسعر الإجمالي للكميات من 1000 pcs - 0.02 EUR
السعر الصافي للكميات من 5000 pcs - 0.01 EURالسعر الإجمالي للكميات من 5000 pcs - 0.01 EUR
104568 في مستودع TME
عدد القطع (المضاعف: 10)
MKP-X2-100NR15/310 | Capacitor: polypropylene; X2; 100nF; 310VAC; 18x12x6mm; THT; ±10%
Capacitor: polypropylene; X2; 100nF; 310VAC; 18x12x6mm; THT; ±10%
رمز الشركة المصنعة: MKP-X2-100NR15/310
الشركة المصنعة: SR PASSIVES
السعر الصافي للكميات من 10 pcs - 0.08 EURالسعر الإجمالي للكميات من 10 pcs - 0.08 EUR
السعر الصافي للكميات من 100 pcs - 0.04 EURالسعر الإجمالي للكميات من 100 pcs - 0.04 EUR
السعر الصافي للكميات من 500 pcs - 0.03 EURالسعر الإجمالي للكميات من 500 pcs - 0.03 EUR
السعر الصافي للكميات من 1000 pcs - 0.03 EURالسعر الإجمالي للكميات من 1000 pcs - 0.03 EUR
السعر الصافي للكميات من 2000 pcs - 0.03 EURالسعر الإجمالي للكميات من 2000 pcs - 0.03 EUR
السعر الصافي للكميات من 5000 pcs - 0.03 EURالسعر الإجمالي للكميات من 5000 pcs - 0.03 EUR
السعر الصافي للكميات من 10000 pcs - 0.03 EURالسعر الإجمالي للكميات من 10000 pcs - 0.03 EUR
السعر الصافي للكميات من 20000 pcs - 0.03 EURالسعر الإجمالي للكميات من 20000 pcs - 0.03 EUR
43517 في مستودع TME
عدد القطع (المضاعف: 10)
UFW1H221MPD | Capacitor: electrolytic; THT; 220uF; 50VDC; Ø10x12.5mm; Pitch: 5mm
Capacitor: electrolytic; THT; 220uF; 50VDC; Ø10x12.5mm; Pitch: 5mm
رمز الشركة المصنعة: UFW1H221MPD
الشركة المصنعة: NICHICON
السعر الصافي للكميات من 1 pcs - 0.39 EURالسعر الإجمالي للكميات من 1 pcs - 0.39 EUR
السعر الصافي للكميات من 10 pcs - 0.23 EURالسعر الإجمالي للكميات من 10 pcs - 0.23 EUR
السعر الصافي للكميات من 50 pcs - 0.19 EURالسعر الإجمالي للكميات من 50 pcs - 0.19 EUR
السعر الصافي للكميات من 100 pcs - 0.18 EURالسعر الإجمالي للكميات من 100 pcs - 0.18 EUR
السعر الصافي للكميات من 200 pcs - 0.16 EURالسعر الإجمالي للكميات من 200 pcs - 0.16 EUR
السعر الصافي للكميات من 600 pcs - 0.15 EURالسعر الإجمالي للكميات من 600 pcs - 0.15 EUR
السعر الصافي للكميات من 1000 pcs - 0.14 EURالسعر الإجمالي للكميات من 1000 pcs - 0.14 EUR
السعر الصافي للكميات من 2600 pcs - 0.13 EURالسعر الإجمالي للكميات من 2600 pcs - 0.13 EUR
السعر الصافي للكميات من 5000 pcs - 0.12 EURالسعر الإجمالي للكميات من 5000 pcs - 0.12 EUR
5824 في مستودع TME
عدد القطع (المضاعف: 1)
JFX-4.7U/250 | Capacitor: polypropylene; 4.7uF; 250VDC; ±5%; Ø20.5x31.5mm; THT
Capacitor: polypropylene; 4.7uF; 250VDC; ±5%; Ø20.5x31.5mm; THT
رمز الشركة المصنعة: JFX-4.7U/250
الشركة المصنعة: Jb Capacitors
السعر الصافي للكميات من 1 pcs - 2.82 EURالسعر الإجمالي للكميات من 1 pcs - 2.82 EUR
السعر الصافي للكميات من 5 pcs - 2.56 EURالسعر الإجمالي للكميات من 5 pcs - 2.56 EUR
السعر الصافي للكميات من 25 pcs - 2.21 EURالسعر الإجمالي للكميات من 25 pcs - 2.21 EUR
السعر الصافي للكميات من 100 pcs - 2.06 EURالسعر الإجمالي للكميات من 100 pcs - 2.06 EUR
226 في مستودع TME
عدد القطع (المضاعف: 1)
EWH1VM471G16OT | Capacitor: electrolytic; THT; 470uF; 35VDC; Ø10x16mm; Pitch: 5mm
Capacitor: electrolytic; THT; 470uF; 35VDC; Ø10x16mm; Pitch: 5mm
رمز الشركة المصنعة: EWH1VM471G16OT
الشركة المصنعة: AISHI
السعر الصافي للكميات من 10 pcs - 0.17 EURالسعر الإجمالي للكميات من 10 pcs - 0.17 EUR
السعر الصافي للكميات من 100 pcs - 0.07 EURالسعر الإجمالي للكميات من 100 pcs - 0.07 EUR
السعر الصافي للكميات من 250 pcs - 0.06 EURالسعر الإجمالي للكميات من 250 pcs - 0.06 EUR
السعر الصافي للكميات من 500 pcs - 0.05 EURالسعر الإجمالي للكميات من 500 pcs - 0.05 EUR
السعر الصافي للكميات من 1000 pcs - 0.05 EURالسعر الإجمالي للكميات من 1000 pcs - 0.05 EUR
السعر الصافي للكميات من 2500 pcs - 0.05 EURالسعر الإجمالي للكميات من 2500 pcs - 0.05 EUR
السعر الصافي للكميات من 5000 pcs - 0.05 EURالسعر الإجمالي للكميات من 5000 pcs - 0.05 EUR
السعر الصافي للكميات من 10000 pcs - 0.05 EURالسعر الإجمالي للكميات من 10000 pcs - 0.05 EUR
السعر الصافي للكميات من 20000 pcs - 0.05 EURالسعر الإجمالي للكميات من 20000 pcs - 0.05 EUR
31113 في مستودع TME
عدد القطع (المضاعف: 10)
CC-104/100 | Capacitor: ceramic; 100nF; 100V; Y5V; -20÷80%; THT; 5mm
Capacitor: ceramic; 100nF; 100V; Y5V; -20÷80%; THT; 5mm
رمز الشركة المصنعة: CC-104/100
الشركة المصنعة: SR PASSIVES
السعر الصافي للكميات من 100 pcs - 0.03 EURالسعر الإجمالي للكميات من 100 pcs - 0.03 EUR
السعر الصافي للكميات من 1000 pcs - 0.02 EURالسعر الإجمالي للكميات من 1000 pcs - 0.02 EUR
السعر الصافي للكميات من 5000 pcs - 0.02 EURالسعر الإجمالي للكميات من 5000 pcs - 0.02 EUR
7100 في مستودع TME
عدد القطع (المضاعف: 100)
TAJA106K010RNJ | Capacitor: tantalum; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ
Capacitor: tantalum; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ
رمز الشركة المصنعة: TAJA106K010RNJ
الشركة المصنعة: KYOCERA AVX
السعر الصافي للكميات من 1 pcs - 0.55 EURالسعر الإجمالي للكميات من 1 pcs - 0.55 EUR
السعر الصافي للكميات من 10 pcs - 0.27 EURالسعر الإجمالي للكميات من 10 pcs - 0.27 EUR
السعر الصافي للكميات من 100 pcs - 0.15 EURالسعر الإجمالي للكميات من 100 pcs - 0.15 EUR
السعر الصافي للكميات من 500 pcs - 0.09 EURالسعر الإجمالي للكميات من 500 pcs - 0.09 EUR
السعر الصافي للكميات من 1000 pcs - 0.08 EURالسعر الإجمالي للكميات من 1000 pcs - 0.08 EUR
السعر الصافي للكميات من 2000 pcs - 0.07 EURالسعر الإجمالي للكميات من 2000 pcs - 0.07 EUR
السعر الصافي للكميات من 4000 pcs - 0.07 EURالسعر الإجمالي للكميات من 4000 pcs - 0.07 EUR
السعر الصافي للكميات من 6000 pcs - 0.07 EURالسعر الإجمالي للكميات من 6000 pcs - 0.07 EUR
السعر الصافي للكميات من 10000 pcs - 0.07 EURالسعر الإجمالي للكميات من 10000 pcs - 0.07 EUR
السعر الصافي للكميات من 20000 pcs - 0.07 EURالسعر الإجمالي للكميات من 20000 pcs - 0.07 EUR
136861 في مستودع TME
عدد القطع (المضاعف: 1)
CL10B104KB8NNNC | Capacitor: ceramic; MLCC; 100nF; 50V; X7R; ±10%; SMD; 0603
Capacitor: ceramic; MLCC; 100nF; 50V; X7R; ±10%; SMD; 0603
رمز الشركة المصنعة: CL10B104KB8NNNC
الشركة المصنعة: SAMSUNG
السعر الصافي للكميات من 1 pcs - 0.05 EURالسعر الإجمالي للكميات من 1 pcs - 0.05 EUR
السعر الصافي للكميات من 10 pcs - 0.02 EURالسعر الإجمالي للكميات من 10 pcs - 0.02 EUR
السعر الصافي للكميات من 100 pcs - 0.01 EURالسعر الإجمالي للكميات من 100 pcs - 0.01 EUR
السعر الصافي للكميات من 1000 pcs - 0.01 EURالسعر الإجمالي للكميات من 1000 pcs - 0.01 EUR
السعر الصافي للكميات من 4000 pcs - 0.01 EURالسعر الإجمالي للكميات من 4000 pcs - 0.01 EUR
329501 في مستودع TME
عدد القطع (المضاعف: 1)
المنتج قليل التوفر
EWH1KM4R7D11OT | Capacitor: electrolytic; THT; 4.7uF; 100VDC; Ø5x11mm; Pitch: 2mm
Capacitor: electrolytic; THT; 4.7uF; 100VDC; Ø5x11mm; Pitch: 2mm
رمز الشركة المصنعة: EWH1KM4R7D11OT
الشركة المصنعة: AISHI
السعر الصافي للكميات من 20 pcs - 0.03 EURالسعر الإجمالي للكميات من 20 pcs - 0.03 EUR
السعر الصافي للكميات من 100 pcs - 0.02 EURالسعر الإجمالي للكميات من 100 pcs - 0.02 EUR
السعر الصافي للكميات من 500 pcs - 0.01 EURالسعر الإجمالي للكميات من 500 pcs - 0.01 EUR
السعر الصافي للكميات من 2500 pcs - 0.01 EURالسعر الإجمالي للكميات من 2500 pcs - 0.01 EUR
السعر الصافي للكميات من 10000 pcs - 0.01 EURالسعر الإجمالي للكميات من 10000 pcs - 0.01 EUR
90062 في مستودع TME
عدد القطع (المضاعف: 10)
R82DC3100DQ50J | Capacitor: polyester; 100nF; 40VAC; 63VDC; 5mm; ±5%; 7.2x2.5x6.5mm
Capacitor: polyester; 100nF; 40VAC; 63VDC; 5mm; ±5%; 7.2x2.5x6.5mm
رمز الشركة المصنعة: R82DC3100DQ50J
الشركة المصنعة: KEMET
السعر الصافي للكميات من 1 pcs - 0.35 EURالسعر الإجمالي للكميات من 1 pcs - 0.35 EUR
السعر الصافي للكميات من 10 pcs - 0.16 EURالسعر الإجمالي للكميات من 10 pcs - 0.16 EUR
السعر الصافي للكميات من 50 pcs - 0.14 EURالسعر الإجمالي للكميات من 50 pcs - 0.14 EUR
السعر الصافي للكميات من 100 pcs - 0.13 EURالسعر الإجمالي للكميات من 100 pcs - 0.13 EUR
السعر الصافي للكميات من 500 pcs - 0.11 EURالسعر الإجمالي للكميات من 500 pcs - 0.11 EUR
السعر الصافي للكميات من 1000 pcs - 0.10 EURالسعر الإجمالي للكميات من 1000 pcs - 0.10 EUR
السعر الصافي للكميات من 3500 pcs - 0.08 EURالسعر الإجمالي للكميات من 3500 pcs - 0.08 EUR
السعر الصافي للكميات من 7000 pcs - 0.07 EURالسعر الإجمالي للكميات من 7000 pcs - 0.07 EUR
السعر الصافي للكميات من 10500 pcs - 0.06 EURالسعر الإجمالي للكميات من 10500 pcs - 0.06 EUR
السعر الصافي للكميات من 24500 pcs - 0.05 EURالسعر الإجمالي للكميات من 24500 pcs - 0.05 EUR
51537 في مستودع TME