مكثفات

(17 721)

A capacitor is one of the basic passive electronic components. Its task is to store energy in the electric field. The amount of stored energy is described by the capacitance of the capacitor, which is expressed in farads (F). The capacitance measured in full farads is not very common. Typically, capacitors have the capacitance of micro- (µ), nano- (n), pico- (p) farads.
The second basic parameter of a capacitor, apart from its capacitance, is its maximum operating voltage. Due to its design, a capacitor is susceptible to the so-called breakdown. Therefore, each capacitor has a parameter that defines the maximum voltage that can appear between its terminals. After exceeding it, a breakdown may occur, resulting in a short-circuit of the capacitor.

Capacitor – design and principle of operation

Capacitors are made of two conductors (capacitor plates) separated from each other by a non-conductive dielectric material. It can be any insulating material such as: air, plastic, ceramics, paper. The operation of a capacitor is based on Coulomb's law. According to that law, the media on both plates of the capacitor interact with each other. Media with the same charge repel each other, while those with the opposite charge attract each other. The effect of such a phenomenon is the presence of opposite charges on the capacitor plates. Their number is equal on both sides. Thanks to the dielectric material contained between the plates, the flow of charges is impossible, and this results in the formation of an electric field.

Types of capacitors

There are many different types of capacitors available on the market, including customized designs for specific tasks. Some of the types of capacitors available at TME are described below. Ceramic capacitors and MLCCs – these are some of the most common electronic components. What is interesting, the number of such capacitors manufactured in a single year is about one trillion. Ceramic capacitors owe their name to the ceramics used as an insulating material. MLCCs (multi-layer ceramic capacitors) are a subtype of conventional ceramic capacitors. An MLCC is a ceramic capacitor made in a multi-layer process. Ceramic capacitors do not have a specific polarisation, so they can be used in AC circuits, they are also available in both THT (through-hole mounting) and SMD (surface mounting) versions.

Electrolytic capacitors – the second most common type of capacitors are electrolytic designs. Thanks to the use of electrolyte, they offer much larger capacitance than ceramic capacitors. Almost all of them require appropriate polarisation – incorrect incorporation of such a capacitor into a circuit may even result in its explosion. These capacitors are also available in THT and SMD versions.

Trimmer – it is a variable capacitor, also called a tuning capacitor or tuning condenser. As the name suggests, the capacitance of such a capacitor can be freely adjusted. Trimmers were used in older designs of radios. At TME, several modern SMD trimmers are available.

Supercapacitors – they are a type of electrolytic capacitors and are able to store huge amounts of energy. Thanks to a special design, their capacitance reaches up to 3kF. In practice, it can be said that supercapacitors combine features of conventional capacitors and rechargeable batteries. Charging speed is their great advantage.

منتجات: 17 721

المستودع:

TME
الكل
الصفحة 1
NEW
EEHZA1K470V | Capacitor: hybrid; H: 10.5mm; 47uF; 80VDC; 1.7A; SMD; ESR: 36mΩ; ZA
Capacitor: hybrid; H: 10.5mm; 47uF; 80VDC; 1.7A; SMD; ESR: 36mΩ; ZA
رمز الشركة المصنعة: EEHZA1K470V
الشركة المصنعة: PANASONIC
السعر الصافي للكميات من 1 pcs - 2.52 USDالسعر الإجمالي للكميات من 1 pcs - 2.52 USD
السعر الصافي للكميات من 5 pcs - 2.15 USDالسعر الإجمالي للكميات من 5 pcs - 2.15 USD
السعر الصافي للكميات من 10 pcs - 1.93 USDالسعر الإجمالي للكميات من 10 pcs - 1.93 USD
السعر الصافي للكميات من 50 pcs - 1.44 USDالسعر الإجمالي للكميات من 50 pcs - 1.44 USD
السعر الصافي للكميات من 100 pcs - 1.30 USDالسعر الإجمالي للكميات من 100 pcs - 1.30 USD
السعر الصافي للكميات من 250 pcs - 1.15 USDالسعر الإجمالي للكميات من 250 pcs - 1.15 USD
السعر الصافي للكميات من 500 pcs - 1.07 USDالسعر الإجمالي للكميات من 500 pcs - 1.07 USD
السعر الصافي للكميات من 1000 pcs - 1.00 USDالسعر الإجمالي للكميات من 1000 pcs - 1.00 USD
السعر الصافي للكميات من 1500 pcs - 0.98 USDالسعر الإجمالي للكميات من 1500 pcs - 0.98 USD
السعر الصافي للكميات من 3500 pcs - 0.92 USDالسعر الإجمالي للكميات من 3500 pcs - 0.92 USD
28 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
HG2W687M35050HC | Capacitor: electrolytic; SNAP-IN; 680uF; 450VDC; Ø35x50mm; ±20%
Capacitor: electrolytic; SNAP-IN; 680uF; 450VDC; Ø35x50mm; ±20%
رمز الشركة المصنعة: HG2W687M35050HC
الشركة المصنعة: SAMWHA
السعر الصافي للكميات من 1 pcs - 6.49 USDالسعر الإجمالي للكميات من 1 pcs - 6.49 USD
السعر الصافي للكميات من 5 pcs - 6.21 USDالسعر الإجمالي للكميات من 5 pcs - 6.21 USD
السعر الصافي للكميات من 10 pcs - 5.91 USDالسعر الإجمالي للكميات من 10 pcs - 5.91 USD
السعر الصافي للكميات من 25 pcs - 5.60 USDالسعر الإجمالي للكميات من 25 pcs - 5.60 USD
السعر الصافي للكميات من 50 pcs - 5.40 USDالسعر الإجمالي للكميات من 50 pcs - 5.40 USD
السعر الصافي للكميات من 100 pcs - 5.12 USDالسعر الإجمالي للكميات من 100 pcs - 5.12 USD
62 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
MSASU31LBB5106KTNA01 | Capacitor: ceramic; MLCC; 10uF; 50VDC; ±10%; SMD; 1206
Capacitor: ceramic; MLCC; 10uF; 50VDC; ±10%; SMD; 1206
رمز الشركة المصنعة: MSASU31LBB5106KTNA01
الشركة المصنعة: TAIYO YUDEN
السعر الصافي للكميات من 1 pcs - 0.27 USDالسعر الإجمالي للكميات من 1 pcs - 0.27 USD
السعر الصافي للكميات من 10 pcs - 0.14 USDالسعر الإجمالي للكميات من 10 pcs - 0.14 USD
السعر الصافي للكميات من 50 pcs - 0.08 USDالسعر الإجمالي للكميات من 50 pcs - 0.08 USD
السعر الصافي للكميات من 100 pcs - 0.06 USDالسعر الإجمالي للكميات من 100 pcs - 0.06 USD
السعر الصافي للكميات من 250 pcs - 0.05 USDالسعر الإجمالي للكميات من 250 pcs - 0.05 USD
السعر الصافي للكميات من 500 pcs - 0.05 USDالسعر الإجمالي للكميات من 500 pcs - 0.05 USD
السعر الصافي للكميات من 1000 pcs - 0.05 USDالسعر الإجمالي للكميات من 1000 pcs - 0.05 USD
السعر الصافي للكميات من 2000 pcs - 0.05 USDالسعر الإجمالي للكميات من 2000 pcs - 0.05 USD
6778 في مستودع TME
عدد القطع (المضاعف: 1)
المنتج قليل التوفر
NEW
RD1C108M10016PA | Capacitor: electrolytic; THT; 1000uF; 16VDC; 10x16mm; ±20%; 2000h
Capacitor: electrolytic; THT; 1000uF; 16VDC; 10x16mm; ±20%; 2000h
رمز الشركة المصنعة: RD1C108M10016PA
الشركة المصنعة: SAMWHA
السعر الصافي للكميات من 1 pcs - 0.09 USDالسعر الإجمالي للكميات من 1 pcs - 0.09 USD
السعر الصافي للكميات من 10 pcs - 0.08 USDالسعر الإجمالي للكميات من 10 pcs - 0.08 USD
السعر الصافي للكميات من 50 pcs - 0.08 USDالسعر الإجمالي للكميات من 50 pcs - 0.08 USD
السعر الصافي للكميات من 100 pcs - 0.07 USDالسعر الإجمالي للكميات من 100 pcs - 0.07 USD
السعر الصافي للكميات من 250 pcs - 0.07 USDالسعر الإجمالي للكميات من 250 pcs - 0.07 USD
السعر الصافي للكميات من 500 pcs - 0.07 USDالسعر الإجمالي للكميات من 500 pcs - 0.07 USD
السعر الصافي للكميات من 1000 pcs - 0.06 USDالسعر الإجمالي للكميات من 1000 pcs - 0.06 USD
السعر الصافي للكميات من 1500 pcs - 0.06 USDالسعر الإجمالي للكميات من 1500 pcs - 0.06 USD
السعر الصافي للكميات من 3000 pcs - 0.06 USDالسعر الإجمالي للكميات من 3000 pcs - 0.06 USD
السعر الصافي للكميات من 6000 pcs - 0.06 USDالسعر الإجمالي للكميات من 6000 pcs - 0.06 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
NXH35VB220M3.5TP8X11.5 | Capacitor: electrolytic; low ESR; THT; 220uF; 35VDC; Pitch: 3.5mm
Capacitor: electrolytic; low ESR; THT; 220uF; 35VDC; Pitch: 3.5mm
رمز الشركة المصنعة: NXH35VB220M3.5TP8X11.5
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.09 USDالسعر الإجمالي للكميات من 1 pcs - 0.09 USD
السعر الصافي للكميات من 10 pcs - 0.08 USDالسعر الإجمالي للكميات من 10 pcs - 0.08 USD
السعر الصافي للكميات من 50 pcs - 0.07 USDالسعر الإجمالي للكميات من 50 pcs - 0.07 USD
السعر الصافي للكميات من 100 pcs - 0.07 USDالسعر الإجمالي للكميات من 100 pcs - 0.07 USD
السعر الصافي للكميات من 250 pcs - 0.06 USDالسعر الإجمالي للكميات من 250 pcs - 0.06 USD
السعر الصافي للكميات من 500 pcs - 0.06 USDالسعر الإجمالي للكميات من 500 pcs - 0.06 USD
السعر الصافي للكميات من 1000 pcs - 0.06 USDالسعر الإجمالي للكميات من 1000 pcs - 0.06 USD
358 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
MKS2D022201A00KSSD | Capacitor: polyester; 22nF; 63VDC,100VDC; 5mm; ±10%; 2.5x6.5x7.2mm
Capacitor: polyester; 22nF; 63VDC,100VDC; 5mm; ±10%; 2.5x6.5x7.2mm
رمز الشركة المصنعة: MKS2D022201A00KSSD
الشركة المصنعة: WIMA
السعر الصافي للكميات من 10000 pcs - 0.13 USDالسعر الإجمالي للكميات من 10000 pcs - 0.13 USD
0 في مستودع TME
عدد القطع (المضاعف: 10 000)
NEW
RD1V477M10016PA | Capacitor: electrolytic; THT; 470uF; 35VDC; 10x16mm; ±20%; 2000h
Capacitor: electrolytic; THT; 470uF; 35VDC; 10x16mm; ±20%; 2000h
رمز الشركة المصنعة: RD1V477M10016PA
الشركة المصنعة: SAMWHA
السعر الصافي للكميات من 1 pcs - 0.11 USDالسعر الإجمالي للكميات من 1 pcs - 0.11 USD
السعر الصافي للكميات من 10 pcs - 0.10 USDالسعر الإجمالي للكميات من 10 pcs - 0.10 USD
السعر الصافي للكميات من 50 pcs - 0.09 USDالسعر الإجمالي للكميات من 50 pcs - 0.09 USD
السعر الصافي للكميات من 100 pcs - 0.09 USDالسعر الإجمالي للكميات من 100 pcs - 0.09 USD
السعر الصافي للكميات من 250 pcs - 0.08 USDالسعر الإجمالي للكميات من 250 pcs - 0.08 USD
السعر الصافي للكميات من 500 pcs - 0.08 USDالسعر الإجمالي للكميات من 500 pcs - 0.08 USD
السعر الصافي للكميات من 1000 pcs - 0.07 USDالسعر الإجمالي للكميات من 1000 pcs - 0.07 USD
السعر الصافي للكميات من 1500 pcs - 0.07 USDالسعر الإجمالي للكميات من 1500 pcs - 0.07 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
NXH50VB470M10X20 | Capacitor: electrolytic; low ESR; THT; 470uF; 50VDC; Pitch: 5mm
Capacitor: electrolytic; low ESR; THT; 470uF; 50VDC; Pitch: 5mm
رمز الشركة المصنعة: NXH50VB470M10X20
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.25 USDالسعر الإجمالي للكميات من 1 pcs - 0.25 USD
السعر الصافي للكميات من 10 pcs - 0.20 USDالسعر الإجمالي للكميات من 10 pcs - 0.20 USD
السعر الصافي للكميات من 25 pcs - 0.19 USDالسعر الإجمالي للكميات من 25 pcs - 0.19 USD
السعر الصافي للكميات من 50 pcs - 0.17 USDالسعر الإجمالي للكميات من 50 pcs - 0.17 USD
السعر الصافي للكميات من 100 pcs - 0.16 USDالسعر الإجمالي للكميات من 100 pcs - 0.16 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
SD2A106M05011PC | Capacitor: electrolytic; THT; 10uF; 100VDC; 5x11mm; ±20%; 2000h
Capacitor: electrolytic; THT; 10uF; 100VDC; 5x11mm; ±20%; 2000h
رمز الشركة المصنعة: SD2A106M05011PC
الشركة المصنعة: SAMWHA
السعر الصافي للكميات من 1 pcs - 0.09 USDالسعر الإجمالي للكميات من 1 pcs - 0.09 USD
السعر الصافي للكميات من 10 pcs - 0.05 USDالسعر الإجمالي للكميات من 10 pcs - 0.05 USD
السعر الصافي للكميات من 100 pcs - 0.02 USDالسعر الإجمالي للكميات من 100 pcs - 0.02 USD
السعر الصافي للكميات من 500 pcs - 0.02 USDالسعر الإجمالي للكميات من 500 pcs - 0.02 USD
السعر الصافي للكميات من 1000 pcs - 0.02 USDالسعر الإجمالي للكميات من 1000 pcs - 0.02 USD
السعر الصافي للكميات من 2000 pcs - 0.02 USDالسعر الإجمالي للكميات من 2000 pcs - 0.02 USD
السعر الصافي للكميات من 4000 pcs - 0.02 USDالسعر الإجمالي للكميات من 4000 pcs - 0.02 USD
السعر الصافي للكميات من 6000 pcs - 0.02 USDالسعر الإجمالي للكميات من 6000 pcs - 0.02 USD
السعر الصافي للكميات من 10000 pcs - 0.01 USDالسعر الإجمالي للكميات من 10000 pcs - 0.01 USD
3952 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
NXH35VB470M10X16 | Capacitor: electrolytic; low ESR; THT; 470uF; 35VDC; Pitch: 5mm
Capacitor: electrolytic; low ESR; THT; 470uF; 35VDC; Pitch: 5mm
رمز الشركة المصنعة: NXH35VB470M10X16
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.13 USDالسعر الإجمالي للكميات من 1 pcs - 0.13 USD
السعر الصافي للكميات من 10 pcs - 0.13 USDالسعر الإجمالي للكميات من 10 pcs - 0.13 USD
السعر الصافي للكميات من 25 pcs - 0.10 USDالسعر الإجمالي للكميات من 25 pcs - 0.10 USD
السعر الصافي للكميات من 50 pcs - 0.09 USDالسعر الإجمالي للكميات من 50 pcs - 0.09 USD
السعر الصافي للكميات من 100 pcs - 0.09 USDالسعر الإجمالي للكميات من 100 pcs - 0.09 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
CS3216X5R107M100NRI | Capacitor: ceramic; MLCC; 100uF; 10V; X5R; ±20%; SMD; 1206
Capacitor: ceramic; MLCC; 100uF; 10V; X5R; ±20%; SMD; 1206
رمز الشركة المصنعة: CS3216X5R107M100NRI
الشركة المصنعة: SAMWHA
السعر الصافي للكميات من 1 pcs - 0.33 USDالسعر الإجمالي للكميات من 1 pcs - 0.33 USD
السعر الصافي للكميات من 10 pcs - 0.29 USDالسعر الإجمالي للكميات من 10 pcs - 0.29 USD
السعر الصافي للكميات من 100 pcs - 0.28 USDالسعر الإجمالي للكميات من 100 pcs - 0.28 USD
السعر الصافي للكميات من 500 pcs - 0.26 USDالسعر الإجمالي للكميات من 500 pcs - 0.26 USD
السعر الصافي للكميات من 1000 pcs - 0.24 USDالسعر الإجمالي للكميات من 1000 pcs - 0.24 USD
السعر الصافي للكميات من 2000 pcs - 0.23 USDالسعر الإجمالي للكميات من 2000 pcs - 0.23 USD
السعر الصافي للكميات من 4000 pcs - 0.22 USDالسعر الإجمالي للكميات من 4000 pcs - 0.22 USD
السعر الصافي للكميات من 10000 pcs - 0.21 USDالسعر الإجمالي للكميات من 10000 pcs - 0.21 USD
7699 في مستودع TME
عدد القطع (المضاعف: 1)
المنتج قليل التوفر
NEW
NXH25VB1000M5.0TP10X25 | Capacitor: electrolytic; low ESR; THT; 1000uF; 25VDC; Pitch: 5mm
Capacitor: electrolytic; low ESR; THT; 1000uF; 25VDC; Pitch: 5mm
رمز الشركة المصنعة: NXH25VB1000M5.0TP10X25
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.31 USDالسعر الإجمالي للكميات من 1 pcs - 0.31 USD
السعر الصافي للكميات من 10 pcs - 0.26 USDالسعر الإجمالي للكميات من 10 pcs - 0.26 USD
السعر الصافي للكميات من 50 pcs - 0.23 USDالسعر الإجمالي للكميات من 50 pcs - 0.23 USD
السعر الصافي للكميات من 100 pcs - 0.22 USDالسعر الإجمالي للكميات من 100 pcs - 0.22 USD
السعر الصافي للكميات من 250 pcs - 0.20 USDالسعر الإجمالي للكميات من 250 pcs - 0.20 USD
السعر الصافي للكميات من 500 pcs - 0.19 USDالسعر الإجمالي للكميات من 500 pcs - 0.19 USD
215 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
NXH35VB47M5X11 | Capacitor: electrolytic; low ESR; THT; 47uF; 35VDC; Pitch: 2mm; ±20%
Capacitor: electrolytic; low ESR; THT; 47uF; 35VDC; Pitch: 2mm; ±20%
رمز الشركة المصنعة: NXH35VB47M5X11
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.10 USDالسعر الإجمالي للكميات من 1 pcs - 0.10 USD
السعر الصافي للكميات من 10 pcs - 0.06 USDالسعر الإجمالي للكميات من 10 pcs - 0.06 USD
السعر الصافي للكميات من 25 pcs - 0.05 USDالسعر الإجمالي للكميات من 25 pcs - 0.05 USD
السعر الصافي للكميات من 50 pcs - 0.05 USDالسعر الإجمالي للكميات من 50 pcs - 0.05 USD
السعر الصافي للكميات من 100 pcs - 0.04 USDالسعر الإجمالي للكميات من 100 pcs - 0.04 USD
السعر الصافي للكميات من 200 pcs - 0.04 USDالسعر الإجمالي للكميات من 200 pcs - 0.04 USD
27 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
NXA25VB100M2.5TP6.3X11 | Capacitor: electrolytic; low ESR; THT; 100uF; 25VDC; Pitch: 2.5mm
Capacitor: electrolytic; low ESR; THT; 100uF; 25VDC; Pitch: 2.5mm
رمز الشركة المصنعة: NXA25VB100M2.5TP6.3X11
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.09 USDالسعر الإجمالي للكميات من 1 pcs - 0.09 USD
السعر الصافي للكميات من 10 pcs - 0.05 USDالسعر الإجمالي للكميات من 10 pcs - 0.05 USD
السعر الصافي للكميات من 50 pcs - 0.05 USDالسعر الإجمالي للكميات من 50 pcs - 0.05 USD
السعر الصافي للكميات من 100 pcs - 0.04 USDالسعر الإجمالي للكميات من 100 pcs - 0.04 USD
السعر الصافي للكميات من 250 pcs - 0.04 USDالسعر الإجمالي للكميات من 250 pcs - 0.04 USD
السعر الصافي للكميات من 500 pcs - 0.04 USDالسعر الإجمالي للكميات من 500 pcs - 0.04 USD
السعر الصافي للكميات من 1000 pcs - 0.03 USDالسعر الإجمالي للكميات من 1000 pcs - 0.03 USD
السعر الصافي للكميات من 1500 pcs - 0.03 USDالسعر الإجمالي للكميات من 1500 pcs - 0.03 USD
1081 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
MSAST21GBB5106MTNA01 | Capacitor: ceramic; MLCC; 10uF; 25VDC; ±20%; SMD; 0805
Capacitor: ceramic; MLCC; 10uF; 25VDC; ±20%; SMD; 0805
رمز الشركة المصنعة: MSAST21GBB5106MTNA01
الشركة المصنعة: TAIYO YUDEN
السعر الصافي للكميات من 1 pcs - 0.12 USDالسعر الإجمالي للكميات من 1 pcs - 0.12 USD
السعر الصافي للكميات من 10 pcs - 0.08 USDالسعر الإجمالي للكميات من 10 pcs - 0.08 USD
السعر الصافي للكميات من 100 pcs - 0.04 USDالسعر الإجمالي للكميات من 100 pcs - 0.04 USD
السعر الصافي للكميات من 500 pcs - 0.04 USDالسعر الإجمالي للكميات من 500 pcs - 0.04 USD
السعر الصافي للكميات من 1500 pcs - 0.03 USDالسعر الإجمالي للكميات من 1500 pcs - 0.03 USD
السعر الصافي للكميات من 3000 pcs - 0.03 USDالسعر الإجمالي للكميات من 3000 pcs - 0.03 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
المنتج قليل التوفر
NEW
CC0402JRNPO9BN101 | Capacitor: ceramic; MLCC; 100pF; 50V; C0G (NP0); ±5%; SMD; 0402
Capacitor: ceramic; MLCC; 100pF; 50V; C0G (NP0); ±5%; SMD; 0402
رمز الشركة المصنعة: CC0402JRNPO9BN101
الشركة المصنعة: YAGEO
السعر الصافي للكميات من 1 pcs - 0.03 USDالسعر الإجمالي للكميات من 1 pcs - 0.03 USD
السعر الصافي للكميات من 10000 pcs - 0.00 USDالسعر الإجمالي للكميات من 10000 pcs - 0.00 USD
السعر الصافي للكميات من 20000 pcs - 0.00 USDالسعر الإجمالي للكميات من 20000 pcs - 0.00 USD
السعر الصافي للكميات من 30000 pcs - 0.00 USDالسعر الإجمالي للكميات من 30000 pcs - 0.00 USD
السعر الصافي للكميات من 50000 pcs - 0.00 USDالسعر الإجمالي للكميات من 50000 pcs - 0.00 USD
السعر الصافي للكميات من 70000 pcs - 0.00 USDالسعر الإجمالي للكميات من 70000 pcs - 0.00 USD
السعر الصافي للكميات من 100000 pcs - 0.00 USDالسعر الإجمالي للكميات من 100000 pcs - 0.00 USD
السعر الصافي للكميات من 200000 pcs - 0.00 USDالسعر الإجمالي للكميات من 200000 pcs - 0.00 USD
السعر الصافي للكميات من 400000 pcs - 0.00 USDالسعر الإجمالي للكميات من 400000 pcs - 0.00 USD
السعر الصافي للكميات من 500000 pcs - 0.00 USDالسعر الإجمالي للكميات من 500000 pcs - 0.00 USD
160892 في مستودع TME
عدد القطع (المضاعف: 1)
المنتج قليل التوفر
NEW
SCF2E103Z14FF8S | Capacitor: ceramic; 10nF; 250V; -20÷80%; THT; 7.5mm
Capacitor: ceramic; 10nF; 250V; -20÷80%; THT; 7.5mm
رمز الشركة المصنعة: SCF2E103Z14FF8S
الشركة المصنعة: SAMWHA
السعر الصافي للكميات من 1 pcs - 0.09 USDالسعر الإجمالي للكميات من 1 pcs - 0.09 USD
السعر الصافي للكميات من 10 pcs - 0.09 USDالسعر الإجمالي للكميات من 10 pcs - 0.09 USD
السعر الصافي للكميات من 50 pcs - 0.09 USDالسعر الإجمالي للكميات من 50 pcs - 0.09 USD
السعر الصافي للكميات من 150 pcs - 0.08 USDالسعر الإجمالي للكميات من 150 pcs - 0.08 USD
السعر الصافي للكميات من 300 pcs - 0.08 USDالسعر الإجمالي للكميات من 300 pcs - 0.08 USD
السعر الصافي للكميات من 600 pcs - 0.08 USDالسعر الإجمالي للكميات من 600 pcs - 0.08 USD
السعر الصافي للكميات من 1200 pcs - 0.08 USDالسعر الإجمالي للكميات من 1200 pcs - 0.08 USD
السعر الصافي للكميات من 2400 pcs - 0.07 USDالسعر الإجمالي للكميات من 2400 pcs - 0.07 USD
السعر الصافي للكميات من 3600 pcs - 0.07 USDالسعر الإجمالي للكميات من 3600 pcs - 0.07 USD
1212 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
WB1V108M12025PL | Capacitor: electrolytic; THT; 1000uF; 35VDC; 12.5x25mm; ±20%; 5000h
Capacitor: electrolytic; THT; 1000uF; 35VDC; 12.5x25mm; ±20%; 5000h
رمز الشركة المصنعة: WB1V108M12025PL
الشركة المصنعة: SAMWHA
السعر الصافي للكميات من 1 pcs - 0.39 USDالسعر الإجمالي للكميات من 1 pcs - 0.39 USD
السعر الصافي للكميات من 10 pcs - 0.35 USDالسعر الإجمالي للكميات من 10 pcs - 0.35 USD
السعر الصافي للكميات من 50 pcs - 0.33 USDالسعر الإجمالي للكميات من 50 pcs - 0.33 USD
السعر الصافي للكميات من 100 pcs - 0.32 USDالسعر الإجمالي للكميات من 100 pcs - 0.32 USD
السعر الصافي للكميات من 200 pcs - 0.30 USDالسعر الإجمالي للكميات من 200 pcs - 0.30 USD
السعر الصافي للكميات من 400 pcs - 0.29 USDالسعر الإجمالي للكميات من 400 pcs - 0.29 USD
السعر الصافي للكميات من 800 pcs - 0.27 USDالسعر الإجمالي للكميات من 800 pcs - 0.27 USD
السعر الصافي للكميات من 1600 pcs - 0.26 USDالسعر الإجمالي للكميات من 1600 pcs - 0.26 USD
1365 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
NBC400VB10M10X16 | Capacitor: electrolytic; THT; 10uF; 400VDC; Pitch: 5mm; ±20%; 10000h
Capacitor: electrolytic; THT; 10uF; 400VDC; Pitch: 5mm; ±20%; 10000h
رمز الشركة المصنعة: NBC400VB10M10X16
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.36 USDالسعر الإجمالي للكميات من 1 pcs - 0.36 USD
السعر الصافي للكميات من 10 pcs - 0.26 USDالسعر الإجمالي للكميات من 10 pcs - 0.26 USD
السعر الصافي للكميات من 25 pcs - 0.23 USDالسعر الإجمالي للكميات من 25 pcs - 0.23 USD
السعر الصافي للكميات من 50 pcs - 0.20 USDالسعر الإجمالي للكميات من 50 pcs - 0.20 USD
السعر الصافي للكميات من 100 pcs - 0.18 USDالسعر الإجمالي للكميات من 100 pcs - 0.18 USD
50 في مستودع TME
عدد القطع (المضاعف: 1)
NEW
NXH35VB100M6.3X11 | Capacitor: electrolytic; low ESR; THT; 100uF; 35VDC; Pitch: 2.5mm
Capacitor: electrolytic; low ESR; THT; 100uF; 35VDC; Pitch: 2.5mm
رمز الشركة المصنعة: NXH35VB100M6.3X11
الشركة المصنعة: SAMYOUNG
السعر الصافي للكميات من 1 pcs - 0.13 USDالسعر الإجمالي للكميات من 1 pcs - 0.13 USD
السعر الصافي للكميات من 10 pcs - 0.08 USDالسعر الإجمالي للكميات من 10 pcs - 0.08 USD
السعر الصافي للكميات من 25 pcs - 0.06 USDالسعر الإجمالي للكميات من 25 pcs - 0.06 USD
السعر الصافي للكميات من 50 pcs - 0.05 USDالسعر الإجمالي للكميات من 50 pcs - 0.05 USD
السعر الصافي للكميات من 100 pcs - 0.05 USDالسعر الإجمالي للكميات من 100 pcs - 0.05 USD
السعر الصافي للكميات من 200 pcs - 0.04 USDالسعر الإجمالي للكميات من 200 pcs - 0.04 USD
السعر الصافي للكميات من 400 pcs - 0.04 USDالسعر الإجمالي للكميات من 400 pcs - 0.04 USD
736 في مستودع TME