مكثفات

(134 989)

A capacitor is one of the basic passive electronic components. Its task is to store energy in the electric field. The amount of stored energy is described by the capacitance of the capacitor, which is expressed in farads (F). The capacitance measured in full farads is not very common. Typically, capacitors have the capacitance of micro- (µ), nano- (n), pico- (p) farads.
The second basic parameter of a capacitor, apart from its capacitance, is its maximum operating voltage. Due to its design, a capacitor is susceptible to the so-called breakdown. Therefore, each capacitor has a parameter that defines the maximum voltage that can appear between its terminals. After exceeding it, a breakdown may occur, resulting in a short-circuit of the capacitor.

Capacitor – design and principle of operation

Capacitors are made of two conductors (capacitor plates) separated from each other by a non-conductive dielectric material. It can be any insulating material such as: air, plastic, ceramics, paper. The operation of a capacitor is based on Coulomb's law. According to that law, the media on both plates of the capacitor interact with each other. Media with the same charge repel each other, while those with the opposite charge attract each other. The effect of such a phenomenon is the presence of opposite charges on the capacitor plates. Their number is equal on both sides. Thanks to the dielectric material contained between the plates, the flow of charges is impossible, and this results in the formation of an electric field.

Types of capacitors

There are many different types of capacitors available on the market, including customized designs for specific tasks. Some of the types of capacitors available at TME are described below. Ceramic capacitors and MLCCs – these are some of the most common electronic components. What is interesting, the number of such capacitors manufactured in a single year is about one trillion. Ceramic capacitors owe their name to the ceramics used as an insulating material. MLCCs (multi-layer ceramic capacitors) are a subtype of conventional ceramic capacitors. An MLCC is a ceramic capacitor made in a multi-layer process. Ceramic capacitors do not have a specific polarisation, so they can be used in AC circuits, they are also available in both THT (through-hole mounting) and SMD (surface mounting) versions.

Electrolytic capacitors – the second most common type of capacitors are electrolytic designs. Thanks to the use of electrolyte, they offer much larger capacitance than ceramic capacitors. Almost all of them require appropriate polarisation – incorrect incorporation of such a capacitor into a circuit may even result in its explosion. These capacitors are also available in THT and SMD versions.

Trimmer – it is a variable capacitor, also called a tuning capacitor or tuning condenser. As the name suggests, the capacitance of such a capacitor can be freely adjusted. Trimmers were used in older designs of radios. At TME, several modern SMD trimmers are available.

Supercapacitors – they are a type of electrolytic capacitors and are able to store huge amounts of energy. Thanks to a special design, their capacitance reaches up to 3kF. In practice, it can be said that supercapacitors combine features of conventional capacitors and rechargeable batteries. Charging speed is their great advantage.

منتجات: 134 989

المستودع:

TME
خارجي
الكل
الصفحة 1
UFW1H101MPD | Capacitor: electrolytic; THT; 100uF; 50VDC; Ø8x11.5mm; Pitch: 3.5mm
Capacitor: electrolytic; THT; 100uF; 50VDC; Ø8x11.5mm; Pitch: 3.5mm
رمز الشركة المصنعة: UFW1H101MPD
الشركة المصنعة: NICHICON
السعر الصافي للكميات من 1 pcs - 0.32 USDالسعر الإجمالي للكميات من 1 pcs - 0.32 USD
السعر الصافي للكميات من 5 pcs - 0.29 USDالسعر الإجمالي للكميات من 5 pcs - 0.29 USD
السعر الصافي للكميات من 10 pcs - 0.27 USDالسعر الإجمالي للكميات من 10 pcs - 0.27 USD
السعر الصافي للكميات من 15 pcs - 0.25 USDالسعر الإجمالي للكميات من 15 pcs - 0.25 USD
السعر الصافي للكميات من 50 pcs - 0.21 USDالسعر الإجمالي للكميات من 50 pcs - 0.21 USD
السعر الصافي للكميات من 100 pcs - 0.18 USDالسعر الإجمالي للكميات من 100 pcs - 0.18 USD
السعر الصافي للكميات من 200 pcs - 0.16 USDالسعر الإجمالي للكميات من 200 pcs - 0.16 USD
السعر الصافي للكميات من 1000 pcs - 0.14 USDالسعر الإجمالي للكميات من 1000 pcs - 0.14 USD
السعر الصافي للكميات من 3000 pcs - 0.13 USDالسعر الإجمالي للكميات من 3000 pcs - 0.13 USD
السعر الصافي للكميات من 12000 pcs - 0.13 USDالسعر الإجمالي للكميات من 12000 pcs - 0.13 USD
2182 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
EEHZA1V470P | Capacitor: hybrid; 47uF; 35VDC; 1.3A; SMD; ESR: 60mΩ; ZA; ±20%; 10000h
Capacitor: hybrid; 47uF; 35VDC; 1.3A; SMD; ESR: 60mΩ; ZA; ±20%; 10000h
رمز الشركة المصنعة: EEHZA1V470P
الشركة المصنعة: PANASONIC
السعر الصافي للكميات من 1 pcs - 1.40 USDالسعر الإجمالي للكميات من 1 pcs - 1.40 USD
السعر الصافي للكميات من 10 pcs - 0.63 USDالسعر الإجمالي للكميات من 10 pcs - 0.63 USD
السعر الصافي للكميات من 50 pcs - 0.44 USDالسعر الإجمالي للكميات من 50 pcs - 0.44 USD
السعر الصافي للكميات من 100 pcs - 0.39 USDالسعر الإجمالي للكميات من 100 pcs - 0.39 USD
السعر الصافي للكميات من 250 pcs - 0.34 USDالسعر الإجمالي للكميات من 250 pcs - 0.34 USD
السعر الصافي للكميات من 500 pcs - 0.31 USDالسعر الإجمالي للكميات من 500 pcs - 0.31 USD
السعر الصافي للكميات من 1000 pcs - 0.30 USDالسعر الإجمالي للكميات من 1000 pcs - 0.30 USD
3268 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
JFX-3.3U/250 | Capacitor: polypropylene; 3.3uF; 250VDC; ±5%; Ø17.5x31.5mm; THT
Capacitor: polypropylene; 3.3uF; 250VDC; ±5%; Ø17.5x31.5mm; THT
رمز الشركة المصنعة: JFX-3.3U/250
الشركة المصنعة: Jb Capacitors
السعر الصافي للكميات من 1 pcs - 2.00 USDالسعر الإجمالي للكميات من 1 pcs - 2.00 USD
السعر الصافي للكميات من 5 pcs - 1.85 USDالسعر الإجمالي للكميات من 5 pcs - 1.85 USD
السعر الصافي للكميات من 25 pcs - 1.61 USDالسعر الإجمالي للكميات من 25 pcs - 1.61 USD
السعر الصافي للكميات من 100 pcs - 1.43 USDالسعر الإجمالي للكميات من 100 pcs - 1.43 USD
666 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
0805B104K500CT | Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0805
Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0805
رمز الشركة المصنعة: 0805B104K500CT
الشركة المصنعة: WALSIN
السعر الصافي للكميات من 1 pcs - 0.12 USDالسعر الإجمالي للكميات من 1 pcs - 0.12 USD
السعر الصافي للكميات من 10 pcs - 0.06 USDالسعر الإجمالي للكميات من 10 pcs - 0.06 USD
السعر الصافي للكميات من 100 pcs - 0.03 USDالسعر الإجمالي للكميات من 100 pcs - 0.03 USD
السعر الصافي للكميات من 1000 pcs - 0.01 USDالسعر الإجمالي للكميات من 1000 pcs - 0.01 USD
السعر الصافي للكميات من 4000 pcs - 0.01 USDالسعر الإجمالي للكميات من 4000 pcs - 0.01 USD
السعر الصافي للكميات من 20000 pcs - 0.01 USDالسعر الإجمالي للكميات من 20000 pcs - 0.01 USD
السعر الصافي للكميات من 40000 pcs - 0.01 USDالسعر الإجمالي للكميات من 40000 pcs - 0.01 USD
السعر الصافي للكميات من 80000 pcs - 0.01 USDالسعر الإجمالي للكميات من 80000 pcs - 0.01 USD
17534811 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
المنتج قليل التوفر
JFX-2.2U/250 | Capacitor: polypropylene; 2.2uF; 250VDC; ±5%; Ø14.5x31.5mm; THT
Capacitor: polypropylene; 2.2uF; 250VDC; ±5%; Ø14.5x31.5mm; THT
رمز الشركة المصنعة: JFX-2.2U/250
الشركة المصنعة: Jb Capacitors
السعر الصافي للكميات من 1 pcs - 1.83 USDالسعر الإجمالي للكميات من 1 pcs - 1.83 USD
السعر الصافي للكميات من 5 pcs - 1.69 USDالسعر الإجمالي للكميات من 5 pcs - 1.69 USD
السعر الصافي للكميات من 25 pcs - 1.55 USDالسعر الإجمالي للكميات من 25 pcs - 1.55 USD
السعر الصافي للكميات من 100 pcs - 1.39 USDالسعر الإجمالي للكميات من 100 pcs - 1.39 USD
402 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
0603B104K500CT | Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0603
Capacitor: ceramic; 100nF; 50V; X7R; ±10%; 0603
رمز الشركة المصنعة: 0603B104K500CT
الشركة المصنعة: WALSIN
السعر الصافي للكميات من 1 pcs - 0.07 USDالسعر الإجمالي للكميات من 1 pcs - 0.07 USD
السعر الصافي للكميات من 10 pcs - 0.03 USDالسعر الإجمالي للكميات من 10 pcs - 0.03 USD
السعر الصافي للكميات من 100 pcs - 0.02 USDالسعر الإجمالي للكميات من 100 pcs - 0.02 USD
السعر الصافي للكميات من 1000 pcs - 0.01 USDالسعر الإجمالي للكميات من 1000 pcs - 0.01 USD
السعر الصافي للكميات من 4000 pcs - 0.00 USDالسعر الإجمالي للكميات من 4000 pcs - 0.00 USD
السعر الصافي للكميات من 12000 pcs - 0.00 USDالسعر الإجمالي للكميات من 12000 pcs - 0.00 USD
السعر الصافي للكميات من 20000 pcs - 0.00 USDالسعر الإجمالي للكميات من 20000 pcs - 0.00 USD
السعر الصافي للكميات من 40000 pcs - 0.00 USDالسعر الإجمالي للكميات من 40000 pcs - 0.00 USD
السعر الصافي للكميات من 80000 pcs - 0.00 USDالسعر الإجمالي للكميات من 80000 pcs - 0.00 USD
السعر الصافي للكميات من 160000 pcs - 0.00 USDالسعر الإجمالي للكميات من 160000 pcs - 0.00 USD
12024661 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
المنتج قليل التوفر
UFW1H221MPD | Capacitor: electrolytic; THT; 220uF; 50VDC; Ø10x12.5mm; Pitch: 5mm
Capacitor: electrolytic; THT; 220uF; 50VDC; Ø10x12.5mm; Pitch: 5mm
رمز الشركة المصنعة: UFW1H221MPD
الشركة المصنعة: NICHICON
السعر الصافي للكميات من 1 pcs - 0.43 USDالسعر الإجمالي للكميات من 1 pcs - 0.43 USD
السعر الصافي للكميات من 10 pcs - 0.26 USDالسعر الإجمالي للكميات من 10 pcs - 0.26 USD
السعر الصافي للكميات من 50 pcs - 0.21 USDالسعر الإجمالي للكميات من 50 pcs - 0.21 USD
السعر الصافي للكميات من 100 pcs - 0.20 USDالسعر الإجمالي للكميات من 100 pcs - 0.20 USD
السعر الصافي للكميات من 200 pcs - 0.18 USDالسعر الإجمالي للكميات من 200 pcs - 0.18 USD
السعر الصافي للكميات من 600 pcs - 0.16 USDالسعر الإجمالي للكميات من 600 pcs - 0.16 USD
السعر الصافي للكميات من 1000 pcs - 0.16 USDالسعر الإجمالي للكميات من 1000 pcs - 0.16 USD
السعر الصافي للكميات من 2600 pcs - 0.14 USDالسعر الإجمالي للكميات من 2600 pcs - 0.14 USD
السعر الصافي للكميات من 5000 pcs - 0.14 USDالسعر الإجمالي للكميات من 5000 pcs - 0.14 USD
3787 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
JFX-4.7U/250 | Capacitor: polypropylene; 4.7uF; 250VDC; ±5%; Ø20.5x31.5mm; THT
Capacitor: polypropylene; 4.7uF; 250VDC; ±5%; Ø20.5x31.5mm; THT
رمز الشركة المصنعة: JFX-4.7U/250
الشركة المصنعة: Jb Capacitors
السعر الصافي للكميات من 1 pcs - 3.26 USDالسعر الإجمالي للكميات من 1 pcs - 3.26 USD
السعر الصافي للكميات من 5 pcs - 2.95 USDالسعر الإجمالي للكميات من 5 pcs - 2.95 USD
السعر الصافي للكميات من 25 pcs - 2.55 USDالسعر الإجمالي للكميات من 25 pcs - 2.55 USD
السعر الصافي للكميات من 100 pcs - 2.39 USDالسعر الإجمالي للكميات من 100 pcs - 2.39 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
TAJA106K016RNJ | Capacitor: tantalum; 10uF; 16VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ
Capacitor: tantalum; 10uF; 16VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ
رمز الشركة المصنعة: TAJA106K016RNJ
الشركة المصنعة: KYOCERA AVX
السعر الصافي للكميات من 1 pcs - 0.54 USDالسعر الإجمالي للكميات من 1 pcs - 0.54 USD
السعر الصافي للكميات من 10 pcs - 0.20 USDالسعر الإجمالي للكميات من 10 pcs - 0.20 USD
السعر الصافي للكميات من 50 pcs - 0.16 USDالسعر الإجمالي للكميات من 50 pcs - 0.16 USD
السعر الصافي للكميات من 100 pcs - 0.15 USDالسعر الإجمالي للكميات من 100 pcs - 0.15 USD
السعر الصافي للكميات من 500 pcs - 0.13 USDالسعر الإجمالي للكميات من 500 pcs - 0.13 USD
السعر الصافي للكميات من 1000 pcs - 0.11 USDالسعر الإجمالي للكميات من 1000 pcs - 0.11 USD
السعر الصافي للكميات من 2000 pcs - 0.11 USDالسعر الإجمالي للكميات من 2000 pcs - 0.11 USD
السعر الصافي للكميات من 4000 pcs - 0.10 USDالسعر الإجمالي للكميات من 4000 pcs - 0.10 USD
السعر الصافي للكميات من 6000 pcs - 0.10 USDالسعر الإجمالي للكميات من 6000 pcs - 0.10 USD
السعر الصافي للكميات من 10000 pcs - 0.10 USDالسعر الإجمالي للكميات من 10000 pcs - 0.10 USD
663 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
المنتج قليل التوفر
TAJB106K016RNJ | Capacitor: tantalum; 10uF; 16VDC; SMD; B; 1411; ±10%; -55÷125°C; TAJ
Capacitor: tantalum; 10uF; 16VDC; SMD; B; 1411; ±10%; -55÷125°C; TAJ
رمز الشركة المصنعة: TAJB106K016RNJ
الشركة المصنعة: KYOCERA AVX
السعر الصافي للكميات من 1 pcs - 0.69 USDالسعر الإجمالي للكميات من 1 pcs - 0.69 USD
السعر الصافي للكميات من 10 pcs - 0.38 USDالسعر الإجمالي للكميات من 10 pcs - 0.38 USD
السعر الصافي للكميات من 50 pcs - 0.25 USDالسعر الإجمالي للكميات من 50 pcs - 0.25 USD
السعر الصافي للكميات من 100 pcs - 0.20 USDالسعر الإجمالي للكميات من 100 pcs - 0.20 USD
السعر الصافي للكميات من 500 pcs - 0.15 USDالسعر الإجمالي للكميات من 500 pcs - 0.15 USD
السعر الصافي للكميات من 1000 pcs - 0.14 USDالسعر الإجمالي للكميات من 1000 pcs - 0.14 USD
السعر الصافي للكميات من 2000 pcs - 0.13 USDالسعر الإجمالي للكميات من 2000 pcs - 0.13 USD
السعر الصافي للكميات من 4000 pcs - 0.13 USDالسعر الإجمالي للكميات من 4000 pcs - 0.13 USD
السعر الصافي للكميات من 6000 pcs - 0.12 USDالسعر الإجمالي للكميات من 6000 pcs - 0.12 USD
السعر الصافي للكميات من 10000 pcs - 0.12 USDالسعر الإجمالي للكميات من 10000 pcs - 0.12 USD
12926 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
المنتج قليل التوفر
CC-104/100 | Capacitor: ceramic; 100nF; 100V; Y5V; -20÷80%; THT; 5mm
Capacitor: ceramic; 100nF; 100V; Y5V; -20÷80%; THT; 5mm
رمز الشركة المصنعة: CC-104/100
الشركة المصنعة: SR PASSIVES
السعر الصافي للكميات من 100 pcs - 0.04 USDالسعر الإجمالي للكميات من 100 pcs - 0.04 USD
السعر الصافي للكميات من 1000 pcs - 0.02 USDالسعر الإجمالي للكميات من 1000 pcs - 0.02 USD
السعر الصافي للكميات من 5000 pcs - 0.02 USDالسعر الإجمالي للكميات من 5000 pcs - 0.02 USD
36500 في مستودع TME
عدد القطع (المضاعف: 100)
أقل كمية يمكن طلبها: 100.
مضاعف : 100.
UES1E470MPM | Capacitor: electrolytic; bipolar; THT; 47uF; 25VDC; Ø10x12.5mm
Capacitor: electrolytic; bipolar; THT; 47uF; 25VDC; Ø10x12.5mm
رمز الشركة المصنعة: UES1E470MPM
الشركة المصنعة: NICHICON
السعر الصافي للكميات من 1 pcs - 0.75 USDالسعر الإجمالي للكميات من 1 pcs - 0.75 USD
السعر الصافي للكميات من 10 pcs - 0.41 USDالسعر الإجمالي للكميات من 10 pcs - 0.41 USD
السعر الصافي للكميات من 50 pcs - 0.35 USDالسعر الإجمالي للكميات من 50 pcs - 0.35 USD
السعر الصافي للكميات من 100 pcs - 0.33 USDالسعر الإجمالي للكميات من 100 pcs - 0.33 USD
السعر الصافي للكميات من 200 pcs - 0.30 USDالسعر الإجمالي للكميات من 200 pcs - 0.30 USD
السعر الصافي للكميات من 600 pcs - 0.27 USDالسعر الإجمالي للكميات من 600 pcs - 0.27 USD
السعر الصافي للكميات من 1000 pcs - 0.26 USDالسعر الإجمالي للكميات من 1000 pcs - 0.26 USD
السعر الصافي للكميات من 2600 pcs - 0.24 USDالسعر الإجمالي للكميات من 2600 pcs - 0.24 USD
السعر الصافي للكميات من 5000 pcs - 0.23 USDالسعر الإجمالي للكميات من 5000 pcs - 0.23 USD
1070 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
293D106X9010A2TE3 | Capacitor: tantalum; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C
Capacitor: tantalum; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C
رمز الشركة المصنعة: 293D106X9010A2TE3
الشركة المصنعة: VISHAY
السعر الصافي للكميات من 1 pcs - 0.21 USDالسعر الإجمالي للكميات من 1 pcs - 0.21 USD
السعر الصافي للكميات من 10 pcs - 0.16 USDالسعر الإجمالي للكميات من 10 pcs - 0.16 USD
السعر الصافي للكميات من 50 pcs - 0.13 USDالسعر الإجمالي للكميات من 50 pcs - 0.13 USD
السعر الصافي للكميات من 100 pcs - 0.12 USDالسعر الإجمالي للكميات من 100 pcs - 0.12 USD
السعر الصافي للكميات من 500 pcs - 0.08 USDالسعر الإجمالي للكميات من 500 pcs - 0.08 USD
السعر الصافي للكميات من 1000 pcs - 0.07 USDالسعر الإجمالي للكميات من 1000 pcs - 0.07 USD
السعر الصافي للكميات من 2000 pcs - 0.07 USDالسعر الإجمالي للكميات من 2000 pcs - 0.07 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
EWH1EV101E11OT | Capacitor: electrolytic; THT; 100uF; 25VDC; Ø6.3x11mm; Pitch: 2.5mm
Capacitor: electrolytic; THT; 100uF; 25VDC; Ø6.3x11mm; Pitch: 2.5mm
رمز الشركة المصنعة: EWH1EV101E11OT
الشركة المصنعة: AISHI
السعر الصافي للكميات من 20 pcs - 0.07 USDالسعر الإجمالي للكميات من 20 pcs - 0.07 USD
السعر الصافي للكميات من 100 pcs - 0.03 USDالسعر الإجمالي للكميات من 100 pcs - 0.03 USD
السعر الصافي للكميات من 500 pcs - 0.02 USDالسعر الإجمالي للكميات من 500 pcs - 0.02 USD
السعر الصافي للكميات من 1000 pcs - 0.02 USDالسعر الإجمالي للكميات من 1000 pcs - 0.02 USD
السعر الصافي للكميات من 5000 pcs - 0.02 USDالسعر الإجمالي للكميات من 5000 pcs - 0.02 USD
78580 في مستودع TME
عدد القطع (المضاعف: 10)
أقل كمية يمكن طلبها: 20.
مضاعف : 10.
EWH1VM471G16OT | Capacitor: electrolytic; THT; 470uF; 35VDC; Ø10x16mm; Pitch: 5mm
Capacitor: electrolytic; THT; 470uF; 35VDC; Ø10x16mm; Pitch: 5mm
رمز الشركة المصنعة: EWH1VM471G16OT
الشركة المصنعة: AISHI
السعر الصافي للكميات من 10 pcs - 0.19 USDالسعر الإجمالي للكميات من 10 pcs - 0.19 USD
السعر الصافي للكميات من 100 pcs - 0.08 USDالسعر الإجمالي للكميات من 100 pcs - 0.08 USD
السعر الصافي للكميات من 250 pcs - 0.07 USDالسعر الإجمالي للكميات من 250 pcs - 0.07 USD
السعر الصافي للكميات من 500 pcs - 0.06 USDالسعر الإجمالي للكميات من 500 pcs - 0.06 USD
السعر الصافي للكميات من 1000 pcs - 0.06 USDالسعر الإجمالي للكميات من 1000 pcs - 0.06 USD
السعر الصافي للكميات من 2500 pcs - 0.06 USDالسعر الإجمالي للكميات من 2500 pcs - 0.06 USD
السعر الصافي للكميات من 5000 pcs - 0.06 USDالسعر الإجمالي للكميات من 5000 pcs - 0.06 USD
السعر الصافي للكميات من 10000 pcs - 0.06 USDالسعر الإجمالي للكميات من 10000 pcs - 0.06 USD
السعر الصافي للكميات من 20000 pcs - 0.06 USDالسعر الإجمالي للكميات من 20000 pcs - 0.06 USD
84120 في مستودع TME
عدد القطع (المضاعف: 10)
أقل كمية يمكن طلبها: 10.
مضاعف : 10.
R82DC3100DQ50K | Capacitor: polyester; 100nF; 40VAC; 63VDC; 5mm; ±10%; 2.5x6.5x7.2mm
Capacitor: polyester; 100nF; 40VAC; 63VDC; 5mm; ±10%; 2.5x6.5x7.2mm
رمز الشركة المصنعة: R82DC3100DQ50K
الشركة المصنعة: KEMET
السعر الصافي للكميات من 1 pcs - 0.36 USDالسعر الإجمالي للكميات من 1 pcs - 0.36 USD
السعر الصافي للكميات من 10 pcs - 0.15 USDالسعر الإجمالي للكميات من 10 pcs - 0.15 USD
السعر الصافي للكميات من 50 pcs - 0.13 USDالسعر الإجمالي للكميات من 50 pcs - 0.13 USD
السعر الصافي للكميات من 100 pcs - 0.12 USDالسعر الإجمالي للكميات من 100 pcs - 0.12 USD
السعر الصافي للكميات من 500 pcs - 0.10 USDالسعر الإجمالي للكميات من 500 pcs - 0.10 USD
السعر الصافي للكميات من 1000 pcs - 0.09 USDالسعر الإجمالي للكميات من 1000 pcs - 0.09 USD
السعر الصافي للكميات من 3500 pcs - 0.08 USDالسعر الإجمالي للكميات من 3500 pcs - 0.08 USD
السعر الصافي للكميات من 7000 pcs - 0.07 USDالسعر الإجمالي للكميات من 7000 pcs - 0.07 USD
السعر الصافي للكميات من 10500 pcs - 0.07 USDالسعر الإجمالي للكميات من 10500 pcs - 0.07 USD
السعر الصافي للكميات من 21000 pcs - 0.06 USDالسعر الإجمالي للكميات من 21000 pcs - 0.06 USD
35352 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
MKS2C041001F00KSSD | Capacitor: polyester; 1uF; 40VAC; 63VDC; 5mm; ±10%; 5x10x7.2mm; MKT
Capacitor: polyester; 1uF; 40VAC; 63VDC; 5mm; ±10%; 5x10x7.2mm; MKT
رمز الشركة المصنعة: MKS2C041001F00KSSD
الشركة المصنعة: WIMA
السعر الصافي للكميات من 1 pcs - 1.00 USDالسعر الإجمالي للكميات من 1 pcs - 1.00 USD
السعر الصافي للكميات من 10 pcs - 0.64 USDالسعر الإجمالي للكميات من 10 pcs - 0.64 USD
السعر الصافي للكميات من 50 pcs - 0.50 USDالسعر الإجمالي للكميات من 50 pcs - 0.50 USD
السعر الصافي للكميات من 100 pcs - 0.46 USDالسعر الإجمالي للكميات من 100 pcs - 0.46 USD
السعر الصافي للكميات من 250 pcs - 0.40 USDالسعر الإجمالي للكميات من 250 pcs - 0.40 USD
السعر الصافي للكميات من 500 pcs - 0.36 USDالسعر الإجمالي للكميات من 500 pcs - 0.36 USD
السعر الصافي للكميات من 1000 pcs - 0.33 USDالسعر الإجمالي للكميات من 1000 pcs - 0.33 USD
السعر الصافي للكميات من 3500 pcs - 0.30 USDالسعر الإجمالي للكميات من 3500 pcs - 0.30 USD
السعر الصافي للكميات من 7000 pcs - 0.30 USDالسعر الإجمالي للكميات من 7000 pcs - 0.30 USD
0 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
المنتج قليل التوفر
K104K10X7RF5UL2 | Capacitor: ceramic; 100nF; 50V; X7R; ±10%; THT; 2.5mm
Capacitor: ceramic; 100nF; 50V; X7R; ±10%; THT; 2.5mm
رمز الشركة المصنعة: K104K10X7RF5UL2
الشركة المصنعة: VISHAY
السعر الصافي للكميات من 1 pcs - 0.23 USDالسعر الإجمالي للكميات من 1 pcs - 0.23 USD
السعر الصافي للكميات من 10 pcs - 0.14 USDالسعر الإجمالي للكميات من 10 pcs - 0.14 USD
السعر الصافي للكميات من 100 pcs - 0.09 USDالسعر الإجمالي للكميات من 100 pcs - 0.09 USD
السعر الصافي للكميات من 500 pcs - 0.07 USDالسعر الإجمالي للكميات من 500 pcs - 0.07 USD
السعر الصافي للكميات من 1000 pcs - 0.07 USDالسعر الإجمالي للكميات من 1000 pcs - 0.07 USD
السعر الصافي للكميات من 2500 pcs - 0.06 USDالسعر الإجمالي للكميات من 2500 pcs - 0.06 USD
السعر الصافي للكميات من 5000 pcs - 0.05 USDالسعر الإجمالي للكميات من 5000 pcs - 0.05 USD
السعر الصافي للكميات من 10000 pcs - 0.05 USDالسعر الإجمالي للكميات من 10000 pcs - 0.05 USD
السعر الصافي للكميات من 20000 pcs - 0.05 USDالسعر الإجمالي للكميات من 20000 pcs - 0.05 USD
8592 في مستودع TME
عدد القطع (المضاعف: 1)
أقل كمية يمكن طلبها: 1.
مضاعف : 1.
MKP-X2-100NR15/310 | Capacitor: polypropylene; X2; 100nF; 310VAC; 18x12x6mm; THT; ±10%
Capacitor: polypropylene; X2; 100nF; 310VAC; 18x12x6mm; THT; ±10%
رمز الشركة المصنعة: MKP-X2-100NR15/310
الشركة المصنعة: SR PASSIVES
السعر الصافي للكميات من 10 pcs - 0.09 USDالسعر الإجمالي للكميات من 10 pcs - 0.09 USD
السعر الصافي للكميات من 100 pcs - 0.05 USDالسعر الإجمالي للكميات من 100 pcs - 0.05 USD
السعر الصافي للكميات من 500 pcs - 0.04 USDالسعر الإجمالي للكميات من 500 pcs - 0.04 USD
السعر الصافي للكميات من 1000 pcs - 0.04 USDالسعر الإجمالي للكميات من 1000 pcs - 0.04 USD
السعر الصافي للكميات من 2000 pcs - 0.03 USDالسعر الإجمالي للكميات من 2000 pcs - 0.03 USD
السعر الصافي للكميات من 5000 pcs - 0.03 USDالسعر الإجمالي للكميات من 5000 pcs - 0.03 USD
السعر الصافي للكميات من 10000 pcs - 0.03 USDالسعر الإجمالي للكميات من 10000 pcs - 0.03 USD
السعر الصافي للكميات من 20000 pcs - 0.03 USDالسعر الإجمالي للكميات من 20000 pcs - 0.03 USD
17727 في مستودع TME
عدد القطع (المضاعف: 10)
أقل كمية يمكن طلبها: 10.
مضاعف : 10.
EEHZA1V100R | Capacitor: hybrid; 10uF; 35VDC; 900mA; SMD; ESR: 100mΩ; ZA; ±20%
Capacitor: hybrid; 10uF; 35VDC; 900mA; SMD; ESR: 100mΩ; ZA; ±20%
رمز الشركة المصنعة: EEHZA1V100R
الشركة المصنعة: PANASONIC
السعر الصافي للكميات من 1 pcs - 1.30 USDالسعر الإجمالي للكميات من 1 pcs - 1.30 USD
السعر الصافي للكميات من 10 pcs - 0.75 USDالسعر الإجمالي للكميات من 10 pcs - 0.75 USD
السعر الصافي للكميات من 50 pcs - 0.64 USDالسعر الإجمالي للكميات من 50 pcs - 0.64 USD
السعر الصافي للكميات من 100 pcs - 0.59 USDالسعر الإجمالي للكميات من 100 pcs - 0.59 USD
السعر الصافي للكميات من 500 pcs - 0.49 USDالسعر الإجمالي للكميات من 500 pcs - 0.49 USD
السعر الصافي للكميات من 1000 pcs - 0.44 USDالسعر الإجمالي للكميات من 1000 pcs - 0.44 USD
السعر الصافي للكميات من 2000 pcs - 0.39 USDالسعر الإجمالي للكميات من 2000 pcs - 0.39 USD
السعر الصافي للكميات من 3000 pcs - 0.37 USDالسعر الإجمالي للكميات من 3000 pcs - 0.37 USD
السعر الصافي للكميات من 5000 pcs - 0.33 USDالسعر الإجمالي للكميات من 5000 pcs - 0.33 USD
السعر الصافي للكميات من 7000 pcs - 0.31 USDالسعر الإجمالي للكميات من 7000 pcs - 0.31 USD
19 في مستودع TME