+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Miniature Electromagnetic Relays

(11 177)

The function performed by electromagnetic relays is trivial but extremely important. Relays are electromechanically operated switches that use a low level control signal to switch a much higher voltage or current supply. They can also perform the opposite function, e.g., turn on a lamp on the panel, signalling the flow of high current in the controlled circuit.

An electromagnetic relay consists of a coil and contacts and uses an electromagnet to close or open the contacts. In other words: applying a voltage to the coil closes or opens the circuit (or several circuits, depending on the pin configuration).

Electromagnetic relays are known in automation for many decades. Their design still undergoes some modifications, but their advantages and limitations remain the same. The main advantage is the isolation of the control and controlled circuits. This gives electromagnetic relays a certain advantage over alternatives such as electronic circuits based on semiconductors (transistors). This feature is particularly appreciated in the consumer electronics and white goods industry, where the safety of users is important, even in the event of improper handling. In many cases relays also have the advantage of being simple in design and easy to use in electronic/electrical circuits. Replacing relays in your vehicle, control unit, and machinery is not a problem. Many relays are designed for quick assembly and disassembly, use dedicated sockets, and are produced in standard formats, which facilitates the work of mechanics, maintenance technicians, etc. Unfortunately, relays also have their drawbacks - although the control currents are low, they can be considered substantial (tens or hundreds of milliamps) for energy-saving applications. As they are mechanical components, they have a certain degree of failure and are not able to match their semiconductor counterparts when it comes to the switching frequency.

Let's take a look at the basic features of electromagnetic relays that should be kept in mind when selecting the right components for your applications or when looking for a replacement for a damaged component.

Relay Contact Configuration

The first aspect is the configuration of the contacts. The most important abbreviations are: NO (normally open) and NC (normally closed). This means that the relay-controlled circuit can be normally closed or normally open, depending on the needs. Obviously, in the case when the purpose of the relay is to temporarily interrupt the supply - a relay that opens the circuit when triggered shall be used. This results in less wear on the relay, which will not consume energy during normal operation of the device.

Apart from the abbreviations NO and NC, the most common contact configurations are:

SPST (Single Pole Single Throw) - the simplest switch used to make or break the connection between each input contact and its designated output contact.

SPDT (Single Pole Double Throw) – this switch contains one input, which can switch between two outputs, i.e., can connect to and switch between two outputs. When there is no voltage applied to the coil one circuit “receives” current, the other one does not.

DPST (Double Pole Single Throw) is a switch that has 2 inputs and 2 outputs. A single control signal activates two independent circuits. Such a relay can be used for simultaneously controlling, e.g. a load and an indicator light.

DPDT (Double Pole Double Throw) - two input contacts that can be in one of two positions, i.e. connected to one set of output contacts.

TME customers looking for more pin pitch options can use the technical drawings visible when hovering the mouse over the information icon in the "Contact Configuration" field (this is one of the filters visible at the top of the page).

Basic parameters of electromagnetic relays

In addition to the contact configuration, the important parameters of relays mainly concern their electrical characteristics. A distinction should be made here:

Relay version - this specifies the general characteristics of the element (e.g., whether it is used to control signals or is resistant to high inrush currents of inductive loads such as motors). There is also a division into bistable and monostable versions. Bistable relays, as the name suggests, do not change their state after disconnecting the control voltage.

Nominal coil voltage - the optimum voltage that must be applied to the coil for the relay to perform its function. A voltage that is too low will be insufficient to run the circuit, while a voltage that is too high can damage the electromagnet. The distinction between AC and DC operated systems is also important here.

Maximum switching voltage - the highest potential difference that can occur in the controlled circuit. Exceeding this value may result not only in damage to the relay, but also in electrical breakdown and failure of the controller (this in turn poses a risk to the health and life of the operators!). The same applies to the Maximum load capacity of AC contacts.

Mounting, size, and pitch - relays usually have a characteristic pin pitch, which prevents their incorrect mounting. For PCB mounted components, the output layout is usually compatible with typical pitches (2.54 mm, 5.08 mm, etc.). There are also surface-mount (SMT) relays. However, in the case of industrial solutions, we most often encounter base-mounted elements - this makes it easier to replace the relay and minimises the resistance of the connections.

Coil resistance - this parameter allows you to determine the energy consumption to be expected when using the component. It also makes it possible to estimate whether the relay will not overheat.

Products: 11 177

Warehouse:

TME
External
All
Page 1
6-1393243-8 | Relay: electromagnetic; Ucoil: 24VDC; DPDT; 8A; 8A/250VAC; 8A/30VDC
Relay: electromagnetic; Ucoil: 24VDC; DPDT; 8A; 8A/250VAC; 8A/30VDC
Manufacturer part number: 6-1393243-8
Manufacturer: TE Connectivity
Net price for quantities from 1 pcs - 2.54 USDGross price for quantities from 1 pcs - 2.54 USD
Net price for quantities from 10 pcs - 2.32 USDGross price for quantities from 10 pcs - 2.32 USD
Net price for quantities from 20 pcs - 2.21 USDGross price for quantities from 20 pcs - 2.21 USD
Net price for quantities from 40 pcs - 1.88 USDGross price for quantities from 40 pcs - 1.88 USD
Net price for quantities from 100 pcs - 1.66 USDGross price for quantities from 100 pcs - 1.66 USD
Net price for quantities from 1000 pcs - 1.44 USDGross price for quantities from 1000 pcs - 1.44 USD
Net price for quantities from 1500 pcs - 1.40 USDGross price for quantities from 1500 pcs - 1.40 USD
26929 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
34.51.7.024.0010 | Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 6A; 5ms
Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 6A; 5ms
Manufacturer part number: 34.51.7.024.0010
Manufacturer: FINDER
Net price for quantities from 1 pcs - 5.48 USDGross price for quantities from 1 pcs - 5.48 USD
Net price for quantities from 40 pcs - 4.93 USDGross price for quantities from 40 pcs - 4.93 USD
Net price for quantities from 60 pcs - 4.81 USDGross price for quantities from 60 pcs - 4.81 USD
10742 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
6-1393243-3 | Relay: electromagnetic; Ucoil: 12VDC; DPDT; 8A; 8A/250VAC; 8A/30VDC
Relay: electromagnetic; Ucoil: 12VDC; DPDT; 8A; 8A/250VAC; 8A/30VDC
Manufacturer part number: 6-1393243-3
Manufacturer: TE Connectivity
Net price for quantities from 1 pcs - 3.84 USDGross price for quantities from 1 pcs - 3.84 USD
Net price for quantities from 10 pcs - 3.49 USDGross price for quantities from 10 pcs - 3.49 USD
Net price for quantities from 20 pcs - 3.15 USDGross price for quantities from 20 pcs - 3.15 USD
Net price for quantities from 40 pcs - 2.73 USDGross price for quantities from 40 pcs - 2.73 USD
Net price for quantities from 80 pcs - 2.63 USDGross price for quantities from 80 pcs - 2.63 USD
37660 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LEG-12F | Relay: electromagnetic; Ucoil: 12VDC; SPDT; Icontacts max: 15A
Relay: electromagnetic; Ucoil: 12VDC; SPDT; Icontacts max: 15A
Manufacturer part number: LEG-12F
Net price for quantities from 1 pcs - 0.61 USDGross price for quantities from 1 pcs - 0.61 USD
Net price for quantities from 10 pcs - 0.55 USDGross price for quantities from 10 pcs - 0.55 USD
Net price for quantities from 50 pcs - 0.46 USDGross price for quantities from 50 pcs - 0.46 USD
Net price for quantities from 300 pcs - 0.41 USDGross price for quantities from 300 pcs - 0.41 USD
Net price for quantities from 1000 pcs - 0.35 USDGross price for quantities from 1000 pcs - 0.35 USD
33803 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RM84-2012-35-1024 | Relay: electromagnetic; Ucoil: 24VDC; DPDT; 8A; 8A/250VAC; 8A/24VDC
Relay: electromagnetic; Ucoil: 24VDC; DPDT; 8A; 8A/250VAC; 8A/24VDC
Manufacturer part number: RM84-2012-35-1024
Manufacturer: RELPOL
Net price for quantities from 1 pcs - 1.68 USDGross price for quantities from 1 pcs - 1.68 USD
Net price for quantities from 5 pcs - 1.45 USDGross price for quantities from 5 pcs - 1.45 USD
Net price for quantities from 20 pcs - 1.43 USDGross price for quantities from 20 pcs - 1.43 USD
11067 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LEG-12 | Relay: electromagnetic; Ucoil: 12VDC; SPDT; Icontacts max: 10A
Relay: electromagnetic; Ucoil: 12VDC; SPDT; Icontacts max: 10A
Manufacturer part number: LEG-12
Net price for quantities from 2 pcs - 0.65 USDGross price for quantities from 2 pcs - 0.65 USD
Net price for quantities from 10 pcs - 0.58 USDGross price for quantities from 10 pcs - 0.58 USD
Net price for quantities from 50 pcs - 0.49 USDGross price for quantities from 50 pcs - 0.49 USD
Net price for quantities from 300 pcs - 0.44 USDGross price for quantities from 300 pcs - 0.44 USD
Net price for quantities from 1000 pcs - 0.37 USDGross price for quantities from 1000 pcs - 0.37 USD
76967 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 2.
Multiplicity: 1.
7-1393243-9 | Relay: electromagnetic; Ucoil: 230VAC; DPDT; 8A; 8A/250VAC; RT2
Relay: electromagnetic; Ucoil: 230VAC; DPDT; 8A; 8A/250VAC; RT2
Manufacturer part number: 7-1393243-9
Manufacturer: TE Connectivity
Net price for quantities from 1 pcs - 5.11 USDGross price for quantities from 1 pcs - 5.11 USD
Net price for quantities from 10 pcs - 4.85 USDGross price for quantities from 10 pcs - 4.85 USD
Net price for quantities from 14 pcs - 4.77 USDGross price for quantities from 14 pcs - 4.77 USD
Net price for quantities from 20 pcs - 4.62 USDGross price for quantities from 20 pcs - 4.62 USD
Net price for quantities from 40 pcs - 4.32 USDGross price for quantities from 40 pcs - 4.32 USD
Net price for quantities from 60 pcs - 4.17 USDGross price for quantities from 60 pcs - 4.17 USD
Net price for quantities from 80 pcs - 4.04 USDGross price for quantities from 80 pcs - 4.04 USD
Net price for quantities from 100 pcs - 3.96 USDGross price for quantities from 100 pcs - 3.96 USD
29623 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
40.52.9.024.0000 | Relay: electromagnetic; Ucoil: 24VDC; DPDT; Icontacts max: 15A
Relay: electromagnetic; Ucoil: 24VDC; DPDT; Icontacts max: 15A
Manufacturer part number: 40.52.9.024.0000
Manufacturer: FINDER
Net price for quantities from 1 pcs - 6.53 USDGross price for quantities from 1 pcs - 6.53 USD
Net price for quantities from 10 pcs - 5.83 USDGross price for quantities from 10 pcs - 5.83 USD
Net price for quantities from 50 pcs - 5.02 USDGross price for quantities from 50 pcs - 5.02 USD
3049 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LEG-24 | Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 10A
Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 10A
Manufacturer part number: LEG-24
Net price for quantities from 1 pcs - 0.61 USDGross price for quantities from 1 pcs - 0.61 USD
Net price for quantities from 12 pcs - 0.55 USDGross price for quantities from 12 pcs - 0.55 USD
Net price for quantities from 48 pcs - 0.46 USDGross price for quantities from 48 pcs - 0.46 USD
Net price for quantities from 300 pcs - 0.41 USDGross price for quantities from 300 pcs - 0.41 USD
Net price for quantities from 1000 pcs - 0.35 USDGross price for quantities from 1000 pcs - 0.35 USD
35184 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RM84-2012-35-1012 | Relay: electromagnetic; Ucoil: 12VDC; DPDT; 8A; 8A/250VAC; 8A/24VDC
Relay: electromagnetic; Ucoil: 12VDC; DPDT; 8A; 8A/250VAC; 8A/24VDC
Manufacturer part number: RM84-2012-35-1012
Manufacturer: RELPOL
Net price for quantities from 1 pcs - 2.25 USDGross price for quantities from 1 pcs - 2.25 USD
Net price for quantities from 5 pcs - 1.93 USDGross price for quantities from 5 pcs - 1.93 USD
Net price for quantities from 20 pcs - 1.54 USDGross price for quantities from 20 pcs - 1.54 USD
Net price for quantities from 500 pcs - 1.47 USDGross price for quantities from 500 pcs - 1.47 USD
9535 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
ALDP124 | Relay: electromagnetic; Ucoil: 24VDC; SPST-NO; Icontacts max: 5A
Relay: electromagnetic; Ucoil: 24VDC; SPST-NO; Icontacts max: 5A
Manufacturer part number: ALDP124
Manufacturer: PANASONIC
Net price for quantities from 1 pcs - 1.28 USDGross price for quantities from 1 pcs - 1.28 USD
Net price for quantities from 10 pcs - 1.20 USDGross price for quantities from 10 pcs - 1.20 USD
Net price for quantities from 25 pcs - 1.15 USDGross price for quantities from 25 pcs - 1.15 USD
Net price for quantities from 50 pcs - 1.11 USDGross price for quantities from 50 pcs - 1.11 USD
Net price for quantities from 100 pcs - 1.07 USDGross price for quantities from 100 pcs - 1.07 USD
Net price for quantities from 200 pcs - 1.02 USDGross price for quantities from 200 pcs - 1.02 USD
Net price for quantities from 500 pcs - 0.98 USDGross price for quantities from 500 pcs - 0.98 USD
Net price for quantities from 5000 pcs - 0.86 USDGross price for quantities from 5000 pcs - 0.86 USD
14312 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
9-1393239-8 | Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 16A
Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 16A
Manufacturer part number: 9-1393239-8
Manufacturer: TE Connectivity
Net price for quantities from 1 pcs - 2.04 USDGross price for quantities from 1 pcs - 2.04 USD
Net price for quantities from 20 pcs - 1.92 USDGross price for quantities from 20 pcs - 1.92 USD
Net price for quantities from 60 pcs - 1.79 USDGross price for quantities from 60 pcs - 1.79 USD
Net price for quantities from 100 pcs - 1.66 USDGross price for quantities from 100 pcs - 1.66 USD
34373 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
AZ822-2C-12DSE | Relay: electromagnetic; Ucoil: 12VDC; DPDT; 2A; 0.5A/120VAC; AZ822
Relay: electromagnetic; Ucoil: 12VDC; DPDT; 2A; 0.5A/120VAC; AZ822
Manufacturer part number: AZ822-2C-12DSE
Manufacturer: ZETTLER
Net price for quantities from 1 pcs - 0.98 USDGross price for quantities from 1 pcs - 0.98 USD
Net price for quantities from 20 pcs - 0.89 USDGross price for quantities from 20 pcs - 0.89 USD
Net price for quantities from 40 pcs - 0.84 USDGross price for quantities from 40 pcs - 0.84 USD
Net price for quantities from 100 pcs - 0.77 USDGross price for quantities from 100 pcs - 0.77 USD
Net price for quantities from 200 pcs - 0.72 USDGross price for quantities from 200 pcs - 0.72 USD
Net price for quantities from 260 pcs - 0.70 USDGross price for quantities from 260 pcs - 0.70 USD
Net price for quantities from 500 pcs - 0.68 USDGross price for quantities from 500 pcs - 0.68 USD
24751 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
AZ822-2C-24DSE | Relay: electromagnetic; Ucoil: 24VDC; DPDT; 2A; 0.5A/120VAC; AZ822
Relay: electromagnetic; Ucoil: 24VDC; DPDT; 2A; 0.5A/120VAC; AZ822
Manufacturer part number: AZ822-2C-24DSE
Manufacturer: ZETTLER
Net price for quantities from 1 pcs - 0.99 USDGross price for quantities from 1 pcs - 0.99 USD
Net price for quantities from 20 pcs - 0.90 USDGross price for quantities from 20 pcs - 0.90 USD
Net price for quantities from 40 pcs - 0.85 USDGross price for quantities from 40 pcs - 0.85 USD
Net price for quantities from 60 pcs - 0.83 USDGross price for quantities from 60 pcs - 0.83 USD
Net price for quantities from 100 pcs - 0.79 USDGross price for quantities from 100 pcs - 0.79 USD
Net price for quantities from 200 pcs - 0.78 USDGross price for quantities from 200 pcs - 0.78 USD
24445 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
RM85-2011-35-1012 | Relay: electromagnetic; Ucoil: 12VDC; SPDT; Icontacts max: 16A
Relay: electromagnetic; Ucoil: 12VDC; SPDT; Icontacts max: 16A
Manufacturer part number: RM85-2011-35-1012
Manufacturer: RELPOL
Net price for quantities from 1 pcs - 7.12 USDGross price for quantities from 1 pcs - 7.12 USD
Net price for quantities from 5 pcs - 3.03 USDGross price for quantities from 5 pcs - 3.03 USD
Net price for quantities from 10 pcs - 2.05 USDGross price for quantities from 10 pcs - 2.05 USD
Net price for quantities from 20 pcs - 1.59 USDGross price for quantities from 20 pcs - 1.59 USD
Net price for quantities from 40 pcs - 1.52 USDGross price for quantities from 40 pcs - 1.52 USD
11628 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
AZ943-1CH-12DE | Relay: electromagnetic; Ucoil: 12VDC; SPDT; 15A; 10A/277VAC; AZ943
Relay: electromagnetic; Ucoil: 12VDC; SPDT; 15A; 10A/277VAC; AZ943
Manufacturer part number: AZ943-1CH-12DE
Manufacturer: ZETTLER
Net price for quantities from 1 pcs - 0.65 USDGross price for quantities from 1 pcs - 0.65 USD
Net price for quantities from 20 pcs - 0.60 USDGross price for quantities from 20 pcs - 0.60 USD
Net price for quantities from 40 pcs - 0.56 USDGross price for quantities from 40 pcs - 0.56 USD
Net price for quantities from 60 pcs - 0.55 USDGross price for quantities from 60 pcs - 0.55 USD
Net price for quantities from 100 pcs - 0.52 USDGross price for quantities from 100 pcs - 0.52 USD
Net price for quantities from 260 pcs - 0.50 USDGross price for quantities from 260 pcs - 0.50 USD
14592 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
2961105 | Relay: miniature; Ucoil: 24VDC; SPDT; Icontacts max: 6A; 3A/230VAC
Relay: miniature; Ucoil: 24VDC; SPDT; Icontacts max: 6A; 3A/230VAC
Manufacturer part number: 2961105
Manufacturer: PHOENIX CONTACT
Net price for quantities from 1 pcs - 6.71 USDGross price for quantities from 1 pcs - 6.71 USD
Net price for quantities from 10 pcs - 6.25 USDGross price for quantities from 10 pcs - 6.25 USD
Net price for quantities from 50 pcs - 5.82 USDGross price for quantities from 50 pcs - 5.82 USD
Net price for quantities from 100 pcs - 5.36 USDGross price for quantities from 100 pcs - 5.36 USD
3953 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
AZ943-1CH-24DE | Relay: electromagnetic; Ucoil: 24VDC; SPDT; 15A; 10A/277VAC; AZ943
Relay: electromagnetic; Ucoil: 24VDC; SPDT; 15A; 10A/277VAC; AZ943
Manufacturer part number: AZ943-1CH-24DE
Manufacturer: ZETTLER
Net price for quantities from 1 pcs - 0.70 USDGross price for quantities from 1 pcs - 0.70 USD
Net price for quantities from 20 pcs - 0.64 USDGross price for quantities from 20 pcs - 0.64 USD
Net price for quantities from 500 pcs - 0.55 USDGross price for quantities from 500 pcs - 0.55 USD
18124 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
LEG-24F | Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 15A
Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 15A
Manufacturer part number: LEG-24F
Net price for quantities from 2 pcs - 0.74 USDGross price for quantities from 2 pcs - 0.74 USD
Net price for quantities from 10 pcs - 0.64 USDGross price for quantities from 10 pcs - 0.64 USD
Net price for quantities from 50 pcs - 0.52 USDGross price for quantities from 50 pcs - 0.52 USD
Net price for quantities from 300 pcs - 0.44 USDGross price for quantities from 300 pcs - 0.44 USD
Net price for quantities from 1000 pcs - 0.39 USDGross price for quantities from 1000 pcs - 0.39 USD
38089 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 2.
Multiplicity: 1.
AZ6991-1C-12DE | Relay: electromagnetic; Ucoil: 12VDC; SPDT; 8A; 6A/277VAC; 6A/30VDC
Relay: electromagnetic; Ucoil: 12VDC; SPDT; 8A; 6A/277VAC; 6A/30VDC
Manufacturer part number: AZ6991-1C-12DE
Manufacturer: ZETTLER
Net price for quantities from 1 pcs - 1.55 USDGross price for quantities from 1 pcs - 1.55 USD
Net price for quantities from 10 pcs - 1.43 USDGross price for quantities from 10 pcs - 1.43 USD
Net price for quantities from 25 pcs - 1.35 USDGross price for quantities from 25 pcs - 1.35 USD
Net price for quantities from 50 pcs - 1.28 USDGross price for quantities from 50 pcs - 1.28 USD
Net price for quantities from 100 pcs - 1.26 USDGross price for quantities from 100 pcs - 1.26 USD
17162 in TME stock