+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

FPGA - definition

FPGA (Field-Programmable Gate Array) is a type of digital integrated circuit whose logic structure can be configured by the user after manufacturing. It consists of a grid of programmable logic blocks that can be interconnected via reconfigurable internal routing, enabling the creation of complex digital systems that perform specific logic, arithmetic, control, or signal processing functions.

The architecture of an FPGA allows for the parallel execution of multiple operations, making it particularly effective in applications requiring high performance along with design flexibility. These devices are often used as alternatives to ASICs in prototyping, embedded systems, industrial equipment, and aerospace applications, where the ability to quickly adapt logic without producing a new fabrication mask is essential.

FPGA programming is carried out using hardware description languages such as [VHDL](/en/news/library-articles/page/69822/ or Verilog, which allow for the precise definition of the circuit’s logic structure. Once programmed, the internal configuration is loaded into the device’s configuration memory, initiating connections and logic functions in accordance with the user’s design. Modern FPGAs may also include dedicated hardware blocks such as multipliers, RAM blocks, communication interfaces, or embedded processor cores, significantly expanding their capabilities.

Thanks to their field reconfigurability and high degree of parallelism, FPGAs play a crucial role in the design of advanced digital systems. Their flexibility and versatility enable the implementation of complex algorithms in real time, with applications in image processing, data encryption, high-throughput communication, and control systems.

FPGA

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO