+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
The Ruhmkorff Coils is a type of spark inductor, belonging to the class of interrupter induction transformers, which is used to generate a high impulse voltage from a low-voltage direct current source. This device was developed in the mid-19th century by German designer Heinrich Ruhmkorff, based on earlier work by William Sturgeon and Nicholas Callan. Its primary use was to power discharge tubes and generate sparks in experiments with electricity and vacuum.
The construction of the Ruhmkorff coil is based on two windings - a primary with a small number of turns and a secondary containing tens of thousands of turns of thin wire. Both windings are wound on a common core made of soft iron, usually in the form of rods grouped in a package. Coils' operation is based on the phenomenon of electromagnetic induction. The rapid interruption of current in the primary winding - realised by means of a mechanical interrupter - causes an alternating magnetic field, which induces high-voltage pulses in the secondary winding. In order to increase efficiency and to protect against arcing, an extinguishing capacitor was often used in the circuit.
The Ruhmkorff coil was widely used in physical experiments, as well as in wireless telegraphy, X-ray tubes and as an ignition element in internal combustion engines, before it was superseded by more advanced Instrumentation. Today, it remains mainly a historical and teaching object, used in demonstrations in electromagnetism.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.