You are browsing international version of the website. Based on location data, the suggested version of the page for you is USA / US

+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Magnetron - definition

The Magnetron is a high-voltage electron tube generating microwaves, whose operation is based on the movement of electrons in an electric and magnetic field, in a closed resonant structure. It is an oscillating device capable of converting electrical energy into electromagnetic radiation at frequencies of the order of gigahertz, used mainly in radar technology, microwave telecommunications and microwave ovens.

The basic design of the magnetron consists of a cylindrical cathode, located in the central part of the device, and a surrounding anode in the form of a ring containing resonant cavities. The space between the electrodes is in a vacuum, and the whole is placed in a magnetic field perpendicular to the plane of electron motion. Electrons emitted from the cathode under the influence of the magnetic field move along curved paths and interact with the resonant cavities of the anode, leading to the excitation of electromagnetic oscillations.

The excited electromagnetic waves are collected from one of the cavities and output via a waveguide. The frequency of the generated signal depends on the geometry of the resonator and the supply voltage. Magnetrons operate in autogenerated mode, meaning that they sustain the oscillations themselves without the need for an external excitation signal. Although they do not offer precise frequency control like other microwave generators, they stand out for their high power and simplicity of design.

In technical applications, magnetrons are used, among others, in radar systems to emit short pulses of high power, in industrial equipment for drying and processing materials, and in households as a source of microwave energy in cookers. Modern designs can be modified to stabilise operation, improve efficiency and integrate with modern control systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO