+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
*An Application Programming Interface* (API) is a set of defined methods, data structures, protocols and tools that enable communication between different software components. An API acts as an intermediary layer that provides specific functionality to a system, service, library or application in a standardised way that is independent of the internal implementation. This allows developers to use ready-made resources or functions without having to learn the details of their operation.
Technically, an API defines how software components can call each other and exchange data, both locally and in distributed environments. In operating systems, APIs provide functions that allow access to hardware, file management or user interface support. In the context of web applications, APIs enable integration with external services such as payment systems, maps, databases or social media platforms. A key feature is the provision of abstraction - an API user can use its functions without having access to source code or having to interfere with the system logic.
Modern APIs are often based on web architectures such as REST (Representational State Transfer) or GraphQL, and use HTTP protocols and JSON or XML data formats. APIs can be public, private or partnered - depending on the extent of availability and the purpose of the integration. The API documentation defines the available resources, request and response formats, authorisation rules and possible usage limits.
A well-designed API is characterised by consistency, transparency and resilience to changes in the host system. Its role is fundamental to the creation of scalable and modular information systems, enabling the construction of multilayer applications, services in microservices architecture and ecosystems based on the sharing of functions and data between different entities.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.