+1 300 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Date of publication: 21-03-2025 🕒 5 min read
Inductance is one of the basic concepts in electrical engineering and electronics, describing the ability of an object (often a coil) to store energy in the form of a magnetic field, when current flows through it. Inductance is measured in henries (H). Inductance has important applications in many technologies, including transformers, electric motors, power transmission systems and many other electrical engineering devices and systems. In this article we will discuss issues such as:
The phenomenon of electromagnetic induction was discovered by Michael Faraday in 1831 and is described by Faraday's law of electromagnetic induction. This law states that the induced voltage in any circuit is equal to the rate of change of magnetic flux through the circuit.
Inductance in circuits is crucial in many aspects of electrical and electronic engineering. Here are some basic points about the role of inductance in circuits
Understanding inductance and its effect on circuits is key to the design and analysis of many electronic and electrical engineering systems.
Electromagnetic induction occurs when, the flux of a magnetic field through a certain area. This phenomenon can be caused by:
The value of magnetic induction is a measure of the intensity of the magnetic field in a given space. The value of magnetic induction depends on many factors:
There are many ways to model and calculate the value of magnetic induction in different situations, from simple formulas for specific geometric configurations, to complex computer simulations for more complex situations.
The phenomena of self-induction and mutual induction are two basic types of electromagnetic induction.
This phenomenon occurs in a circuit, when the current in that circuit changes. The change in current leads to a change in the magnetic field flux inside that circuit.
This change in magnetic flux induces a voltage in the same circuit, which acts in the opposite direction to the change in current, according to Lenz's law.
An example of an element in which the phenomenon of self-induction occurs is a coil
This phenomenon occurs between two circuits, when a change in current in one circuit leads to an induction of voltage in a neighboring circuit.
When the current in one circuit (e.g., the primary coil of a transformer) changes, this causes a change in the magnetic field flux. If a second circuit (e.g., the secondary coil of a transformer) is near, this changing magnetic field flux crosses this second circuit, inducing a voltage in it.
The value of the induced voltage in the second circuit depends on the rate of change of current in the first circuit and on the configuration and properties of both circuits.
To summarize:
Intrinsic induction refers to the induced voltage in a circuit resulting from a change in current in the same circuit.
Mutual induction refers to the induced voltage in one circuit resulting from a change in current in a neighboring circuit.
Both of these phenomena are crucial in electrical engineering.
Yes, mutual inductance can take on negative values, depending on the mutual orientation and winding direction of the coils. Mutual inductance describes the ability of one coil to induce a voltage in a second coil as a result of a change in current in the first coil.
The direction of the induced voltage depends on the orientation of the coils relative to each other and the direction of winding. If the coils are wound in such a way, that the induced voltage in one coil acts in the opposite direction to the change in current in the other coil, the mutual inductance will be negative.
For example, if we have two parallel wires, current flowing in one direction in one wire induces a voltage in the other wire in the same direction. However, if the current in one wire flows in the opposite direction, the induced voltage will be in the opposite direction.
Negative mutual inductance is often found in cases, where the coils are wound in opposite directions or have opposite orientation with respect to each other.
In practical applications, when designing devices with coils of known mutual inductance, it is important to understand and consider the winding direction and orientation of the coils, to ensure the desired system behavior.
The inductance of a coil depends on many factors, such as the number of turns, the shape of the coil, its dimensions and the material of the core. For a solenoid coil (that is, a long, cylindrical coil) with uniform coils and an air core, the inductance L can be calculated using the following formula:
where:
For elements with a core other than air, the value should be replaced by the magnetic permeability of the material, which is the product of and the relative permeability of the material, of which the core is built. It is also worth noting, that this formula is an approximation and assumes an ideal solenoidal coil geometry. In reality, there may be various factors, such as skewed coils, boundary effects and non-uniform magnetic field, that affect the exact value of the coil's inductance. In more complex cases, calculations may require more complicated methods or computer simulations. It is also worth adding, that there are actually other issues that affect the value of inductance. We are talking about losses, parasitic capacitance, or even the way the coils are wound. For more information about coils, see the article.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,300,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.