+1 300 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Date of publication: 30-04-2026 🕒 17 min read
Allen spanners, are small but extremely versatile hand tools. They are used to tighten and loosen hexagon socket bolts found in furniture, bicycles, electronic devices and industrial structures, among others. Although deceptively simple, their improper fit or the use of a low-quality version can lead to problems such as rounding of the socket or loss of fastening effectiveness.
Highlights at a glance:Here is an abbreviated list of the most important and reliable information to remember after reading an article about allen spanners:
Depending on the needs of the user and the specific work to be carried out, allen keys are available in several design variants. Each offers different capabilities in terms of ergonomics, torque or access to hard-to-reach bolts. Below, we discuss the two most common types - the classic allen spanner and more advanced solutions with a handle.
This is the basic and most common version of the hexagonal hex key, made of a uniform steel bar with a hexagonal cross-section, bent at a right angle. This shape allows two-sided use - the shorter arm provides higher torque, while the longer arm allows easier access to deeper-set bolts. L-shaped spanners are lightweight, compact and work well in most applications, especially where precision and mobility are important.
For those doing repetitive tasks that require more force, spanners with a T-handle or screwdriver version are a convenient solution. The handle allows for a more secure grip and makes it easier to apply force when tightening or loosening bolts, which translates into comfort. Tools of this type are often used in bicycle repair shops, precision mechanics and industrial services.However, please note that the larger size and design of the handle may make it difficult to work in tight spaces, where a classic T-handle spanner will perform better.
Spanners fitted with a ball-end allow the spanner axis to be worked at an offset from the bolt axis, usually up to an angle of 25-30 degrees. This is a very practical solution, especially when access to the bolt is obstructed by Enclosures, frames or other structural elements. It allows you to start screwing or unscrewing without having to position the Tools perfectly in the axis of the socket.
It is worth bearing in mind, however, that a ball end does not provide as good an interlock as a classic flat profile. If more torque is applied, there is a risk of the spanner slipping out of the socket or damaging the bit itself, especially in smaller sizes. For this reason, ball-ended Allen keys are not recommended for heavy tightening or for first loosening of seized connections.
For mobile users and field service providers, Allen keys have also been developed in the form of folding "pocket knives", as well as sockets and bits for use with screwdrivers, ratchets or magnetic handles. These types of solutions are extremely compact and allow quick access to multiple spanner sizes in a single tool.
Their biggest advantage is their mobility - they are easy to store in a pocket, tool bag or bicycle case. The downside can be less precision working, limited leverage and difficulty reaching deep sockets, especially with folding models. In situations where the spanner has to work with a lot of force or has to reach hard-to-reach bolts, classic tools prove to be more effective.
Choosing the right size of allen spanner is crucial not only for the effectiveness of the job, but also for protecting fasteners from damage. Although at first glance the differences between some sizes may seem insignificant, even a minimal amount of play in the socket can lead to it growing. This is why it is so important to understand how the size designation system works and how to correctly select a spanner for a particular joint.
There are two main size systems on the market - metric, popular in Europe, and inch (SAE), widely used in the US and in some industries. Metric spanners are marked in millimetres and their sizes usually range from 0.7 mm to 22 mm. The standard for this is ISO 2936.
The inch system is based on fractions of an inch and its specification is defined by the ASME B18.3 standard. Typical sizes start at 0.028" and go up to 3/4". In practice, spanners from 1/16" to 3/8" are most common.
Dangerous situations arise when trying to use a spanner from one system for a bolt designed in another. Some of the sizes are sometimes very close to each other, which can lead to a mis-match. For example:
Although they may seem suitable at first, such pairs lead to increased play and rapid socket edge wiping.
To ensure maximum grip and avoid the risk of damage to the bolt, it is important to select a spanner that exactly matches the size of the socket. The size is measured "across flats", i.e. between two parallel, flat sides of the hexagon. This is the value that determines the compatibility of the spanner with the socket in question.
For an accurate measurement, it is best to use a caliper, which can accurately determine the width of the inner socket or the key itself. Alternatively, a hex gauge can be used, which works by matching the gauges to the bolt size.
There is always a risk in using a spanner that is marginally too small. In practice, this leads to a situation where only part of the surface is in contact with the socket. This in turn results in point pressure concentration, microscopic edge shearing and ultimately rounding of the socket. Bolts destroyed in this way are difficult to remove and often require the use of specialised extraction tools.
For this reason, it is advisable to avoid 'by eye' solutions and always choose a spanner with a perfect fit - even if the difference seems negligible.
The material from which an allen key is made largely determines its durability, resistance to deformation and comfort of use. The choice is not only limited to the type of steel. Heat treatment processes and the type of Protective Coatings used also play an important role. It is useful to know the differences between the available variants in order to select the right Tools for specific applications and expectations.
The cheapest spanners are made from ordinary carbon steel. These are sufficient for occasional, light work, but with more intensive use they quickly wear, wear out or bend. Much better performance is provided by chrome vanadium alloy steel (Cr-V), which has good deformation resistance and is the standard in the medium class of hand tools.
Even higher strength is offered by chrome-molybdenum (Cr-Mo), used most often in professional workshops where the spanner is operated at high torque. The most advanced option is type S2 tool steel, which undergoes a special hardening process. This type of material combines high hardness with resistance to cracking, even under heavy loads.
It is worth going for allen spanners made from premium materials when tools are used frequently, for demanding connections or in service applications, where their failure can cause delays or additional costs.
The surface of a spanner is not only aesthetically important, but above all practical. The right coating protects against corrosion, improves grip in the hand and increases the life of the Tools. The most common are:
The right coating is particularly important in environments exposed to moisture, dust or aggressive chemicals. In workshop applications, spanners with a blackened or phosphated surface are best suited.
In addition to the material and finish itself, an important difference is the quality of the workmanship - especially in terms of dimensional tolerances and ergonomics. Professional spanners feature a precision-machined cross-section, which ensures a better fit in the socket and reduces the risk of damage. Such Tools are often equipped with comfortable Handles, size markings and are available in extensive sets that also include ball, short or socket versions.
In comparison, budget spanners often have looser tolerances, which can result in edge wear after just a few uses. Their ergonomics can be limited and sets focus on basic sizes, with no specialised options.
| Feature | Professional spanners | Budget spanners |
|---|---|---|
| Material | Cr-V, Cr-Mo, S2 tool steel | Carbon steel or low-quality alloy |
| Dimensional tolerances | very accurate, near perfect fit | greater play, risk of socket damage |
| Protective Coatings | blackening, chrome, phosphating | often none or simply painted |
| Ergonomics | Handles, markings, better grip | no handles, limited comfort |
| Range of sets | full sizes, ball end pieces, sockets | basic sizes in L-shape |
For occasional users, cheaper spanners may be sufficient. For professional or service applications, it is far better to invest in a higher quality set - especially in the most commonly used sizes.
Although allen spanners are mainly associated with furniture assembly, their use goes far beyond the home workshop. Due to their simple design, small size and effective performance, they are used in a wide range of fields - from bicycles and automobiles to electronics and precision mechanics. Below, we discuss the most common areas where the use of Allen screws is an everyday occurrence.
For self-assembly furniture (also known as RTA - ready to assemble), Allen keys are a standard tool included in the kit. Simple L-form constructions with small dimensions allow users without experience to assemble cabinets, tables or shelves efficiently.
It is worth bearing in mind, however, that the tools supplied by furniture manufacturers tend to be of low quality and usually intended for one-off use. For more frequent assembly or working with harder materials, sturdier, full-size Allen spanners or Handles models are better suited.
On bicycles, allen spanners are indispensable for adjusting and removing almost all components - from bridges and saddles to brake calipers or derailleur mechanisms. Their small size allows easy access to bolts even in dense areas.
In the automotive sector, Allen keys are used to service fuel systems, valve covers or vehicle interior components. Due to the considerably higher forces involved in bolted connections, it is crucial that the correct tightening torque is maintained here. The use of Torque Wrenches with Allen bits avoids damage to the threads and ensures operational safety.
In electronic devices, laboratory apparatus or Measuring Instruments, allen spanners are used for working with very small bolts. Typical applications are the fixing of shields, Heatsinks, Enclosures or Connectors Integrated circuits.
In these situations, it is crucial to use appropriately sized bits (often in the form of precision bits) that allow delicate and controlled work without risking damage to small components. Torque screwdrivers are also useful here and tools with small working diameters that allow manoeuvring in confined spaces.
In order for an Allen spanner to work properly and serve for a long time, it is not enough just to ensure that it is the right size. Equally important is the technique of its use, attention to the condition of the bolts and sockets, and proper storage of the tool. Incorrect use can lead to socketing, damage to Tools and, in extreme cases, accidents during operation. Below we discuss the principles that help to keep imbibers safe and effective in everyday use.
To avoid damaging a bolt or spanner, the first thing to do is to use a tool of exactly the right size. The spanner should be inserted as far as it will go so that the entire length of the shank works evenly with the socket surface. Working at an angle or only on part of the surface will result in point pressure and rapid wear.
It is also important to direct the force of torque application axially relative to the bolt. Tightening from the side or by force can lead to bending of the spanner or breakage of the socket. When tightening - especially parts made of aluminium, plastic or screwed into soft materials - excessive torque should be avoided. When exact values are required, it is advisable to reach for Torque Tools.
A contaminated socket, even with fine sand or dust, increases the risk of the spanner slipping. Before starting work, it is a good idea to remove dirt from it - for example with compressed air or a soft brush. In some situations, especially with bolts that have not been used for a long time, it can be helpful to apply a little grease or penetrating oil.
Lubrication reduces friction, makes it easier to insert the spanner and reduces the risk of rounding the edges of the socket. It is a good idea to wipe down both the spanner and bolt after use, especially if the equipment will be stored for a long time.
Imbues, although small, are easily lost or damaged by inadequate storage. It is best to keep them in their original handle, case or marked case, which makes it easier to identify sizes and prevents accidental confusion between the metric and inch systems.
To prevent corrosion, keys should be stored in a dry place and occasionally wiped down with a lightly oiled cloth. Worn, rounded bits should not be used - not only do they impair the effectiveness of the work, they can also lead to permanent damage to the bolts. It is worth inspecting them regularly and replacing the most commonly used sizes before they become problematic.
Even with careful and correct use, problematic situations can arise when working with allen spanners. These most often relate to damaged bolt sockets that become difficult to unscrew or completely blocked. These cases usually occur due to incorrect tool selection, haste or material wear.
The most common damage encountered when working with bolts is so-called stripping, i.e. rounding of the edge of the bolt socket. This occurs when the spanner used is too small or loose in cross-section, is worn, or has not been inserted all the way in. This results in an uneven distribution of force and shearing of the edge, which over time leads to an oval-shaped hole where the tool no longer has grip.
Another factor contributing to socket deformation is the non-axial application of force and attempts to loosen baked-on bolts without first loosening them. A damaged socket not only prevents further tightening or disassembly, but often requires the use of special tools or even replacement of the entire component.
In the case of a damaged socket, there are several emergency methods that can help to remove it. One popular technique is to use a Torx spanner of a slightly larger size, which, when pushed or driven into the deformed socket, can make good enough contact to allow unscrewing.
If this method fails, other solutions can be considered, such as:
All of these methods involve the risk of damaging surrounding components or the material itself, so it is only worth using them when conventional methods fail. Before proceeding with such measures, it is a good idea to assess whether the component from which you wish to remove the bolt will be irreparably damaged.
Although Hex and Torx keys are sometimes confused with each other, especially by novice users, the differences between the two are important both in terms of construction and application. Both systems are commonly used in assembly technology, but each was designed with different construction requirements in mind.
The main difference between an allen and Torx spanner is the shape of the socket. The Allen uses a classic hexagon with equal sides, while the Torx is based on a six-pointed star pattern with rounded edges. This geometry not only affects the appearance, but also the way force is transmitted.
The Torx socket provides a larger contact area between Tools and Bolts, allowing for more efficient torque transfer without the risk of slippage. This allows higher forces to be applied with less wear on both tool and socket. The Allen, despite its simplicity, has a tendency to apply point pressure, which can lead to faster edge wear - especially with a poor fit.
Despite the visual similarities and similar sizes, using an Allen key in a Torx bolt (or vice versa) is definitely not advisable. These tools are not designed to work with other systems, which means that using them outside of their proper purpose risks damaging both the tool and the bolt.
Exceptions to this are emergency situations where the allen socket is already damaged and the classic spanner has no point of attachment. In such cases, a suitably sized Torx wrench can temporarily act as a 'Screw Extractors' if its arms are able to penetrate the remaining edges of the socket. However, this is an emergency solution that should be used carefully and only when there are no other options.
Although today the allen spanner seems such an obvious tool that it is hard to imagine everyday work in the workshop or furniture assembly without it, its history dates back only to the early 20th century. It was born out of the need to simplify bolt design and improve safety in industry. Others may find it interesting that the tool itself is known by different names depending on the region, and its popularisation was closely linked to the development of mass production and heavy industry.
William G. Allen, an American engineer, is considered to be the creator of the modern hexagonal spanner, having developed the inner socket bolts system and the corresponding spanner in the early 20th century. In 1910, the Allen Manufacturing Company was granted a patent for this system, which quickly became popular in the US as Allen key.
In Europe, the German company Bauer & Schaurte played the biggest role, developing a similar solution in the 1930s, calling it by the acronym INBUS (from Innensechskantschraube Bauer und Schaurte). In Poland, the common name imbus derives from this version.
In turn, Unbrako is a brand of spanners and bolts produced by SPS Technologies, which popularised heavy-duty solutions used in aviation and heavy industry. Today, all these terms - Allen, Allen, INBUS or Unbrako - are sometimes used interchangeably, although technically they refer to different manufacturers or systems.
The introduction of hexagon socket screws has had a major impact on workplace safety and manufacturing efficiency. Traditional external head bolts often protruded above the surface of equipment, posing a risk of catching Clothing or injury during work. The new solution allowed bolts to be installed 'flush' with the surface, significantly improving ergonomics and reducing accidents - especially in rotating machine components.
After the Second World War, Allen spanners began to be used on a mass scale, primarily in the automotive and aerospace industries, as well as in the manufacture of tools and furniture. Their small size, simplicity of construction and ease of storage meant that they quickly became an assembly standard in many countries. Today, it is difficult to imagine any workshop or professional's toolbox without at least a few Allen keys in various sizes.
What is the ball end in an allen key used for?
The ball (ball end) in an allen key allows you to loosen and tighten bolts at an angle, usually up to 25-30°, making it easier to work in hard-to-reach places. It is not suitable for firm tightening - it risks slipping or damaging the socket.
Are ampoule and allen spanners the same thing?
Yes, ampoule and allen spanners are the same tool - both terms refer to hex keys designed for bolts with a hex socket. Others names are due to local language habits.
Are ball end Allen spanners better?
Ball-ended Allen spanners are not better, but complementary. They allow working at an angle, which makes them more convenient in tight places, but they transmit less torque and slip more easily. For heavy tightening, spanners with a classic tip are better.
Is it possible to buy individual allen keys?
Yes, allen keys are available both in sets and as individual pieces - in various sizes, lengths and variations (e.g. with ball end). You can find individual Allen keys in the TME catalogue in the category Hex and Torx keys
How do I measure the size of an Allen key?
To measure the size of an Allen key, measure the distance between the opposite flat sides of its hexagonal cross-section - the so-called dimension across flats.
The easiest way to do this is with:
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,300,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.