DC/DC pārveidotāji

(32 122)

DC/DC converters are usually small-size components used to change direct current (DC) to DC with different parameters. They can be found in various packages (housings): as a single block adapted to THT (through-hole technology) mounting, e.g. in packages compliant with DIP standards (Dual In-line Package) or SIP (Single In-line Package), adapted to SMD (surface-mount device) mounting technology, but also in LGA packages (Land Grind Array) or in a brick standard of various sizes, e.g. half brick or quarter brick. Especially hobbyists, who do not create complex electronic circuits, will associate them with ready-made modules soldered onto PCBs or devices in packages for building-in or mounting on a DIN rail. The last type of mounting technology is mainly used in industrial control and electrical cabinets. The variety of packages in which DC/DC converters can be found results from their common use. Except for AC motors, direct current (DC) is used to power most electrical and electronic devices. For this reason, these components can be found, for example, as integrated circuits in computer power supplies, motherboards, or graphics cards, where they generate different DC voltages for the individual electronic components.

The main distinction among DC/DC converters is a result of the ratio of output voltage to their input voltage, so it is possible to find converters reducing voltage, called step-down converters, those increasing voltage, i.e. so-called step-up converters, or those that can produce at the output voltage that is both higher and lower than the input voltage, i.e. step-up/step-down converters. Very often, they feature adjustable output voltage, which allows to obtain a very wide range of its parameters. In such cases, it is usually set using a small potentiometer, integrated with the electronic circuit of the converter.

DC/DC converters – safeguards

Many DC/DC converters manufactured nowadays feature galvanically separated input and output. Such systems are often called isolated converters. This provides additional protection of the powered system against overvoltage and power surges, which could damage the converter itself as well as the powered device, resulting in permanent damage. Galvanic isolation of the input and output is required for safety reasons e.g. in medical devices. Of course DC/DC converters, as well as most other power supply devices, also offer other protections, among which we can distinguish continuous short-circuit protection, overload protection, overvoltage protection, reverse polarity protection, overheating protection or protection in the event of a drop in supply voltage. Simply put, the more protections a given device has, the lower the chance of a malfunction or permanent damage to the powered devices and the converter itself.

How to choose a DC/DC converter

While choosing the right DC/DC converter for your application, it is important to take a look at a few aspects. The first is the input voltage value, which is given in volts [V]. The input voltage range of a converter must contain the value of the voltage it will be supplied with. Applying too low voltage can cause converter malfunction, while applying too high input voltage can permanently damage it. Another parameter is the output voltage. The value that the user wants to obtain at the output of the converter should be determined depending on the devices that it will power. It must be identical with the value specified by the manufacturer of a given device in its technical documentation. The output voltage of DC/DC converters is often adjustable within a given range, thanks to which they can supply power to devices with different power supply parameters.

Another parameter which you must properly choose before buying the DC/DC converter is the maximum output current, given in amperes [A], often defined as the current efficiency. It represents the maximum electrical current that a given device can produce while still operating properly. The DC/DC converter current efficiency should be higher than the current required by the system being powered (in extreme cases equal to it). A power device operating within the limits of its maximum current efficiency will generate a significant amount of heat, which, if operated for a long time in such conditions, may lead to damage. This situation is particularly likely if the converter does not have any overload or overheat protection. It is good practice to choose a converter with a higher current efficiency than required. It is mainly to avoid work at the upper limit of its current efficiency, but also so as not lead to a situation where it is necessary to replace the currently installed converter with a new one, with a higher current efficiency, when the system undergoes slight expansion. Often, to compare which converter is more efficient, the power of a given converter is considered, which is given in watts [W]. Power is the product of voltage and current, so with equal voltage values it is easy to compare which device will be able to generate more current.

Another aspect that is sometimes important is the temperature range in which a given converter can operate. Some applications may require operation in sub-zero temperatures or in an environment where the temperature will be much higher than the room temperature. There are converters that are designed for temperatures as low as -50°C, but also for as extreme temperatures as 150°C. The temperature difference is significant, and when choosing a converter for a specific application, this aspect must not be overlooked in order not to damage the converter.

Some DC/DC converters can have more than one output. Then, each output has a different voltage value. Of course, in addition to the number of outputs, there can also be a larger number of electrical connections, e.g., in the form of a terminal strip integrated in the system. Sometimes DC/DC converters have integrated cables for electrical connection. When choosing this type of a device, you can also pay attention to its efficiency. The higher it is, the lower the power losses which most often occur as a conversion of electrical energy into thermal energy. To sum up, all DC/DC converter parameters should be selected depending on the target application and the criteria imposed by the cooperating elements, i.e., those supplying the converter and those that will be powered by it.

Produktu: 32 122

Noliktava:

TME
Ārējā
Visi
Lapa 1
TSR 1-2450 | Converter: DC/DC; Uin: 6.5÷36VDC; Uout: 5VDC; Iout: 1A; SIP3; THT
Converter: DC/DC; Uin: 6.5÷36VDC; Uout: 5VDC; Iout: 1A; SIP3; THT
Oriģināls simbols: TSR 1-2450
Ražotājs: TRACO POWER
Neto cena par daudzumiem no 1 gab - 5.58 USDBruto cena par daudzumiem no 1 gab - 6.74 USD
Neto cena par daudzumiem no 10 gab - 5.21 USDBruto cena par daudzumiem no 10 gab - 6.31 USD
Neto cena par daudzumiem no 100 gab - 4.86 USDBruto cena par daudzumiem no 100 gab - 5.88 USD
Neto cena par daudzumiem no 1000 gab - 4.51 USDBruto cena par daudzumiem no 1000 gab - 5.45 USD
7019 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
AM1S-0505SZ | Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP4
Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP4
Oriģināls simbols: AM1S-0505SZ
Ražotājs: AIMTEC
Neto cena par daudzumiem no 1 gab - 4.74 USDBruto cena par daudzumiem no 1 gab - 5.73 USD
Neto cena par daudzumiem no 5 gab - 3.81 USDBruto cena par daudzumiem no 5 gab - 4.61 USD
Neto cena par daudzumiem no 40 gab - 3.39 USDBruto cena par daudzumiem no 40 gab - 4.11 USD
Neto cena par daudzumiem no 80 gab - 3.27 USDBruto cena par daudzumiem no 80 gab - 3.95 USD
Neto cena par daudzumiem no 120 gab - 3.20 USDBruto cena par daudzumiem no 120 gab - 3.87 USD
Neto cena par daudzumiem no 1000 gab - 3.06 USDBruto cena par daudzumiem no 1000 gab - 3.71 USD
6467 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
R-78E5.0-0.5 | Converter: DC/DC; 2.5W; Uin: 7÷28VDC; Uout: 5VDC; Iout: 0.5A; SIP3
Converter: DC/DC; 2.5W; Uin: 7÷28VDC; Uout: 5VDC; Iout: 0.5A; SIP3
Oriģināls simbols: R-78E5.0-0.5
Ražotājs: RECOM
Neto cena par daudzumiem no 1 gab - 2.86 USDBruto cena par daudzumiem no 1 gab - 3.46 USD
Neto cena par daudzumiem no 25 gab - 2.68 USDBruto cena par daudzumiem no 25 gab - 3.24 USD
Neto cena par daudzumiem no 42 gab - 2.65 USDBruto cena par daudzumiem no 42 gab - 3.21 USD
2789 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
TSR 1-2433 | Converter: DC/DC; Uin: 4.75÷36VDC; Uout: 3.3VDC; Iout: 1A; SIP3; THT
Converter: DC/DC; Uin: 4.75÷36VDC; Uout: 3.3VDC; Iout: 1A; SIP3; THT
Oriģināls simbols: TSR 1-2433
Ražotājs: TRACO POWER
Neto cena par daudzumiem no 1 gab - 5.14 USDBruto cena par daudzumiem no 1 gab - 6.21 USD
Neto cena par daudzumiem no 5 gab - 4.75 USDBruto cena par daudzumiem no 5 gab - 5.75 USD
Neto cena par daudzumiem no 10 gab - 4.61 USDBruto cena par daudzumiem no 10 gab - 5.58 USD
4224 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
TSR 1-24120 | Converter: DC/DC; Uin: 15÷36VDC; Uout: 12VDC; Iout: 1A; SIP3; THT
Converter: DC/DC; Uin: 15÷36VDC; Uout: 12VDC; Iout: 1A; SIP3; THT
Oriģināls simbols: TSR 1-24120
Ražotājs: TRACO POWER
Neto cena par daudzumiem no 1 gab - 5.11 USDBruto cena par daudzumiem no 1 gab - 6.19 USD
Neto cena par daudzumiem no 5 gab - 4.75 USDBruto cena par daudzumiem no 5 gab - 5.75 USD
Neto cena par daudzumiem no 10 gab - 4.61 USDBruto cena par daudzumiem no 10 gab - 5.58 USD
2886 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
TEA 1-0505 | Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP4
Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP4
Oriģināls simbols: TEA 1-0505
Ražotājs: TRACO POWER
Neto cena par daudzumiem no 1 gab - 1.47 USDBruto cena par daudzumiem no 1 gab - 1.78 USD
Neto cena par daudzumiem no 5 gab - 1.39 USDBruto cena par daudzumiem no 5 gab - 1.69 USD
Neto cena par daudzumiem no 30 gab - 1.35 USDBruto cena par daudzumiem no 30 gab - 1.64 USD
Neto cena par daudzumiem no 100 gab - 1.32 USDBruto cena par daudzumiem no 100 gab - 1.59 USD
0 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
DDR-15G-5 | Converter: DC/DC; 15W; Uin: 9÷36VDC; Uout: 5VDC; Iout: 3A; DDR; OUT: 1
Converter: DC/DC; 15W; Uin: 9÷36VDC; Uout: 5VDC; Iout: 3A; DDR; OUT: 1
Oriģināls simbols: DDR-15G-5
Ražotājs: MEAN WELL
Neto cena par daudzumiem no 1 gab - 20.51 USDBruto cena par daudzumiem no 1 gab - 24.81 USD
Neto cena par daudzumiem no 5 gab - 19.50 USDBruto cena par daudzumiem no 5 gab - 23.60 USD
Neto cena par daudzumiem no 10 gab - 18.70 USDBruto cena par daudzumiem no 10 gab - 22.63 USD
Neto cena par daudzumiem no 20 gab - 18.10 USDBruto cena par daudzumiem no 20 gab - 21.91 USD
43 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
TSR 1-2450E | Converter: DC/DC; Uin: 7÷36VDC; Uout: 5VDC; Iout: 1A; SIP3; THT; OUT: 1
Converter: DC/DC; Uin: 7÷36VDC; Uout: 5VDC; Iout: 1A; SIP3; THT; OUT: 1
Oriģināls simbols: TSR 1-2450E
Ražotājs: TRACO POWER
Neto cena par daudzumiem no 1 gab - 3.21 USDBruto cena par daudzumiem no 1 gab - 3.89 USD
Neto cena par daudzumiem no 5 gab - 2.99 USDBruto cena par daudzumiem no 5 gab - 3.61 USD
Neto cena par daudzumiem no 10 gab - 2.82 USDBruto cena par daudzumiem no 10 gab - 3.41 USD
Neto cena par daudzumiem no 20 gab - 2.73 USDBruto cena par daudzumiem no 20 gab - 3.31 USD
0 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
R-78E5.0-1.0 | Converter: DC/DC; 5W; Uin: 8÷28VDC; Uout: 5VDC; Iout: 1A; SIP3; PCB
Converter: DC/DC; 5W; Uin: 8÷28VDC; Uout: 5VDC; Iout: 1A; SIP3; PCB
Oriģināls simbols: R-78E5.0-1.0
Ražotājs: RECOM
Neto cena par daudzumiem no 1 gab - 3.45 USDBruto cena par daudzumiem no 1 gab - 4.17 USD
Neto cena par daudzumiem no 42 gab - 3.25 USDBruto cena par daudzumiem no 42 gab - 3.93 USD
Neto cena par daudzumiem no 210 gab - 3.22 USDBruto cena par daudzumiem no 210 gab - 3.90 USD
597 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
TEA 1-0505E | Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP7
Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP7
Oriģināls simbols: TEA 1-0505E
Ražotājs: TRACO POWER
Neto cena par daudzumiem no 1 gab - 1.59 USDBruto cena par daudzumiem no 1 gab - 1.92 USD
Neto cena par daudzumiem no 5 gab - 1.50 USDBruto cena par daudzumiem no 5 gab - 1.82 USD
Neto cena par daudzumiem no 30 gab - 1.46 USDBruto cena par daudzumiem no 30 gab - 1.76 USD
Neto cena par daudzumiem no 100 gab - 1.40 USDBruto cena par daudzumiem no 100 gab - 1.70 USD
5915 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
DDR-15G-12 | Converter: DC/DC; 15W; Uin: 9÷36VDC; Uout: 12VDC; Iout: 1.25A; DDR
Converter: DC/DC; 15W; Uin: 9÷36VDC; Uout: 12VDC; Iout: 1.25A; DDR
Oriģināls simbols: DDR-15G-12
Ražotājs: MEAN WELL
Neto cena par daudzumiem no 1 gab - 20.51 USDBruto cena par daudzumiem no 1 gab - 24.81 USD
Neto cena par daudzumiem no 5 gab - 19.50 USDBruto cena par daudzumiem no 5 gab - 23.60 USD
Neto cena par daudzumiem no 10 gab - 18.70 USDBruto cena par daudzumiem no 10 gab - 22.63 USD
Neto cena par daudzumiem no 20 gab - 18.10 USDBruto cena par daudzumiem no 20 gab - 21.91 USD
635 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
RSD-60G-12 | Converter: DC/DC; 60W; Uin: 9÷36VDC; Uout: 12VDC; Iout: 5A; RSD; OUT: 1
Converter: DC/DC; 60W; Uin: 9÷36VDC; Uout: 12VDC; Iout: 5A; RSD; OUT: 1
Oriģināls simbols: RSD-60G-12
Ražotājs: MEAN WELL
Neto cena par daudzumiem no 1 gab - 43.70 USDBruto cena par daudzumiem no 1 gab - 52.88 USD
Neto cena par daudzumiem no 5 gab - 41.60 USDBruto cena par daudzumiem no 5 gab - 50.34 USD
Neto cena par daudzumiem no 10 gab - 39.81 USDBruto cena par daudzumiem no 10 gab - 48.16 USD
Neto cena par daudzumiem no 20 gab - 38.61 USDBruto cena par daudzumiem no 20 gab - 46.71 USD
75 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
TSR 2-2450 | Converter: DC/DC; Uin: 6.5÷36VDC; Uout: 5VDC; Iout: 2A; SIP3; THT
Converter: DC/DC; Uin: 6.5÷36VDC; Uout: 5VDC; Iout: 2A; SIP3; THT
Oriģināls simbols: TSR 2-2450
Ražotājs: TRACO POWER
Neto cena par daudzumiem no 1 gab - 11.43 USDBruto cena par daudzumiem no 1 gab - 13.82 USD
Neto cena par daudzumiem no 5 gab - 10.85 USDBruto cena par daudzumiem no 5 gab - 13.13 USD
Neto cena par daudzumiem no 30 gab - 10.42 USDBruto cena par daudzumiem no 30 gab - 12.60 USD
Neto cena par daudzumiem no 100 gab - 10.28 USDBruto cena par daudzumiem no 100 gab - 12.43 USD
0 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
DDR-120B-48 | Converter: DC/DC; 120W; Uin: 16.8÷33.6VDC; Uout: 48VDC; Iout: 2.5A
Converter: DC/DC; 120W; Uin: 16.8÷33.6VDC; Uout: 48VDC; Iout: 2.5A
Oriģināls simbols: DDR-120B-48
Ražotājs: MEAN WELL
Neto cena par daudzumiem no 1 gab - 69.20 USDBruto cena par daudzumiem no 1 gab - 83.74 USD
Neto cena par daudzumiem no 5 gab - 65.91 USDBruto cena par daudzumiem no 5 gab - 79.75 USD
Neto cena par daudzumiem no 10 gab - 63.00 USDBruto cena par daudzumiem no 10 gab - 76.23 USD
Neto cena par daudzumiem no 20 gab - 61.21 USDBruto cena par daudzumiem no 20 gab - 74.05 USD
63 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
OKI-78SR-5/1.5-W36-C | Converter: DC/DC; 7.5W; Uin: 7÷36VDC; Uout: 5VDC; Iout: 1.5A; THT
Converter: DC/DC; 7.5W; Uin: 7÷36VDC; Uout: 5VDC; Iout: 1.5A; THT
Oriģināls simbols: OKI-78SR-5/1.5-W36-C
Neto cena par daudzumiem no 1 gab - 4.69 USDBruto cena par daudzumiem no 1 gab - 5.68 USD
Neto cena par daudzumiem no 80 gab - 4.30 USDBruto cena par daudzumiem no 80 gab - 5.20 USD
Neto cena par daudzumiem no 100 gab - 4.13 USDBruto cena par daudzumiem no 100 gab - 5.00 USD
0 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
DDR-60G-24 | Converter: DC/DC; 60W; Uin: 9÷36VDC; Uout: 24VDC; Iout: 2.5A; DDR
Converter: DC/DC; 60W; Uin: 9÷36VDC; Uout: 24VDC; Iout: 2.5A; DDR
Oriģināls simbols: DDR-60G-24
Ražotājs: MEAN WELL
Neto cena par daudzumiem no 1 gab - 34.21 USDBruto cena par daudzumiem no 1 gab - 41.39 USD
Neto cena par daudzumiem no 5 gab - 32.60 USDBruto cena par daudzumiem no 5 gab - 39.45 USD
Neto cena par daudzumiem no 10 gab - 31.10 USDBruto cena par daudzumiem no 10 gab - 37.64 USD
Neto cena par daudzumiem no 20 gab - 30.21 USDBruto cena par daudzumiem no 20 gab - 36.55 USD
336 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
SBTN01L-05 | Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 20÷200mA
Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 20÷200mA
Oriģināls simbols: SBTN01L-05
Ražotājs: MEAN WELL
Neto cena par daudzumiem no 1 gab - 3.17 USDBruto cena par daudzumiem no 1 gab - 3.84 USD
Neto cena par daudzumiem no 5 gab - 3.00 USDBruto cena par daudzumiem no 5 gab - 3.62 USD
Neto cena par daudzumiem no 10 gab - 2.83 USDBruto cena par daudzumiem no 10 gab - 3.42 USD
Neto cena par daudzumiem no 20 gab - 2.65 USDBruto cena par daudzumiem no 20 gab - 3.20 USD
597 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
DDR-30G-12 | Converter: DC/DC; 30W; Uin: 9÷36VDC; Uout: 12VDC; Iout: 2.5A; DDR
Converter: DC/DC; 30W; Uin: 9÷36VDC; Uout: 12VDC; Iout: 2.5A; DDR
Oriģināls simbols: DDR-30G-12
Ražotājs: MEAN WELL
Neto cena par daudzumiem no 1 gab - 27.60 USDBruto cena par daudzumiem no 1 gab - 33.40 USD
Neto cena par daudzumiem no 5 gab - 26.21 USDBruto cena par daudzumiem no 5 gab - 31.71 USD
Neto cena par daudzumiem no 10 gab - 25.10 USDBruto cena par daudzumiem no 10 gab - 30.37 USD
Neto cena par daudzumiem no 20 gab - 24.40 USDBruto cena par daudzumiem no 20 gab - 29.53 USD
645 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
RFM-0505S | Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP4
Converter: DC/DC; 1W; Uin: 4.5÷5.5VDC; Uout: 5VDC; Iout: 200mA; SIP4
Oriģināls simbols: RFM-0505S
Ražotājs: RECOM
Neto cena par daudzumiem no 1 gab - 1.91 USDBruto cena par daudzumiem no 1 gab - 2.31 USD
Neto cena par daudzumiem no 42 gab - 1.73 USDBruto cena par daudzumiem no 42 gab - 2.08 USD
Neto cena par daudzumiem no 126 gab - 1.63 USDBruto cena par daudzumiem no 126 gab - 1.98 USD
1357 TME noliktavā
Gabalu skaits (Daudzkārtīgums: 1)
Minimālais daudzums, ko iespējams pasūtīt: 1.
Daudzkārtīgums: 1.
R-78K5.0-0.5 | Converter: DC/DC; Uin: 6.5÷36VDC; Uout: 5VDC; Iout: 500mA; SIP3; THT
Converter: DC/DC; Uin: 6.5÷36VDC; Uout: 5VDC; Iout: 500mA; SIP3; THT
Oriģināls simbols: R-78K5.0-0.5
Ražotājs: RECOM
Neto cena par daudzumiem no 1 gab - 2.75 USDBruto cena par daudzumiem no 1 gab - 3.32 USD
Neto cena par daudzumiem no 43 gab - 2.56 USDBruto cena par daudzumiem no 43 gab - 3.10 USD
Neto cena par daudzumiem no 86 gab - 2.48 USDBruto cena par daudzumiem no 86 gab - 3.00 USD
Neto cena par daudzumiem no 129 gab - 2.39 USDBruto cena par daudzumiem no 129 gab - 2.89 USD
375 TME noliktavā