+1 500 000 toodet pakkumises

7000 iga päev välja saadetavat pakki

+300 000 klienti 150 riigis

Quick Buy Lemmikud
Ostukorv

Teabebaas

What should be considered when choosing cable ties?

What should be considered when choosing cable ties?

Tie wraps are also called cable ties (or colloquially zip ties). The two first names indicate the main application and the mode of action which should be considered while choosing the components.

IP kaitseastmed ja IK mehaanilise kaitse klassid

IP kaitseastmed ja IK mehaanilise kaitse klassid

Seadmete või elektroonikatoodete valikul on oluline aspekt kasutaja ohutus. Korpusel ja pakendil nähtavad iseloomulikud märgid võimaldavad tutvuda konkreetse elemendi kaitse- ja tihedusastmega.

Optimaalne juhtmekimbu valik

Optimaalne juhtmekimbu valik

Automaatika ja robootika maailmas on usaldusväärsus aluseks. Iga masina seiskumine võib tähendada kahjusid, seetõttu isegi näiliselt väikesed elemendid, nagu juhtmed kaablite juhtimissüsteemides, mängivad võtmerolli. Need vastutavad liikuvate osade süsteemidesse ohutu energia, signaalide ja meediumide tarnimise eest. Nende vale valik võib põhjustada kiiret kulumist, kahjustusi ja kulukaid rikkeid.

Choosing the right cables and inverters

Choosing the right cables and inverters

Knowledge of the working mechanism of inverters, their basic features and parameters can significantly facilitate the process of choosing the right device. The stability of the system depends on the device and its dedicated cabling.

Transformer as an element of household power supply units

Transformer as an element of household power supply units

While selecting a power supply unit, a consumer must often choose between a power supply unit and transformer. However, good choice is not a matter of buyer’s intuition, but depends on the knowledge regarding a given device and its power supply method.

Mälukaartide omadused ja valikukriteeriumid

Mälukaartide omadused ja valikukriteeriumid

Fotod ja filmid, mida me loome, mida loome isiklikuks või professionaalseks kasutamiseks, vajavad salvestusruumi ja võimalust reaalajas salvestada. See on mälukaartide roll, kui andmesalvestusruumi, mitmekesine ja kohandatud vastavalt seadmete vajadustele.

Fiber optic patchcords and pigtails

Fiber optic patchcords and pigtails

Data transmission with the use of light is currently the most modern technology supporting, among others, ICT and telecommunications industry. Fiber optics make it possible to transport data with a range that cannot be compared to an electrical signal and are the basis for the increase of the available Internet speed.

Selecting an inductive sensor – different diameters and outputs

Selecting an inductive sensor – different diameters and outputs

Appropriately selected inductive sensor serves as the basis for properly operating technological line and for devices using this kind of automation components everyday. Currently, sensors are responsible for measurements, localising metal objects, counting, or drawing up transport routes in numerous manufacturing industries.

Juhtkaabli valiku juhised

Juhtkaabli valiku juhised

Kontrollkaablid kasutatakse andmete edastamiseks masinatele ja seadmetele, mida kasutatakse tootmisprotsesside liinides. Automaatikasüsteemide ja struktuurlahenduste pideva arengu tõttu seisavad kontrollkaablite tootjad silmitsi üha rangemate nõuetega.

Data acquisition and Industry 4.0

Data acquisition and Industry 4.0

Industry 4.0 aims to create an intelligent factory, combining the intelligence of IT systems with automation.

How to connect an electric motor to an Arduino platform?

How to connect an electric motor to an Arduino platform?

The use of Arduino to control electric motors gives designers a wide range of possibilities.

KKK - kõige populaarsemad küsimused patareide ja akude kohta

KKK - kõige populaarsemad küsimused patareide ja akude kohta