+1 300 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
SMD (Standard Military Drawing) is a designation used in United States military documentation, referring to standardized technical drawings of electronic components developed for the needs of the U.S. Armed Forces. This standard was introduced by the Defense Logistics Agency (DLA) to ensure uniform classification, identification, and quality control of components used in military, aerospace, and other high-reliability applications.
The Standard Military Drawing includes constructional, electrical, and environmental specifications for a given component, along with information about the manufacturer, catalog number, limiting parameters, and testing methods. The objective of this system is to guarantee interoperability and repeatability of technical parameters across electronic components, regardless of the supplier—an essential factor in the long-term maintenance and logistics of weapon systems and military equipment.
In practice, the SMD designation may apply to resistors, capacitors, diodes, transistors, and other active and passive components that meet strict military standards (MIL-STD). SMD numbers are assigned by the appropriate institutions and are printed on components and included in technical documentation as unique identifiers of compliance with military standards. These often come with additional requirements related to radiation resistance, temperature range, humidity, vibration, or long-term parameter stability.
In civilian contexts, the term “SMD” is often incorrectly equated solely with surface-mount devices (Surface-Mount Device), but in military nomenclature, it specifically refers to technical drawing standards and quality specifications for components. The Standard Military Drawing thus represents a crucial element of the quality assurance and reliability framework in critical applications, where only components with documented compliance to military requirements are acceptable.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,300,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.