You are browsing the website for customers from: United Kingdom. Based on location data, the suggested version of the page for you is USA / US

+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Motion detector (PIR) - definition

PIR (Passive Infrared) motion detector. Passive Infrared) is a detection device using passive infrared infrared to identify changes in the thermal radiation emitted by objects in the detector's field of view. Its operation is based on the analysis of temperature differences between the background and a moving heat source, usually a human or animal, which makes it a key component of automation systems, alarm and control systems.

The core of the design is a pyroelectric infrared detector, made of a material with properties that allow it to convert thermal radiation into an electrical signal. This element reacts to dynamic temperature changes, therefore, static heat sources do not activate the system. To increase the detection performance, pIR sensors are fitted with Fresnel lenses or optical reflectors, which modify the field of field of view, by dividing it into sectors of varying sensitivity, which allows more efficient motion detection and minimises false alarms.

The detector electronics comprise a signal amplifier and a data processing circuit, which analyses the voltage differences generated by the detector and decides whether to activate the control output. Modern designs often incorporate temperature compensation systems, algorithms filtering algorithms and interfaces communication interfaces for integration into intelligent control systems. Additional functions, such as sensitivity adjustment, detection range or response time, allow the sensor to be tailored to specific application conditions.

PRI motion sensors are widely used in security systems, building automation and energy-efficient lighting control. Their ability to detect presence without actively emitting electromagnetic waves makes them, they are energy-efficient and do not interfere with other electronic devices. This technology, combined with modern methods of signal processing methods, allows high-precision detection with reduced false triggering, resulting from environmental factors or mechanical interference.

PIR sensors

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO