You are browsing the website for customers from: United Kingdom. Based on location data, the suggested version of the page for you is USA / US

+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Joystick - definition

A Joystick is an input device used to control movement or position in electronic, computer and mechatronic systems. It consists of a lever whose position is recorded relative to one or more axes and then converted into electrical signals transmitted to the system being controlled. The mechanism of operation of a joystick is usually based on analogue (e.g. potentiometric, magnetic or optical) or digital (e.g. Microswitches or Encoders) transducers that detect swings in the X, Y and sometimes Z or rotary axes.

Joysticks are used in applications ranging from computer games and simulators to industrial control desktops to systems Automation, robotics, medical devices and mobile machine control. In interactive systems, they act as an ergonomic interface user interface for intuitive control of objects, navigation in three-dimensional space or adjustment of parameters. In specialised applications, Joysticks can be equipped with additional buttons, rollers and switches to enable multiple functions to be performed simultaneously.

Thanks to its design, the joystick enables smooth proportional control, where the degree of tilt translates into the intensity or speed of the actuation system. In analogue versions, the output signal is a voltage depending on the position of the lever, while digital versions generate logic pulses corresponding to specific directions of movement. Advanced models can use Capacitive Sensors, gyroscopes or haptic systems, increasing precision and interactivity.

Joystick design must consider mechanical factors such as durability, overload resistance, elasticity of return to neutral position and signal stability under vibration conditions. In industrial interfaces, these devices often communicate using analogue standards (0-10 V, 4-20 mA) or digital transmission protocols such as USB, CAN or RS-232, depending on the application environment.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO