+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Fuseholders for Cable

(94)

The idea of using different types of fuses in a wide range of electrical and electronic applications has been known for a long time and is present in every new project or device. The simplest and in many respects most effective solution is the so-called overcurrent protection. If the device has a specific current rating, a sudden or long-lasting increase in this parameter may indicate a device malfunction. As a result, electronic devices, actuators, or wire insulation may catch fire. There can be many reasons for an increase in the current value, such as the seizure of the bearings, which, when blocked, start to draw continuously more current than the rated current (in the case of high shaft load), or a short circuit in the electronic part of the power supply of the device, caused, for example, by the breakdown of a rectifying diode.

Overcurrent protection devices, which are called circuit breakers, can be found in every household distribution board. In older installations, these can be D-type fuses or automatic fuses. Circuit breakers are reusable; just flip the switch back to protect the circuit again; panels in older houses use fuses. Although the latter are no longer used as overcurrent protection in modern household electrical installations, they are still widely used in electronic circuits.

The main component of the fuse, is a metal (usually made of copper) wire (one wire or several wires in parallel). Heat energy is generated across a wire due to the current flowing through it; this is related to current intensity. If this is too high, the amount of heat released will eventually melt the wire, which will consequently disconnect the current circuit.

Cable fuse and the type of electrical wire

If you are designing a device yourself or want to add a fuse to an existing machine that does not have such overcurrent protection, you can use, for example, cable fuse holders, i.e., the popular cable fuses. However, it should be borne in mind that we can only use it for a single conductor cable - it will be impossible to use it for multicore cables.

Selection of cable fuse

To select the right cable fuse you need to specify several criteria. The first of these is the outer diameter of the cable. Some cable fuses are supplied with pre-wired cables of the length and cross-section specified by the manufacturer. The most common sizes defining their conductor diameter range from 10 to 20 AWG (American Wire Gauge).

You also need to remember the rated voltage of the fuse holder. This is an especially important parameter that must be taken into account to maintain the safety of the device. These values will range from about 32 V to 600 V.The next key parameter is the current rating of the fuse holder. The higher the current, the larger the amount of heat generated. The current ratings can range from 1A up to 30 A. It is important that this value, assigned to a particular fuse holder, is at least equal, although it is recommended to be greater than the rated current of the fuse that will be used.Sometimes it may be important, especially when using such a fuse holder, to know the dimensions of the compatible fuse. Cylindrical fuses come in the following sizes: 5x20mm, 6.3x25mm, 6.3x30mm, or 6.3x32mm. Fuse cables can also differ in the fuse body material, colour, operating temperature, or contact material. This is usually less important information but is nevertheless worth knowing.

Products: 94

Warehouse:

TME
External
All
Page 1
R3-32A2A | Fuse holder; 5x20mm; on cable; Imax: 15A; brass; nickel plated
Fuse holder; 5x20mm; on cable; Imax: 15A; brass; nickel plated
Manufacturer part number: R3-32A2A
Manufacturer: SCI
Net price for quantities from 1 pcs - 1.41 USDGross price for quantities from 1 pcs - 1.41 USD
Net price for quantities from 5 pcs - 1.21 USDGross price for quantities from 5 pcs - 1.21 USD
Net price for quantities from 20 pcs - 1.00 USDGross price for quantities from 20 pcs - 1.00 USD
Net price for quantities from 100 pcs - 0.84 USDGross price for quantities from 100 pcs - 0.84 USD
Net price for quantities from 500 pcs - 0.70 USDGross price for quantities from 500 pcs - 0.70 USD
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
FX0380 | Fuse holder; 5x20mm; on cable; Imax: 10A; Urated: 50V; Leads: cables
Fuse holder; 5x20mm; on cable; Imax: 10A; Urated: 50V; Leads: cables
Manufacturer part number: FX0380
Manufacturer: BULGIN
Net price for quantities from 1 pcs - 7.64 USDGross price for quantities from 1 pcs - 7.64 USD
Net price for quantities from 5 pcs - 6.37 USDGross price for quantities from 5 pcs - 6.37 USD
Net price for quantities from 10 pcs - 5.92 USDGross price for quantities from 10 pcs - 5.92 USD
Net price for quantities from 50 pcs - 5.00 USDGross price for quantities from 50 pcs - 5.00 USD
Net price for quantities from 100 pcs - 4.72 USDGross price for quantities from 100 pcs - 4.72 USD
Net price for quantities from 125 pcs - 4.62 USDGross price for quantities from 125 pcs - 4.62 USD
Net price for quantities from 250 pcs - 4.34 USDGross price for quantities from 250 pcs - 4.34 USD
Net price for quantities from 300 pcs - 4.26 USDGross price for quantities from 300 pcs - 4.26 USD
Net price for quantities from 600 pcs - 4.00 USDGross price for quantities from 600 pcs - 4.00 USD
Net price for quantities from 1200 pcs - 3.76 USDGross price for quantities from 1200 pcs - 3.76 USD
10813 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
FX0380/BK | Fuse holder; 5x20mm; on cable; Imax: 10A; Urated: 50V; Leads: cables
Fuse holder; 5x20mm; on cable; Imax: 10A; Urated: 50V; Leads: cables
Manufacturer part number: FX0380/BK
Manufacturer: BULGIN
Net price for quantities from 1 pcs - 6.52 USDGross price for quantities from 1 pcs - 6.52 USD
Net price for quantities from 2 pcs - 6.30 USDGross price for quantities from 2 pcs - 6.30 USD
Net price for quantities from 5 pcs - 5.60 USDGross price for quantities from 5 pcs - 5.60 USD
Net price for quantities from 10 pcs - 5.27 USDGross price for quantities from 10 pcs - 5.27 USD
Net price for quantities from 25 pcs - 5.02 USDGross price for quantities from 25 pcs - 5.02 USD
Net price for quantities from 75 pcs - 4.01 USDGross price for quantities from 75 pcs - 4.01 USD
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
FX0385 | Fuse holder; 5x20mm; on cable; Imax: 10A; Urated: 50V; Leads: cables
Fuse holder; 5x20mm; on cable; Imax: 10A; Urated: 50V; Leads: cables
Manufacturer part number: FX0385
Manufacturer: BULGIN
Net price for quantities from 1 pcs - 13.31 USDGross price for quantities from 1 pcs - 13.31 USD
Net price for quantities from 5 pcs - 8.55 USDGross price for quantities from 5 pcs - 8.55 USD
Net price for quantities from 10 pcs - 8.22 USDGross price for quantities from 10 pcs - 8.22 USD
Net price for quantities from 25 pcs - 7.83 USDGross price for quantities from 25 pcs - 7.83 USD
Net price for quantities from 50 pcs - 7.55 USDGross price for quantities from 50 pcs - 7.55 USD
Net price for quantities from 100 pcs - 7.24 USDGross price for quantities from 100 pcs - 7.24 USD
Net price for quantities from 200 pcs - 6.94 USDGross price for quantities from 200 pcs - 6.94 USD
Net price for quantities from 300 pcs - 6.77 USDGross price for quantities from 300 pcs - 6.77 USD
Net price for quantities from 600 pcs - 6.47 USDGross price for quantities from 600 pcs - 6.47 USD
Net price for quantities from 1200 pcs - 6.17 USDGross price for quantities from 1200 pcs - 6.17 USD
4120 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
R3-48 | Fuse holder; 5x20mm; on cable; Imax: 5A; brass; tinned; 20AWG
Fuse holder; 5x20mm; on cable; Imax: 5A; brass; tinned; 20AWG
Manufacturer part number: R3-48
Manufacturer: SCI
Net price for quantities from 1 pcs - 1.40 USDGross price for quantities from 1 pcs - 1.40 USD
Net price for quantities from 5 pcs - 1.21 USDGross price for quantities from 5 pcs - 1.21 USD
Net price for quantities from 20 pcs - 1.07 USDGross price for quantities from 20 pcs - 1.07 USD
Net price for quantities from 100 pcs - 0.81 USDGross price for quantities from 100 pcs - 0.81 USD
Net price for quantities from 500 pcs - 0.75 USDGross price for quantities from 500 pcs - 0.75 USD
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
8601.2001.08 | Fuse holder; 5x20mm; on cable; Urated: 32V; bronze; tinned; UL94V-0
Fuse holder; 5x20mm; on cable; Urated: 32V; bronze; tinned; UL94V-0
Manufacturer part number: 8601.2001.08
Manufacturer: SCHURTER
Net price for quantities from 1 pcs - 2.82 USDGross price for quantities from 1 pcs - 2.82 USD
Net price for quantities from 5 pcs - 2.50 USDGross price for quantities from 5 pcs - 2.50 USD
Net price for quantities from 10 pcs - 2.34 USDGross price for quantities from 10 pcs - 2.34 USD
Net price for quantities from 20 pcs - 2.19 USDGross price for quantities from 20 pcs - 2.19 USD
Net price for quantities from 50 pcs - 1.99 USDGross price for quantities from 50 pcs - 1.99 USD
Net price for quantities from 100 pcs - 1.84 USDGross price for quantities from 100 pcs - 1.84 USD
Net price for quantities from 250 pcs - 1.67 USDGross price for quantities from 250 pcs - 1.67 USD
Net price for quantities from 500 pcs - 1.55 USDGross price for quantities from 500 pcs - 1.55 USD
Net price for quantities from 1000 pcs - 1.46 USDGross price for quantities from 1000 pcs - 1.46 USD
Net price for quantities from 5000 pcs - 1.38 USDGross price for quantities from 5000 pcs - 1.38 USD
2319 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
ZH9-20ZW | Fuse holder; 5x20mm; on cable; Imax: 1.165A; 0.258mm2; 23AWG
Fuse holder; 5x20mm; on cable; Imax: 1.165A; 0.258mm2; 23AWG
Manufacturer part number: ZH9-20ZW
Manufacturer: PROFFUSE
Net price for quantities from 5 pcs - 0.59 USDGross price for quantities from 5 pcs - 0.59 USD
Net price for quantities from 40 pcs - 0.54 USDGross price for quantities from 40 pcs - 0.54 USD
Net price for quantities from 100 pcs - 0.47 USDGross price for quantities from 100 pcs - 0.47 USD
Net price for quantities from 500 pcs - 0.42 USDGross price for quantities from 500 pcs - 0.42 USD
Net price for quantities from 1000 pcs - 0.35 USDGross price for quantities from 1000 pcs - 0.35 USD
3118 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 5.
Multiple of: 1.
01500274Z | Fuse holder; 5x20mm; on cable; Imax: 10A; brass; Leads: cables
Fuse holder; 5x20mm; on cable; Imax: 10A; brass; Leads: cables
Manufacturer part number: 01500274Z
Manufacturer: LITTELFUSE
Net price for quantities from 1 pcs - 3.60 USDGross price for quantities from 1 pcs - 3.60 USD
Net price for quantities from 5 pcs - 2.96 USDGross price for quantities from 5 pcs - 2.96 USD
Net price for quantities from 10 pcs - 2.80 USDGross price for quantities from 10 pcs - 2.80 USD
Net price for quantities from 25 pcs - 2.68 USDGross price for quantities from 25 pcs - 2.68 USD
1089 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
8601.2000 | Fuse holder; 5x20mm; on cable; Urated: 32V; bronze; tinned; UL94V-0
Fuse holder; 5x20mm; on cable; Urated: 32V; bronze; tinned; UL94V-0
Manufacturer part number: 8601.2000
Manufacturer: SCHURTER
Net price for quantities from 1 pcs - 2.14 USDGross price for quantities from 1 pcs - 2.14 USD
Net price for quantities from 5 pcs - 1.96 USDGross price for quantities from 5 pcs - 1.96 USD
Net price for quantities from 10 pcs - 1.82 USDGross price for quantities from 10 pcs - 1.82 USD
Net price for quantities from 20 pcs - 1.66 USDGross price for quantities from 20 pcs - 1.66 USD
Net price for quantities from 50 pcs - 1.45 USDGross price for quantities from 50 pcs - 1.45 USD
Net price for quantities from 100 pcs - 1.38 USDGross price for quantities from 100 pcs - 1.38 USD
Net price for quantities from 200 pcs - 1.30 USDGross price for quantities from 200 pcs - 1.30 USD
Net price for quantities from 250 pcs - 1.27 USDGross price for quantities from 250 pcs - 1.27 USD
Net price for quantities from 500 pcs - 1.21 USDGross price for quantities from 500 pcs - 1.21 USD
Net price for quantities from 1000 pcs - 1.15 USDGross price for quantities from 1000 pcs - 1.15 USD
1574 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
R3-64 | Fuse holder; 6.3x30mm,6.3x32mm; on cable; Imax: 10A; brass; 16AWG
Fuse holder; 6.3x30mm,6.3x32mm; on cable; Imax: 10A; brass; 16AWG
Manufacturer part number: R3-64
Manufacturer: SCI
Net price for quantities from 1 pcs - 1.22 USDGross price for quantities from 1 pcs - 1.22 USD
Net price for quantities from 5 pcs - 1.11 USDGross price for quantities from 5 pcs - 1.11 USD
Net price for quantities from 20 pcs - 0.92 USDGross price for quantities from 20 pcs - 0.92 USD
Net price for quantities from 100 pcs - 0.80 USDGross price for quantities from 100 pcs - 0.80 USD
Net price for quantities from 500 pcs - 0.67 USDGross price for quantities from 500 pcs - 0.67 USD
0 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
LPC-24B-12R | Fuse holder; 5x20mm; Imax: 20A; brass; nickel plated; Leads: cables
Fuse holder; 5x20mm; Imax: 20A; brass; nickel plated; Leads: cables
Manufacturer part number: LPC-24B-12R
Manufacturer: OPTIFUSE
Net price for quantities from 1 pcs - 4.80 USDGross price for quantities from 1 pcs - 4.80 USD
Net price for quantities from 20 pcs - 4.33 USDGross price for quantities from 20 pcs - 4.33 USD
Net price for quantities from 50 pcs - 3.41 USDGross price for quantities from 50 pcs - 3.41 USD
Net price for quantities from 100 pcs - 2.94 USDGross price for quantities from 100 pcs - 2.94 USD
Net price for quantities from 200 pcs - 2.79 USDGross price for quantities from 200 pcs - 2.79 USD
530 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
01500322H | Fuse holder; 6.3x32mm; THT; Imax: 15A; Urated: 500V; Leads: cables
Fuse holder; 6.3x32mm; THT; Imax: 15A; Urated: 500V; Leads: cables
Manufacturer part number: 01500322H
Manufacturer: LITTELFUSE
Net price for quantities from 1 pcs - 7.74 USDGross price for quantities from 1 pcs - 7.74 USD
Net price for quantities from 2 pcs - 7.24 USDGross price for quantities from 2 pcs - 7.24 USD
Net price for quantities from 5 pcs - 6.53 USDGross price for quantities from 5 pcs - 6.53 USD
Net price for quantities from 10 pcs - 6.01 USDGross price for quantities from 10 pcs - 6.01 USD
Net price for quantities from 50 pcs - 5.07 USDGross price for quantities from 50 pcs - 5.07 USD
Net price for quantities from 100 pcs - 4.90 USDGross price for quantities from 100 pcs - 4.90 USD
1397 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
R3-32B2 | Fuse holder; 6.3x30mm,6.3x32mm; on cable; Imax: 15A; brass; 14AWG
Fuse holder; 6.3x30mm,6.3x32mm; on cable; Imax: 15A; brass; 14AWG
Manufacturer part number: R3-32B2
Manufacturer: SCI
Net price for quantities from 1 pcs - 1.57 USDGross price for quantities from 1 pcs - 1.57 USD
Net price for quantities from 5 pcs - 1.24 USDGross price for quantities from 5 pcs - 1.24 USD
Net price for quantities from 20 pcs - 0.97 USDGross price for quantities from 20 pcs - 0.97 USD
Net price for quantities from 100 pcs - 0.81 USDGross price for quantities from 100 pcs - 0.81 USD
Net price for quantities from 500 pcs - 0.65 USDGross price for quantities from 500 pcs - 0.65 USD
598 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
121720 | Fuse holder; 5x20mm,6.3x32mm; Imax: 6.3A; Leads: cables; 250VAC
Fuse holder; 5x20mm,6.3x32mm; Imax: 6.3A; Leads: cables; 250VAC
Manufacturer part number: 121720
Manufacturer: ESKA
Net price for quantities from 1 pcs - 1.90 USDGross price for quantities from 1 pcs - 1.90 USD
Net price for quantities from 20 pcs - 1.74 USDGross price for quantities from 20 pcs - 1.74 USD
Net price for quantities from 100 pcs - 1.53 USDGross price for quantities from 100 pcs - 1.53 USD
Net price for quantities from 200 pcs - 1.31 USDGross price for quantities from 200 pcs - 1.31 USD
Net price for quantities from 1000 pcs - 1.17 USDGross price for quantities from 1000 pcs - 1.17 USD
1227 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
Hardly available product
121710 | Fuse holder; 5x20mm,6.3x32mm; Imax: 6.3A; Leads: screw terminals
Fuse holder; 5x20mm,6.3x32mm; Imax: 6.3A; Leads: screw terminals
Manufacturer part number: 121710
Manufacturer: ESKA
Net price for quantities from 1 pcs - 1.40 USDGross price for quantities from 1 pcs - 1.40 USD
Net price for quantities from 20 pcs - 1.30 USDGross price for quantities from 20 pcs - 1.30 USD
Net price for quantities from 100 pcs - 1.14 USDGross price for quantities from 100 pcs - 1.14 USD
Net price for quantities from 200 pcs - 0.98 USDGross price for quantities from 200 pcs - 0.98 USD
Net price for quantities from 1000 pcs - 0.86 USDGross price for quantities from 1000 pcs - 0.86 USD
1456 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
Hardly available product
01500274LXN | Fuse holder; 5x20mm; Imax: 5A; Urated: 350V; Leads: cables; UL94V-0
Fuse holder; 5x20mm; Imax: 5A; Urated: 350V; Leads: cables; UL94V-0
Manufacturer part number: 01500274LXN
Manufacturer: LITTELFUSE
Net price for quantities from 1 pcs - 3.64 USDGross price for quantities from 1 pcs - 3.64 USD
Net price for quantities from 5 pcs - 3.07 USDGross price for quantities from 5 pcs - 3.07 USD
Net price for quantities from 10 pcs - 2.86 USDGross price for quantities from 10 pcs - 2.86 USD
Net price for quantities from 20 pcs - 2.69 USDGross price for quantities from 20 pcs - 2.69 USD
Net price for quantities from 40 pcs - 2.59 USDGross price for quantities from 40 pcs - 2.59 USD
302 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
FX0180 | Fuse holder; 6.3x32mm; on cable; Imax: 10A; Urated: 50V; UL94V-0
Fuse holder; 6.3x32mm; on cable; Imax: 10A; Urated: 50V; UL94V-0
Manufacturer part number: FX0180
Manufacturer: BULGIN
Net price for quantities from 1 pcs - 8.68 USDGross price for quantities from 1 pcs - 8.68 USD
Net price for quantities from 5 pcs - 7.04 USDGross price for quantities from 5 pcs - 7.04 USD
Net price for quantities from 10 pcs - 6.36 USDGross price for quantities from 10 pcs - 6.36 USD
Net price for quantities from 25 pcs - 5.48 USDGross price for quantities from 25 pcs - 5.48 USD
Net price for quantities from 50 pcs - 4.97 USDGross price for quantities from 50 pcs - 4.97 USD
Net price for quantities from 100 pcs - 4.72 USDGross price for quantities from 100 pcs - 4.72 USD
Net price for quantities from 125 pcs - 4.63 USDGross price for quantities from 125 pcs - 4.63 USD
Net price for quantities from 200 pcs - 4.46 USDGross price for quantities from 200 pcs - 4.46 USD
Net price for quantities from 250 pcs - 4.38 USDGross price for quantities from 250 pcs - 4.38 USD
Net price for quantities from 300 pcs - 4.31 USDGross price for quantities from 300 pcs - 4.31 USD
1196 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 1.
Multiple of: 1.
120100 | Fuse holder; 6.3x32mm; Imax: 16A; brass; nickel plated; 250VAC
Fuse holder; 6.3x32mm; Imax: 16A; brass; nickel plated; 250VAC
Manufacturer part number: 120100
Manufacturer: ESKA
Net price for quantities from 10 pcs - 0.08 USDGross price for quantities from 10 pcs - 0.08 USD
Net price for quantities from 20 pcs - 0.07 USDGross price for quantities from 20 pcs - 0.07 USD
Net price for quantities from 100 pcs - 0.06 USDGross price for quantities from 100 pcs - 0.06 USD
Net price for quantities from 200 pcs - 0.05 USDGross price for quantities from 200 pcs - 0.05 USD
Net price for quantities from 1000 pcs - 0.05 USDGross price for quantities from 1000 pcs - 0.05 USD
1320 in TME stock
No. of pieces (Multiple of: 10)
Minimum order quantity: 10.
Multiple of: 10.
Hardly available product
121000 | Fuse holder; 5x20mm; Imax: 6.3A; brass; silver plated; Leads: axial
Fuse holder; 5x20mm; Imax: 6.3A; brass; silver plated; Leads: axial
Manufacturer part number: 121000
Manufacturer: ESKA
Net price for quantities from 5 pcs - 0.21 USDGross price for quantities from 5 pcs - 0.21 USD
Net price for quantities from 20 pcs - 0.19 USDGross price for quantities from 20 pcs - 0.19 USD
Net price for quantities from 100 pcs - 0.17 USDGross price for quantities from 100 pcs - 0.17 USD
Net price for quantities from 200 pcs - 0.14 USDGross price for quantities from 200 pcs - 0.14 USD
Net price for quantities from 1000 pcs - 0.13 USDGross price for quantities from 1000 pcs - 0.13 USD
1014 in TME stock
No. of pieces (Multiple of: 1)
Minimum order quantity: 5.
Multiple of: 1.
Hardly available product
LPC-08B-18R | Fuse holder; 5x20mm; Imax: 10A; brass; Leads: cables; 18AWG; 250VAC
Fuse holder; 5x20mm; Imax: 10A; brass; Leads: cables; 18AWG; 250VAC
Manufacturer part number: LPC-08B-18R
Manufacturer: OPTIFUSE
Net price for quantities from 1 pcs - 3.77 USDGross price for quantities from 1 pcs - 3.77 USD
Net price for quantities from 20 pcs - 3.47 USDGross price for quantities from 20 pcs - 3.47 USD
Net price for quantities from 100 pcs - 3.18 USDGross price for quantities from 100 pcs - 3.18 USD
Net price for quantities from 200 pcs - 2.87 USDGross price for quantities from 200 pcs - 2.87 USD
82 in TME stock