+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Ring ferrites

(120)

Ring ferrites belong to the family of ferrite filters, also known as ferrite cores. These filters come in a variety of sizes and shapes, such as cylinders with a hole along their axis of rotation, or the previously mentioned rings. They are often found at the ends of various types of cables and wires, e.g. computer mice, switching power supplies, or USB cables, sometimes even on both sides, near the plugs, and thus close to the input and output ‘to’ and ‘from’ a particular device.

How do ring ferrites work?

Ferrite filters, in the simplest of terms, serve to supress, in both directions, high-frequency interference. Their operation does not differ much from commonly used chokes or inductors. In their applications, ferrites are characterised primarily by impedance, but indirectly they can introduce a kind of capacitance and also resistance into the circuit. Applied to both DC and AC conductors, they act as a low-pass filters, suppressing interference at higher frequencies, and in fact dissipating their energy by converting it into thermal energy, which is then given off to the environment. Interference can be the result of e.g. electromagnetic influence of another device or electronic circuit located near the output signal. Such a situation is typical e.g. for switching-mode power supplies, due to the specific nature of their operation and switching currents at high frequency. This interference is referred to as electromagnetic interference, the so-called EMI or RFI (radio-frequency interference) noise. A current flowing through a conductor, according to Ampère's law, creates a magnetic field around it. In the case of current interference, this field is not constant and is subject to fluctuations, which then interact with the ferrite filter. This, in turn, suppresses the electrical signal interference that arises in the conductor.

In simple terms, as the interference frequency increases, the impedance of the conductor on which the ferrite core is embedded increases. However, this is only half true. Ferrites have frequency characteristics that show for which oscillating voltage frequency values they have the highest impedance. After passing a certain frequency value, however, their impedance begins to decrease again. When selecting a suitable ring ferrite, it is extremely important to choose one whose impedance value is the highest for the interference frequencies of our system. To find them, and at the same time to choose a suitable filter, experiments and tests can be carried out, e.g. by using frequency analysis, otherwise known as spectrum analysis.

Choosing ring ferrites – what to look for?

When designing an electronic circuit in which we want to use a ring ferrite, its heating must be taken into account. It is therefore necessary to provide adequate passive or active cooling using forced air circulation, e.g. by a fan. High current values and large interference at high frequencies will not only cause a significant amount of heat to be emitted, but may also lead to the saturation of the ferrite core, i.e. a drop in its inductance by as much as 90%.

Ring ferrites application

Ferrite cores are a simple and inexpensive way to apply low-pass filtering to an already existing cable infrastructure, for example by creating a choke, or in other words, an inductor. In the case of ring ferrites it is sufficient to wrap a conductor several (typically 5 to 7) times through the centre around the ring to provide adequate filtering against high-frequency interference.

Ring ferrites can be found in outdoor cabling, but ferrite filters are just as often found inside various types of equipment, e.g. in the form of ferrite beads or chokes, as filters for incoming power, but also to filter signals directly on PCBs, near transistors, microprocessors and other integrated circuits, as well as connectors.

The application of ferrite filters is also useful in the case of devices that may emit radio frequency energy, because in such a case the cable may behave like an antenna, so the signal transmitted through will be distorted. Such a phenomenon may lead to unpredictable behaviour of powered devices. The same may occur for signal cables, which can cause distortions in communication between integrated circuits.

When selecting a ring ferrite, you should pay attention to several factors, depending on the specific application, currents flowing through the conductor, as well as the space available, e.g. in the housing of a given device. The dimensions of the filter can be taken into account, including the internal opening, which should allow for winding a wire of a given diameter through its centre several times, the material of the core, which will translate into its frequency characteristics, and the inductance factor. Before selecting a ferrite core, it is also worth reading its detailed technical documentation provided by the manufacturer, which will contain all the most important information, along with the aforementioned characteristics.

Products: 120

Warehouse:

TME
All
Page 1
NEW
5943002701 | Ferrite: toroidal; Core mat: 43; -55÷90°C; 885nH; 35.5x23x12.7mm
Ferrite: toroidal; Core mat: 43; -55÷90°C; 885nH; 35.5x23x12.7mm
Manufacturer part number: 5943002701
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 2.98 EURGross price for quantities from 1 pcs - 2.98 EUR
Net price for quantities from 5 pcs - 2.40 EURGross price for quantities from 5 pcs - 2.40 EUR
Net price for quantities from 10 pcs - 2.23 EURGross price for quantities from 10 pcs - 2.23 EUR
Net price for quantities from 25 pcs - 1.98 EURGross price for quantities from 25 pcs - 1.98 EUR
Net price for quantities from 53 pcs - 1.80 EURGross price for quantities from 53 pcs - 1.80 EUR
Net price for quantities from 106 pcs - 1.68 EURGross price for quantities from 106 pcs - 1.68 EUR
672 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5943003801 | Ferrite: toroidal; Core mat: 43; -55÷90°C; 1075nH; 61x35.55x12.7mm
Ferrite: toroidal; Core mat: 43; -55÷90°C; 1075nH; 61x35.55x12.7mm
Manufacturer part number: 5943003801
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 9.37 EURGross price for quantities from 1 pcs - 9.37 EUR
Net price for quantities from 20 pcs - 7.84 EURGross price for quantities from 20 pcs - 7.84 EUR
Net price for quantities from 40 pcs - 7.05 EURGross price for quantities from 40 pcs - 7.05 EUR
Net price for quantities from 60 pcs - 6.27 EURGross price for quantities from 60 pcs - 6.27 EUR
Net price for quantities from 80 pcs - 5.48 EURGross price for quantities from 80 pcs - 5.48 EUR
Net price for quantities from 100 pcs - 5.17 EURGross price for quantities from 100 pcs - 5.17 EUR
69 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5961001201 | Ferrite: toroidal; Core mat: 61; -55÷90°C; 145nH; 29x19x13.85mm
Ferrite: toroidal; Core mat: 61; -55÷90°C; 145nH; 29x19x13.85mm
Manufacturer part number: 5961001201
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 2.02 EURGross price for quantities from 1 pcs - 2.02 EUR
Net price for quantities from 74 pcs - 1.69 EURGross price for quantities from 74 pcs - 1.69 EUR
Net price for quantities from 148 pcs - 1.52 EURGross price for quantities from 148 pcs - 1.52 EUR
Net price for quantities from 223 pcs - 1.35 EURGross price for quantities from 223 pcs - 1.35 EUR
Net price for quantities from 297 pcs - 1.18 EURGross price for quantities from 297 pcs - 1.18 EUR
Net price for quantities from 371 pcs - 1.11 EURGross price for quantities from 371 pcs - 1.11 EUR
729 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5952003801 | Ferrite: toroidal; Core mat: 52; -55÷90°C; 325nH; 61x35.55x12.7mm
Ferrite: toroidal; Core mat: 52; -55÷90°C; 325nH; 61x35.55x12.7mm
Manufacturer part number: 5952003801
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 10.74 EURGross price for quantities from 1 pcs - 10.74 EUR
Net price for quantities from 5 pcs - 9.37 EURGross price for quantities from 5 pcs - 9.37 EUR
Net price for quantities from 10 pcs - 8.15 EURGross price for quantities from 10 pcs - 8.15 EUR
Net price for quantities from 25 pcs - 7.55 EURGross price for quantities from 25 pcs - 7.55 EUR
Net price for quantities from 100 pcs - 7.08 EURGross price for quantities from 100 pcs - 7.08 EUR
94 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5961002701 | Ferrite: toroidal; Core mat: 61; -55÷90°C; 140nH; 35.55x23x12.7mm
Ferrite: toroidal; Core mat: 61; -55÷90°C; 140nH; 35.55x23x12.7mm
Manufacturer part number: 5961002701
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 3.26 EURGross price for quantities from 1 pcs - 3.26 EUR
Net price for quantities from 5 pcs - 2.62 EURGross price for quantities from 5 pcs - 2.62 EUR
Net price for quantities from 10 pcs - 2.44 EURGross price for quantities from 10 pcs - 2.44 EUR
Net price for quantities from 25 pcs - 2.18 EURGross price for quantities from 25 pcs - 2.18 EUR
Net price for quantities from 53 pcs - 1.90 EURGross price for quantities from 53 pcs - 1.90 EUR
Net price for quantities from 106 pcs - 1.80 EURGross price for quantities from 106 pcs - 1.80 EUR
330 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5967002701 | Ferrite: toroidal; Core mat: 67; -55÷90°C; 45nH; 35.55x23x12.7mm
Ferrite: toroidal; Core mat: 67; -55÷90°C; 45nH; 35.55x23x12.7mm
Manufacturer part number: 5967002701
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 6.31 EURGross price for quantities from 1 pcs - 6.31 EUR
Net price for quantities from 42 pcs - 5.26 EURGross price for quantities from 42 pcs - 5.26 EUR
Net price for quantities from 84 pcs - 4.74 EURGross price for quantities from 84 pcs - 4.74 EUR
Net price for quantities from 126 pcs - 4.21 EURGross price for quantities from 126 pcs - 4.21 EUR
Net price for quantities from 168 pcs - 3.68 EURGross price for quantities from 168 pcs - 3.68 EUR
Net price for quantities from 210 pcs - 3.47 EURGross price for quantities from 210 pcs - 3.47 EUR
301 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5961000601 | Ferrite: toroidal; Core mat: 61; -55÷90°C; 75nH; 21x13.2x6.35mm
Ferrite: toroidal; Core mat: 61; -55÷90°C; 75nH; 21x13.2x6.35mm
Manufacturer part number: 5961000601
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 1.22 EURGross price for quantities from 1 pcs - 1.22 EUR
Net price for quantities from 183 pcs - 1.01 EURGross price for quantities from 183 pcs - 1.01 EUR
Net price for quantities from 365 pcs - 0.91 EURGross price for quantities from 365 pcs - 0.91 EUR
Net price for quantities from 548 pcs - 0.81 EURGross price for quantities from 548 pcs - 0.81 EUR
Net price for quantities from 730 pcs - 0.72 EURGross price for quantities from 730 pcs - 0.72 EUR
Net price for quantities from 913 pcs - 0.67 EURGross price for quantities from 913 pcs - 0.67 EUR
909 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5961003801 | Ferrite: toroidal; Core mat: 61; -55÷90°C; 170nH; 61x35.55x12.7mm
Ferrite: toroidal; Core mat: 61; -55÷90°C; 170nH; 61x35.55x12.7mm
Manufacturer part number: 5961003801
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 13.30 EURGross price for quantities from 1 pcs - 13.30 EUR
Net price for quantities from 20 pcs - 11.08 EURGross price for quantities from 20 pcs - 11.08 EUR
Net price for quantities from 40 pcs - 9.98 EURGross price for quantities from 40 pcs - 9.98 EUR
Net price for quantities from 60 pcs - 8.87 EURGross price for quantities from 60 pcs - 8.87 EUR
Net price for quantities from 80 pcs - 7.76 EURGross price for quantities from 80 pcs - 7.76 EUR
Net price for quantities from 100 pcs - 7.31 EURGross price for quantities from 100 pcs - 7.31 EUR
98 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5961001001 | Ferrite: toroidal; Core mat: 61; -55÷90°C; 80nH; 29x19x7.5mm
Ferrite: toroidal; Core mat: 61; -55÷90°C; 80nH; 29x19x7.5mm
Manufacturer part number: 5961001001
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 1.36 EURGross price for quantities from 1 pcs - 1.36 EUR
Net price for quantities from 95 pcs - 1.14 EURGross price for quantities from 95 pcs - 1.14 EUR
Net price for quantities from 191 pcs - 1.02 EURGross price for quantities from 191 pcs - 1.02 EUR
Net price for quantities from 286 pcs - 0.91 EURGross price for quantities from 286 pcs - 0.91 EUR
Net price for quantities from 382 pcs - 0.79 EURGross price for quantities from 382 pcs - 0.79 EUR
Net price for quantities from 477 pcs - 0.75 EURGross price for quantities from 477 pcs - 0.75 EUR
954 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
5978003801 | Ferrite: toroidal; Core mat: 78; -55÷90°C; 3155nH; 61x35.55x12.7mm
Ferrite: toroidal; Core mat: 78; -55÷90°C; 3155nH; 61x35.55x12.7mm
Manufacturer part number: 5978003801
Manufacturer: FAIR-RITE
Net price for quantities from 1 pcs - 9.81 EURGross price for quantities from 1 pcs - 9.81 EUR
Net price for quantities from 20 pcs - 8.15 EURGross price for quantities from 20 pcs - 8.15 EUR
Net price for quantities from 40 pcs - 7.33 EURGross price for quantities from 40 pcs - 7.33 EUR
Net price for quantities from 60 pcs - 6.51 EURGross price for quantities from 60 pcs - 6.51 EUR
Net price for quantities from 80 pcs - 5.71 EURGross price for quantities from 80 pcs - 5.71 EUR
Net price for quantities from 100 pcs - 5.38 EURGross price for quantities from 100 pcs - 5.38 EUR
100 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Ferrite: toroidal; Øint: 13.97mm; Øout: 22.86mm; 90nH; H: 7.62mm
Manufacturer part number: MP-090125-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 4.49 EURGross price for quantities from 1 pcs - 4.49 EUR
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Ferrite: toroidal; Core mat: 75; -55÷90°C; 785nH; 5.95x3.05x1.65mm
Manufacturer part number: 5975000101
Manufacturer: FAIR-RITE
Net price for quantities from 6000 pcs - 0.12 EURGross price for quantities from 6000 pcs - 0.12 EUR
0 in TME stock
No. of pieces (Multiplicity: 6 000)
Minimum order quantity: 6 000.
Multiplicity: 6 000.
NEW
Ferrite: toroidal; Øint: 14.22mm; Øout: 23.93mm; 2.9nH; H: 7.92mm
Manufacturer part number: T94-17
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 1.43 EURGross price for quantities from 1 pcs - 1.43 EUR
Net price for quantities from 5 pcs - 1.24 EURGross price for quantities from 5 pcs - 1.24 EUR
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Ferrite: toroidal; Øint: 31.75mm; Øout: 50.8mm; 12nH; H: 13.97mm
Manufacturer part number: T200-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 7.76 EURGross price for quantities from 1 pcs - 7.76 EUR
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Ferrite: toroidal; Øint: 5.21mm; Øout: 9.53mm; 4nH; H: 3.25mm
Manufacturer part number: T37-2
Manufacturer: MICROMETALS
Net price for quantities from 1 pcs - 0.59 EURGross price for quantities from 1 pcs - 0.59 EUR
Net price for quantities from 5 pcs - 0.47 EURGross price for quantities from 5 pcs - 0.47 EUR
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Ferrite: toroidal; Core mat: 75; -55÷90°C; 6uH; 12.7x7.9x12.7mm
Manufacturer part number: 5975001901
Manufacturer: FAIR-RITE
Net price for quantities from 1052 pcs - 0.57 EURGross price for quantities from 1052 pcs - 0.57 EUR
0 in TME stock
No. of pieces (Multiplicity: 1 052)
Minimum order quantity: 1 052.
Multiplicity: 1 052.
NEW
Ferrite: toroidal; Core mat: 61; -55÷90°C; 69nH; 12.7x7.15x4.9mm
Manufacturer part number: 5961000301
Manufacturer: FAIR-RITE
Net price for quantities from 3360 pcs - 0.23 EURGross price for quantities from 3360 pcs - 0.23 EUR
0 in TME stock
No. of pieces (Multiplicity: 3 360)
Minimum order quantity: 3 360.
Multiplicity: 3 360.
NEW
Ferrite: toroidal; Core mat: 77; -55÷90°C; 2.95uH; 61x35.55x12.7mm
Manufacturer part number: 5977003801
Manufacturer: FAIR-RITE
Net price for quantities from 200 pcs - 4.39 EURGross price for quantities from 200 pcs - 4.39 EUR
0 in TME stock
No. of pieces (Multiplicity: 200)
Minimum order quantity: 200.
Multiplicity: 200.
NEW
Ferrite: toroidal; Core mat: 77; -55÷90°C; 1.3uH; 12.7x7.9x6.35mm
Manufacturer part number: 5977001101
Manufacturer: FAIR-RITE
Net price for quantities from 2800 pcs - 0.23 EURGross price for quantities from 2800 pcs - 0.23 EUR
0 in TME stock
No. of pieces (Multiplicity: 2 800)
Minimum order quantity: 2 800.
Multiplicity: 2 800.
NEW
Ferrite: toroidal; Core mat: 43; -55÷90°C; 470nH; 21x13.2x6.35mm
Manufacturer part number: 5943000601
Manufacturer: FAIR-RITE
Net price for quantities from 1826 pcs - 0.48 EURGross price for quantities from 1826 pcs - 0.48 EUR
0 in TME stock
No. of pieces (Multiplicity: 1 826)
Minimum order quantity: 1 826.
Multiplicity: 1 826.